![]() |
![]() |
BLE-Stack APIs
3.00.01
|
Connection parameters for the peripheral device. More...
Data Fields | |
uint16_t | intervalMax |
2 Byte More... | |
uint16_t | intervalMin |
2 Byte More... | |
uint16_t | latency |
2 Byte More... | |
uint16_t | timeout |
2 Byte More... | |
Connection parameters for the peripheral device.
These numbers are used to compare against connection events and request connection parameter updates with the master. this structure is used to update the parameter SNP_GGS_PERI_CONN_PARAM_ATT of the GAP/GATT service.
uint16_t intervalMax |
2 Byte
uint16_t intervalMin |
2 Byte
uint16_t latency |
2 Byte
uint16_t timeout |
2 Byte