![]() |
![]() |
BLE-Stack APIs
3.00.01
|
PDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init(). More...
Data Fields | |
bool | applyCompression |
PDMCC26XX_CallbackFxn | callbackFxn |
uintptr_t | custom |
int32_t * | decimationFilter |
PDMCC26XX_FreeFxn | freeFxn |
PDMCC26XX_MallocFxn | mallocFxn |
PDMCC26XX_Gain | micGain |
bool | micPowerActiveHigh |
uint8_t | pdmBufferQueueDepth |
uint16_t | retBufSizeInBytes |
uint32_t | startupDelayWithClockInSamples |
bool | useDefaultFilter |
PDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init().
bool applyCompression |
Set to TRUE to apply compression. Setting it to FALSE allows user to apply own compression scheme.
PDMCC26XX_CallbackFxn callbackFxn |
Callback function pointer
uintptr_t custom |
Custom argument used by driver implementation
int32_t* decimationFilter |
Filter that is applied if PDMCC26XX_Params::useDefaultFilter is set to FALSE
PDMCC26XX_FreeFxn freeFxn |
Free function pointer
PDMCC26XX_MallocFxn mallocFxn |
Malloc function pointer
PDMCC26XX_Gain micGain |
Microphone gain
bool micPowerActiveHigh |
Set to TRUE if setting the GPIO high powers the microphone
uint16_t retBufSizeInBytes |
PDM buffer queue depth in number of blocks. We assume that we will be able to consume approximately one buffer per 2ms. This allows us to use the minium number of blocks (3) for the PDMCC26XX driver. If the application can not service the PDM task within the 2ms time window, increase this value to permit more latency in processing incoming PDM data at the cost of increased RAM useage.Size of returned buffers. It is not reccomended to make this value less than 64, the driver will not crash, but the equence numbers may become unaligned with the data in the buffer.
uint32_t startupDelayWithClockInSamples |
Some digital microphones have a startup delay. Set the number of samples to discard after powering the microphone starting to clock in data.
bool useDefaultFilter |
Set to TRUE to apply default filter. Set to FALSE to apply PDMCC26XX_Params::decimationFilter.