#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_ints.h"
#include "../inc/hw_nvic.h"
#include "../inc/hw_types.h"
#include "debug.h"
#include "interrupt.h"
Functions | |
static void | SysTickEnable (void) |
Enables the SysTick counter. More... | |
static void | SysTickDisable (void) |
Disables the SysTick counter. More... | |
static void | SysTickIntRegister (void(*pfnHandler)(void)) |
Registers an interrupt handler for the SysTick interrupt. More... | |
static void | SysTickIntUnregister (void) |
Unregisters the interrupt handler for the SysTick interrupt. More... | |
static void | SysTickIntEnable (void) |
Enables the SysTick interrupt. More... | |
static void | SysTickIntDisable (void) |
Disables the SysTick interrupt. More... | |
static void | SysTickPeriodSet (uint32_t ui32Period) |
Sets the period of the SysTick counter. More... | |
static uint32_t | SysTickPeriodGet (void) |
Gets the period of the SysTick counter. More... | |
static uint32_t | SysTickValueGet (void) |
Gets the current value of the SysTick counter. More... | |