#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_ints.h"
#include "../inc/hw_types.h"
#include "../inc/hw_nvic.h"
#include "debug.h"
#include "cpu.h"
Macros | |
#define | INT_PRIORITY_MASK 0x000000E0 |
#define | INT_PRI_LEVEL0 0x00000000 |
#define | INT_PRI_LEVEL1 0x00000020 |
#define | INT_PRI_LEVEL2 0x00000040 |
#define | INT_PRI_LEVEL3 0x00000060 |
#define | INT_PRI_LEVEL4 0x00000080 |
#define | INT_PRI_LEVEL5 0x000000A0 |
#define | INT_PRI_LEVEL6 0x000000C0 |
#define | INT_PRI_LEVEL7 0x000000E0 |
Functions | |
static bool | IntMasterEnable (void) |
Enables the processor interrupt. More... | |
static bool | IntMasterDisable (void) |
Disables the processor interrupt. More... | |
void | IntRegister (uint32_t ui32Interrupt, void(*pfnHandler)(void)) |
Registers a function to be called when an interrupt occurs. More... | |
void | IntUnregister (uint32_t ui32Interrupt) |
Unregisters the function to be called when an interrupt occurs. More... | |
void | IntPriorityGroupingSet (uint32_t ui32Bits) |
Sets the priority grouping of the interrupt controller. More... | |
uint32_t | IntPriorityGroupingGet (void) |
Gets the priority grouping of the interrupt controller. More... | |
void | IntPrioritySet (uint32_t ui32Interrupt, uint8_t ui8Priority) |
Sets the priority of an interrupt. More... | |
int32_t | IntPriorityGet (uint32_t ui32Interrupt) |
Gets the priority of an interrupt. More... | |
void | IntEnable (uint32_t ui32Interrupt) |
Enables an interrupt. More... | |
void | IntDisable (uint32_t ui32Interrupt) |
Disables an interrupt. More... | |
void | IntPendSet (uint32_t ui32Interrupt) |
Pends an interrupt. More... | |
bool | IntPendGet (uint32_t ui32Interrupt) |
Query whether an interrupt is pending. More... | |
void | IntPendClear (uint32_t ui32Interrupt) |
Unpends an interrupt. More... | |
static void | IntPriorityMaskSet (uint32_t ui32PriorityMask) |
Sets the priority masking level. More... | |
static uint32_t | IntPriorityMaskGet (void) |
Gets the priority masking level. More... | |