#include "interrupt.h"
Functions | |
static void | IntDefaultHandler (void) |
The default interrupt handler. More... | |
void | IntRegister (uint32_t ui32Interrupt, void(*pfnHandler)(void)) |
Registers a function to be called when an interrupt occurs. More... | |
void | IntUnregister (uint32_t ui32Interrupt) |
Unregisters the function to be called when an interrupt occurs. More... | |
void | IntPriorityGroupingSet (uint32_t ui32Bits) |
Sets the priority grouping of the interrupt controller. More... | |
uint32_t | IntPriorityGroupingGet (void) |
Gets the priority grouping of the interrupt controller. More... | |
void | IntPrioritySet (uint32_t ui32Interrupt, uint8_t ui8Priority) |
Sets the priority of an interrupt. More... | |
int32_t | IntPriorityGet (uint32_t ui32Interrupt) |
Gets the priority of an interrupt. More... | |
void | IntEnable (uint32_t ui32Interrupt) |
Enables an interrupt. More... | |
void | IntDisable (uint32_t ui32Interrupt) |
Disables an interrupt. More... | |
void | IntPendSet (uint32_t ui32Interrupt) |
Pends an interrupt. More... | |
bool | IntPendGet (uint32_t ui32Interrupt) |
Query whether an interrupt is pending. More... | |
void | IntPendClear (uint32_t ui32Interrupt) |
Unpends an interrupt. More... | |
Variables | |
static const uint32_t | g_pui32Priority [] |
static const uint32_t | g_pui32Regs [] |
void(* | g_pfnRAMVectors [NUM_INTERRUPTS])(void) |
|
static |
The default interrupt handler.
This is the default interrupt handler for all interrupts. It simply loops forever so that the system state is preserved for observation by a debugger. Since interrupts should be disabled before unregistering the corresponding handler, this should never be called.
Referenced by IntUnregister().
void(* g_pfnRAMVectors[NUM_INTERRUPTS])(void) |
Referenced by IntRegister(), and IntUnregister().
|
static |
This is a mapping between priority grouping encodings and the number of preemption priority bits.
Referenced by IntPriorityGroupingGet(), and IntPriorityGroupingSet().
|
static |
This is a mapping between interrupt number and the register that contains the priority encoding for that interrupt.
Referenced by IntPriorityGet(), and IntPrioritySet().