![]() |
![]() |
|
BLE-Stack APIs
3.00.00
|
Multi layer interface.
Go to the source code of this file.
Data Structures | |
| union | gapMultiRoleEvent_t |
| Multi GAPRole Event Structure. More... | |
| struct | gapRole_updateConnParams_t |
| Multi GAPRole Parameter Update Structure. More... | |
| struct | gapRolesCBs_t |
| Peripheral GAPRole Callback structure. More... | |
Macros | |
| #define | GAPROLE_ADV_CHANNEL_MAP 0x30C |
| Which channels to advertise on (Read/Write) More... | |
| #define | GAPROLE_ADV_DIRECT_ADDR 0x30B |
| Direct Advertisement Address (Read/Write) More... | |
| #define | GAPROLE_ADV_DIRECT_TYPE 0x30A |
| Direct Advertisement Type (Read/Write) More... | |
| #define | GAPROLE_ADV_EVENT_TYPE 0x309 |
| Advertisement Types (Read/Write) More... | |
| #define | GAPROLE_ADV_FILTER_POLICY 0x30D |
| Policy for filtering advertisements (Read/Write) More... | |
| #define | GAPROLE_ADV_NONCONN_ENABLED 0x31B |
| Enable / Disable non-connectable advertising (Read/Write) More... | |
| #define | GAPROLE_ADVERT_DATA 0x307 |
| Advertisement data (Read/Write) More... | |
| #define | GAPROLE_ADVERT_ENABLED 0x305 |
| Enable/Disable Connectable Advertising (Read/Write) More... | |
| #define | GAPROLE_ADVERT_OFF_TIME 0x306 |
| How long to remain off (in sec) after advertising stops before starting again (Read/Write) More... | |
| #define | GAPROLE_BD_ADDR 0x304 |
| Device Address read from the controller (Read-only) More... | |
| #define | GAPROLE_IRK 0x301 |
| Identity Resolving Key (Read/Write) Size is uint8_t[KEYLEN]. More... | |
| #define | GAPROLE_LINK_PARAM_UPDATE_ACCEPT 0 |
| Accept all parameter update requests. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_APP_DECIDES 2 |
| Notify app for it to decide. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_NUM_OPTIONS 3 |
| Number of options. Used for parameter checking. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_REJECT 1 |
| Reject all parameter update requests. | |
| #define | GAPROLE_MAX_CONN_INTERVAL 0x312 |
| Maximum connection interval (n * 1.25 ms) to use when performing param update (Read/Write) More... | |
| #define | GAPROLE_MAX_SCAN_RES 0x404 |
| Maximmum number of scan reports to store from GAPCentralRole_StartDiscovery (Read/Write) More... | |
| #define | GAPROLE_MIN_CONN_INTERVAL 0x311 |
| Minimum connection interval (n * 1.25 ms) to use when performing param update (Read/Write) More... | |
| #define | GAPROLE_NO_ACTION 0 |
| Take no action upon unsuccessful parameter updates. | |
| #define | GAPROLE_PROFILEROLE 0x300 |
| This parameter will return GAP Role type (Read-only) More... | |
| #define | GAPROLE_RESEND_PARAM_UPDATE 1 |
| Continue to resend request until successful update. | |
| #define | GAPROLE_SCAN_RSP_DATA 0x308 |
| Scan Response Data (Read/Write) More... | |
| #define | GAPROLE_SIGNCOUNTER 0x303 |
| Sign Counter (Read/Write) More... | |
| #define | GAPROLE_SLAVE_LATENCY 0x313 |
| Slave latency to use when performing param update (Read/Write) More... | |
| #define | GAPROLE_SRK 0x302 |
| Signature Resolving Key (Read/Write) More... | |
| #define | GAPROLE_TERMINATE_LINK 2 |
| Terminate link upon unsuccessful parameter updates. | |
| #define | GAPROLE_TIMEOUT_MULTIPLIER 0x314 |
| Supervision timeout (n x 10 ms) to use when performing param update (Read/Write) More... | |
Typedefs | |
| typedef void(* | paramUpdateAppDecision_t )(gapUpdateLinkParamReq_t *pReq, gapUpdateLinkParamReqReply_t *pRsp) |
| typedef uint8_t(* | passThroughToApp_t )(gapMultiRoleEvent_t *pEvent) |
| Multi Event Callback Function. More... | |
Functions | |
| bStatus_t | GAPRole_CancelDiscovery (void) |
| Cancel a device discovery scan. More... | |
| bStatus_t | gapRole_connUpdate (uint8_t handleFailure, gapRole_updateConnParams_t *pConnParams) |
| Send a connection parameter update to a connected device. More... | |
| bStatus_t | GAPRole_EstablishLink (uint8_t highDutyCycle, uint8_t whiteList, uint8_t addrTypePeer, uint8_t *peerAddr) |
| Establish a link to a peer device. More... | |
| bStatus_t | GAPRole_GetParameter (uint16_t param, void *pValue, uint8 connHandle) |
| Get a GAP Role parameter. More... | |
| bStatus_t | GAPRole_SetParameter (uint16_t param, uint8_t len, void *pValue, uint8 connHandle) |
| Set a GAP Role parameter. More... | |
| bStatus_t | GAPRole_StartDevice (gapRolesCBs_t *pAppCallbacks, uint8_t *numConns) |
| Initialize the GAP layer. More... | |
| bStatus_t | GAPRole_StartDiscovery (uint8_t mode, uint8_t activeScan, uint8_t whiteList) |
| Start a device discovery scan. More... | |
| bStatus_t | GAPRole_TerminateConnection (uint16_t connHandle) |
| Terminates the existing connection. More... | |