![]() |
![]() |
|
BLE-Stack APIs
3.00.00
|
Data Structures | |
| struct | gapRolesCBs_t |
| Peripheral GAPRole Callback structure. More... | |
Typedefs | |
| typedef void(* | paramUpdateAppDecision_t )(gapUpdateLinkParamReq_t *pReq, gapUpdateLinkParamReqReply_t *pRsp) |
| typedef uint8_t(* | passThroughToApp_t )(gapMultiRoleEvent_t *pEvent) |
| Multi Event Callback Function. More... | |
These are functions whose pointers are passed from the application to the GAPRole so that the GAPRole can send events to the application
| typedef uint8_t(* passThroughToApp_t)(gapMultiRoleEvent_t *pEvent) |
Multi Event Callback Function.
This callback is used by the Multi GAPRole to forward GAP_Events to the application.
If the message is successfully queued to the application for later processing, FALSE is returned because the application deallocates it later. Consider the following state change event from multi_role as an example of this:
If the message is not successfully queued to the application, TRUE is returned so that the GAPRole can deallocate the message. If the heap has enough room, the message must always be successfully enqueued.
| pEvent | Pointer to event structure |