![]() |
![]() |
BLE-Stack APIs
3.00.00
|
Data Structures | |
struct | ugBcastCBs_t |
Set of Broadcaster callbacks - must be setup by the application. More... | |
Typedefs | |
typedef void(* | ugbAdvDoneCb_t )(bStatus_t status) |
Callback of when an Advertising Event has just been done. More... | |
typedef void(* | ugbAdvPrepareCb_t )(void) |
Callback of when the next Adverting Event is about to start. More... | |
typedef void(* | ugbStateChangeCb_t )(ugBcastState_t state) |
Callback of when the Broadcaster's state changes. More... | |
Variables | |
PACKED_TYPEDEF_STRUCT | |
Message payload for the event UGB_EVT_STATE_CHANGE. More... | |
ugbMsgAdvPostprocess_t | |
ugbMsgStateChange_t | |
typedef void(* ugbAdvDoneCb_t)(bStatus_t status) |
Callback of when an Advertising Event has just been done.
status | status of advertising done event |
typedef void(* ugbAdvPrepareCb_t)(void) |
Callback of when the next Adverting Event is about to start.
The application can use this to update the payload if necessary
typedef void(* ugbStateChangeCb_t)(ugBcastState_t state) |
Callback of when the Broadcaster's state changes.
state | uGAP Broadcaster States |
PACKED_TYPEDEF_STRUCT |
Message payload for the event UGB_EVT_STATE_CHANGE.
Message payload for the event UGB_EVT_ADV_POSTPROCESS.