Dynamic Power Control¶
Description¶
Change power mode dynamically from task code
This resource allows the Sensor Controller to switch between the active and low-power power modes within task code blocks.
This can be used instead of, or in combination with, static configuration in the Power and Clock Settings Panel in Sensor Controller Studio.
The table below shows clock rate and availability in the different power modes for each task resource:
| Task Resource | Clock Rate | Active Mode | Low-Power Mode | Standby Mode |
| Accumulator Based Math | Same as Sensor Controller | Available | Available | |
| ADC | Same as AUX bus | Available | ||
| COMPA | Analog / asynchronous | Available | Available | Available |
| COMPB | 32 kHz | Available | Available* | Available |
| Delay Insertion | 2 MHz | Available | Available | |
| Digital GPIO | Same as Sensor Controller | Available | Available | |
| ISRC | Analog / asynchronous | Available | ||
| Reference DAC | Automatically adapted | Available | Available | Available |
| Pulse Counter | Asynchronous | Available | Available | Available |
| I2C Master | Same as Sensor Controller | Available | ||
| SPI Chip Select | Same as Sensor Controller | Available | Available | |
| SPI Data Transfer | Same as Sensor Controller | Available | Available | |
| TDC | Same as AUX bus | Available | ||
| Timer 0 | Same as Sensor Controller | Available | Available | |
| Timer 1 | Same as Sensor Controller | Available | Available | |
| Timer 2 | 24 MHz, 2 MHz or 32 kHz | Available | Available | Available |
| LCD Controller | Same as Sensor Controller | Available | Available | Between updates |
| UART Emulator | Based on Timer 0 | Available | ||
| COMPA Event Trigger | Asynchronous | Wake-up trigger | ||
| COMPB Event Trigger | Asynchronous (32 kHz) | Wake-up trigger | ||
| GPIO Event Trigger | Asynchronous | Wake-up trigger | ||
| System Event Trigger | Asynchronous | Wake-up trigger | ||
| Timer 0 Event Trigger | 4 kHz signal from RTC | Wake-up trigger | ||
| Timer 1 Event Trigger | 4 kHz signal from RTC | Wake-up trigger | ||
| Timer 2 Event Trigger | Based on Timer 2 | Wake-up trigger |
* The procedures that enable/disable COMPB can only be called when the Sensor Controller (or System CPU) is in active mode.
Examples¶
Entering Active Mode Only During Some Wakeups¶
// The task code block starts in low-power mode
// If some condition is met ...
if (...) {
// Enter active mode
pwrRequestAndWaitForActiveMode();
// Get one ADC sample
adcEnableSync(ADC_REF_FIXED, ADC_SAMPLE_TIME_2P7_US, ADC_TRIGGER_MANUAL);
adcGenManualTrigger();
adcReadFifo(output.adcValue);
adcDisable();
// Return to low-power mode
pwrRequestAndWaitForLowPowerMode();
}
// The task code block ends in low-power mode, so unless changed by the static configuration,
// the Sensor Controller will start in low-power mode at the next wake-up
Procedures Overview¶
| Name | Brief description |
pwrRequestActiveMode() |
Requests change to the active power mode. More … |
pwrRequestAndWaitForActiveMode() |
Requests change to the active power mode, and waits for it to take effect. More … |
pwrRequestAndWaitForLowPowerMode() |
Requests change to the low-power power mode, and waits for it to take effect. More … |
pwrRequestLowPowerMode() |
Requests change to the low-power power mode. More … |
pwrWaitForActiveMode() |
Waits for change to the active power mode to take effect. More … |
pwrWaitForLowPowerMode() |
Waits for change to the low-power power mode to take effect. More … |
Constants¶
None.
Global Variables¶
None.
Procedures¶
pwrRequestActiveMode¶
Prototype: pwrRequestActiveMode()
Requests change to the active power mode.
This request must be followed by a call to pwrWaitForActiveMode() before:
- Calling any other other dynamic power control procedures
- The end of the task code block
pwrRequestAndWaitForActiveMode¶
Prototype: pwrRequestAndWaitForActiveMode()
Requests change to the active power mode, and waits for it to take effect.
pwrRequestAndWaitForLowPowerMode¶
Prototype: pwrRequestAndWaitForLowPowerMode()
Requests change to the low-power power mode, and waits for it to take effect.
pwrRequestLowPowerMode¶
Prototype: pwrRequestLowPowerMode()
Requests change to the low-power power mode.
This request must be followed by a call to pwrWaitForLowPowerMode() before:
- Calling any other other dynamic power control procedures
- The end of the task code block
pwrWaitForActiveMode¶
Prototype: pwrWaitForActiveMode()
Waits for change to the active power mode to take effect.
Note: Deadlock will occur if this procedure is called without a prior call to pwrRequestActiveMode() .
pwrWaitForLowPowerMode¶
Prototype: pwrWaitForLowPowerMode()
Waits for change to the low-power power mode to take effect.
Note: Deadlock will occur if this procedure is called without a prior call to pwrRequestLowPowerMode() .