Using the Memory BrowserΒΆ
Both IAR and CCS are able to show a representation of the memory on the device. In CCS, you can index by address or by symbol name. As an example, consider the stack that was overrun in Figure 116.:
Simple Peripheral Task’s stack. Note BE watermark |
GAPRole Task’s stack. Note it’s completely filled. |
|
|
The solution in this case would be to increase the stack size for the failing task
and see what the stack peak really is. The stackPeak reported is relying on
how many watermark bytes are overwritten, so it can’t know how much the overrun
amounts to.
Because stacks are utilized from higher addresses towards lower addressed (upwards in the picture), stacks that overrun will tend to overwrite data at locations immediately before the stack.