![]() |
![]() |
SPI Global configuration. More...
#include <SPI.h>
Data Fields | |
| SPI_FxnTable const * | fxnTablePtr |
| void * | object |
| void const * | hwAttrs |
SPI Global configuration.
The SPI_Config structure contains a set of pointers used to characterize the SPI driver implementation.
This structure needs to be defined before calling SPI_init() and it must not be changed thereafter.
| SPI_FxnTable const* SPI_Config_::fxnTablePtr |
Pointer to a table of driver-specific implementations of SPI APIs
| void* SPI_Config_::object |
Pointer to a driver specific data object
| void const* SPI_Config_::hwAttrs |
Pointer to a driver specific hardware attributes structure