423 #ifndef ti_drivers_SPI__include   424 #define ti_drivers_SPI__include   451 #define SPI_CMD_RESERVED           (32)   465 #define SPI_STATUS_RESERVED        (-32)   480 #define SPI_STATUS_SUCCESS         (0)   488 #define SPI_STATUS_ERROR           (-1)   497 #define SPI_STATUS_UNDEFINEDCMD    (-2)   517 #define SPI_WAIT_FOREVER           (~(0U))   726 extern void SPI_close(SPI_Handle handle);
   765 extern int_fast16_t 
SPI_control(SPI_Handle handle, uint_fast16_t cmd,
 void SPI_init(void)
This function initializes the SPI module. 
SPI_Mode mode
Definition: SPI.h:624
enum SPI_Status_ SPI_Status
Status codes that are set by the SPI driver. 
void * rxBuf
Definition: SPI.h:547
SPI_FrameFormat_
Definitions for various SPI data frame formats. 
Definition: SPI.h:576
SPI_CloseFxn closeFxn
Definition: SPI.h:677
void const  * hwAttrs
Definition: SPI.h:714
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK. 
Definition: SPI.h:561
enum SPI_Mode_ SPI_Mode
Definitions for various SPI modes of operation. 
SPI_InitFxn initFxn
Definition: SPI.h:683
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:543
SPI_ControlFxn controlFxn
Definition: SPI.h:680
SPI_TransferFxn transferFxn
Definition: SPI.h:689
uint32_t bitRate
Definition: SPI.h:625
uint32_t dataSize
Definition: SPI.h:626
void SPI_transferCancel(SPI_Handle handle)
Function to cancel SPI transactions. 
SPI_FxnTable const  * fxnTablePtr
Definition: SPI.h:708
void SPI_Params_init(SPI_Params *params)
Function to initialize the SPI_Params struct to its defaults. 
bool(* SPI_TransferFxn)(SPI_Handle handle, SPI_Transaction *transaction)
A function pointer to a driver specific implementation of SPI_transfer(). 
Definition: SPI.h:661
size_t count
Definition: SPI.h:545
struct SPI_Transaction_ SPI_Transaction
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
SPI_TransferCancelFxn transferCancelFxn
Definition: SPI.h:692
void(* SPI_TransferCancelFxn)(SPI_Handle handle)
A function pointer to a driver specific implementation of SPI_transferCancel(). 
Definition: SPI.h:668
SPI_Status_
Status codes that are set by the SPI driver. 
Definition: SPI.h:527
uint32_t transferTimeout
Definition: SPI.h:621
enum SPI_TransferMode_ SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
void(* SPI_CloseFxn)(SPI_Handle handle)
A function pointer to a driver specific implementation of SPI_close(). 
Definition: SPI.h:636
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:675
SPI Parameters. 
Definition: SPI.h:619
SPI_Status status
Definition: SPI.h:551
int_fast16_t SPI_control(SPI_Handle handle, uint_fast16_t cmd, void *controlArg)
Function performs implementation specific features on a given SPI_Handle. 
struct SPI_Params_ SPI_Params
SPI Parameters. 
void * txBuf
Definition: SPI.h:546
bool SPI_transfer(SPI_Handle handle, SPI_Transaction *transaction)
Function to perform SPI transactions. 
struct SPI_Config_ SPI_Config
SPI Global configuration. 
SPI Global configuration. 
Definition: SPI.h:706
SPI_OpenFxn openFxn
Definition: SPI.h:686
SPI_Mode_
Definitions for various SPI modes of operation. 
Definition: SPI.h:567
void * custom
Definition: SPI.h:628
enum SPI_FrameFormat_ SPI_FrameFormat
Definitions for various SPI data frame formats. 
void SPI_close(SPI_Handle handle)
Function to close a SPI peripheral specified by the SPI handle. 
SPI_TransferMode transferMode
Definition: SPI.h:620
struct SPI_Config_ * SPI_Handle
A handle that is returned from a SPI_open() call. 
Definition: SPI.h:522
SPI_Handle SPI_open(uint_least8_t index, SPI_Params *params)
This function opens a given SPI peripheral. 
void * arg
Definition: SPI.h:548
int_fast16_t(* SPI_ControlFxn)(SPI_Handle handle, uint_fast16_t cmd, void *arg)
A function pointer to a driver specific implementation of SPI_control(). 
Definition: SPI.h:642
void(* SPI_InitFxn)(SPI_Handle handle)
A function pointer to a driver specific implementation of SPI_init(). 
Definition: SPI.h:649
SPI_Handle(* SPI_OpenFxn)(SPI_Handle handle, SPI_Params *params)
A function pointer to a driver specific implementation of SPI_open(). 
Definition: SPI.h:655
SPI_FrameFormat frameFormat
Definition: SPI.h:627
struct SPI_FxnTable_ SPI_FxnTable
The definition of a SPI function table that contains the required set of functions to control a speci...
SPI_CallbackFxn transferCallbackFxn
Definition: SPI.h:623
SPI_TransferMode_
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:597
void * object
Definition: SPI.h:711