Driver for the Texas Instruments TMP007 infra-red thermopile sensor.
Driver include
This header file should be included in an application as follows:
#include "stdint.h"
#include "stdbool.h"
Go to the source code of this file.
§ SensorTmp007_init()
| bool SensorTmp007_init |
( |
void |
| ) |
|
Initialize the temperature sensor driver.
- Returns
- true if success
§ SensorTmp007_enable()
| bool SensorTmp007_enable |
( |
bool |
enable | ) |
|
Enable/disable measurement cycle.
- Parameters
-
| enable | - flag to turn the sensor on/off |
- Returns
- true if success
§ SensorTmp007_test()
| bool SensorTmp007_test |
( |
void |
| ) |
|
Run a sensor self-test.
- Returns
- true if passed
§ SensorTmp007_read()
| bool SensorTmp007_read |
( |
uint16_t * |
rawLocalTemp, |
|
|
uint16_t * |
rawObjTemp |
|
) |
| |
Read the sensor temperature registers.
- Parameters
-
| rawLocalTemp | - local temperature in 16 bit format |
| rawObjTemp | - object temperature in 16 bit format |
- Returns
- true if valid data
§ SensorTmp007_convert()
| void SensorTmp007_convert |
( |
uint16_t |
rawLocalTemp, |
|
|
uint16_t |
rawObjTemp, |
|
|
float * |
tObj, |
|
|
float * |
tLocal |
|
) |
| |
Convert raw data to temperature [C].
- Parameters
-
| rawLocalTemp | - raw temperature from sensor |
| rawObjTemp | - raw temperature from sensor |
| tObj | - converted object temperature |
| tLocal | - converted die temperature |