44 #ifndef SENSOR_TMP007_H 45 #define SENSOR_TMP007_H 116 void SensorTmp007_convert(uint16_t rawLocalTemp, uint16_t rawObjTemp,
float *tObj,
float *tLocal);
bool SensorTmp007_test(void)
Run a sensor self-test.
bool SensorTmp007_read(uint16_t *rawLocalTemp, uint16_t *rawObjTemp)
Read the sensor temperature registers.
void SensorTmp007_convert(uint16_t rawLocalTemp, uint16_t rawObjTemp, float *tObj, float *tLocal)
Convert raw data to temperature [C].
bool SensorTmp007_enable(bool enable)
Enable/disable measurement cycle.
bool SensorTmp007_init(void)
Initialize the temperature sensor driver.