![]() |
![]() |
Driver for Texas Instruments HCD1000 humidity sensor.
This header file should be included in an application as follows:
#include "stdbool.h"#include "stdint.h"Go to the source code of this file.
Functions | |
| bool | SensorHdc1000_init (void) |
| Initialize the sensor. More... | |
| void | SensorHdc1000_start (void) |
| Start measurement. More... | |
| bool | SensorHdc1000_read (uint16_t *pRawTemp, uint16_t *pRawHum) |
| Read humidity sensor data. More... | |
| void | SensorHdc1000_convert (uint16_t rawTemp, uint16_t rawHum, float *pTemp, float *pHum) |
| Convert raw data to temperature and humidity. More... | |
| bool | SensorHdc1000_test (void) |
| Humidity sensor self test. More... | |
| bool SensorHdc1000_init | ( | void | ) |
Initialize the sensor.
Configure reading of temperature and humidity as one read cycle, and use 14 bit data size.
| void SensorHdc1000_start | ( | void | ) |
Start measurement.
| bool SensorHdc1000_read | ( | uint16_t * | pRawTemp, |
| uint16_t * | pRawHum | ||
| ) |
Read humidity sensor data.
| pRawTemp | - buffer for raw temperature |
| pRawHum | - buffer for raw humidity |
| void SensorHdc1000_convert | ( | uint16_t | rawTemp, |
| uint16_t | rawHum, | ||
| float * | pTemp, | ||
| float * | pHum | ||
| ) |
Convert raw data to temperature and humidity.
Calculate relative humidity and temperature based on provided raw data.
| rawTemp | - raw temperature value |
| rawHum | - raw humidity value |
| pTemp | - converted temperature [deg. C] |
| pHum | - converted humidity |
| bool SensorHdc1000_test | ( | void | ) |
Humidity sensor self test.