44 #ifndef SENSOR_HDC1000_H 45 #define SENSOR_HDC1000_H 109 float *pTemp,
float *pHum);
void SensorHdc1000_start(void)
Start measurement.
bool SensorHdc1000_test(void)
Humidity sensor self test.
bool SensorHdc1000_init(void)
Initialize the sensor.
bool SensorHdc1000_read(uint16_t *pRawTemp, uint16_t *pRawHum)
Read humidity sensor data.
void SensorHdc1000_convert(uint16_t rawTemp, uint16_t rawHum, float *pTemp, float *pHum)
Convert raw data to temperature and humidity.