TIOVX User Guide
|
Internal private implementation of object descriptor. More...
Go to the source code of this file.
Data Structures | |
struct | tivx_obj_desc_cmd_t |
Command object descriptor. More... | |
struct | tivx_obj_desc_kernel_name_t |
Command object descriptor. More... | |
struct | tivx_obj_desc_queue_blocked_nodes_t |
Data structure to get information about node blocked on this object descriptor to be ready. More... | |
struct | tivx_obj_desc_queue_t |
Object descriptor queue. More... | |
struct | tivx_obj_desc_data_ref_q_t |
Data reference queue. More... | |
struct | tivx_obj_desc_graph_t |
Graph object descriptor as placed in shared memory. More... | |
struct | tivx_obj_desc_super_node_edge_t |
Super Node edge object descriptor. More... | |
struct | tivx_obj_desc_super_node_t |
Super Node object descriptor. More... | |
union | tivx_obj_desc_shm_entry_t |
Object Descriptor Shared memory entry which can hold any of the supported object descriptor types. More... | |
struct | tivx_obj_desc_table_info_t |
Data structure to hold info about object descriptor table. More... | |
Macros | |
#define | TIVX_OBJ_DESC_QUEUE_MAX_BLOCKED_NODES (8u) |
Max nodes that can be blocked on object descriptor queue not empty. | |
#define | TIVX_OBJ_DESC_QUEUE_MAX_DEPTH (32u) |
Max elements in a object descriptor queue. | |
#define | TIVX_CMD_MAX_OBJ_DESCS (16u) |
Max object descriptors than be parameters in a command object. | |
#define | TIVX_CMD_FLAG_SEND_ACK (0x00000001u) |
Flag to indicate if command receiver needs to ACK this command. | |
#define | TIVX_CMD_FLAG_IS_ACK (0x00000002u) |
Flag to indicate if this is a command or ACK for a command. | |
#define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_IS_ENABLE_REF_CONSUMED_EVENT (0x00000001u) |
Data Ref Q flag to determine if ref consumed event should be sent. | |
#define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_IS_REF_ACQUIRED (0x00000002u) |
Data Ref Q flag to determine if ref is acquired for this data ref q. | |
#define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_IS_IN_DELAY (0x00000004u) |
Data Ref Q flag to determine if this obj desc is part of some delay. | |
#define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_DELAY_SLOT_AUTO_AGE (0x00000008u) |
Data Ref Q flag to determine if delay slot to which this obj desc belongs should be auto aged. More... | |
#define | TIVX_OBJ_DESC_ID_SHIFT (12u) |
Shift for storing Object Descriptor id in 32bit variable. | |
#define | TIVX_OBJ_DESC_ID_MASK (0x0000FFFFu) |
Mask for storing Object Descriptor id in 32bit variable. | |
#define | TIVX_OBJ_DESC_BIDIR_FLAG (0x10000U) |
Mask for storing Object Descriptor id in 32bit variable. | |
Functions | |
tivx_obj_desc_t * | ownObjDescAlloc (vx_enum ref_type, vx_reference ref) |
Allocate a Object descriptor. More... | |
vx_status | ownObjDescFree (tivx_obj_desc_t **obj_desc) |
Free a previously allocated object descriptor. More... | |
vx_status | ownObjDescSend (uint32_t dst_target_id, uint16_t obj_desc_id) |
Sends a object descriptor to specified target. More... | |
tivx_obj_desc_t * | ownObjDescGet (uint16_t obj_desc_id) |
Get obj descriptor corresponding to the object descriptor ID. More... | |
vx_bool | ownObjDescIsValidType (const tivx_obj_desc_t *obj_desc, tivx_obj_desc_type_e obj_type) |
Checks if object desc pointer is valid and it is of required type. | |
void | ownObjDescInit (void) |
Init object descriptor module. | |
uint16_t | ownReferenceGetObjDescId (vx_reference ref) |
Function to get the descriptor object from the given reference. | |
Internal private implementation of object descriptor.
Definition in file tivx_obj_desc_priv.h.