TIOVX User Guide
|
Interface to Event Queue APIs. More...
Go to the source code of this file.
Data Structures | |
struct | tivx_event_queue_elem_t |
Element inserted into event queue. More... | |
struct | tivx_event_queue_t |
Event queue object. More... | |
Enumerations | |
enum | tivx_queue_type_e { TIVX_EVENT_GRAPH_QUEUE = VX_ATTRIBUTE_BASE(VX_ID_TI, (int32_t)0) + 0x1, TIVX_EVENT_CONTEXT_QUEUE = VX_ATTRIBUTE_BASE(VX_ID_TI, (int32_t)0) + 0x2 } |
Type of event that can be generated during system execution. More... | |
Functions | |
vx_status | ownEventQueueCreate (tivx_event_queue_t *event_q) |
Create a event queue. More... | |
vx_status | ownEventQueueDelete (tivx_event_queue_t *event_q) |
Delete a event queue. More... | |
vx_status | ownEventQueueAddEvent (tivx_event_queue_t *event_q, vx_enum event_id, uint64_t timestamp, uint32_t app_value, uintptr_t param1, uintptr_t param2, uintptr_t param3) |
Add event to event queue. More... | |
void | ownEventQueueEnableEvents (tivx_event_queue_t *event_q, vx_bool enable) |
Enable an event queue. | |
vx_status | vxWaitEventQueue (tivx_event_queue_t *event_q, vx_event_t *event, vx_bool do_not_block) |
Generic wait event queue API. | |
vx_status | ownRegisterEvent (vx_reference ref, enum tivx_queue_type_e queue_type, enum vx_event_type_e event_type, vx_uint32 param, vx_uint32 app_value) |
Registers an event to a given event queue. | |
Interface to Event Queue APIs.
Event Queue can be used to collect framework generated events into a queue. When user calls vxWaitEvent the event is returned to the user in a first-in first out manner
Definition in file tivx_event_queue.h.
enum tivx_queue_type_e |
Type of event that can be generated during system execution.
Definition at line 131 of file tivx_event_queue.h.
vx_status ownEventQueueCreate | ( | tivx_event_queue_t * | event_q | ) |
Create a event queue.
vx_status ownEventQueueDelete | ( | tivx_event_queue_t * | event_q | ) |
Delete a event queue.
vx_status ownEventQueueAddEvent | ( | tivx_event_queue_t * | event_q, |
vx_enum | event_id, | ||
uint64_t | timestamp, | ||
uint32_t | app_value, | ||
uintptr_t | param1, | ||
uintptr_t | param2, | ||
uintptr_t | param3 | ||
) |
Add event to event queue.
When events are disabled, event is not added to the event_q