TIOVX User Guide
hwa_vpac_ldc.h
Go to the documentation of this file.
1 /*
2  *
3  * Copyright (c) 2019-2021 Texas Instruments Incorporated
4  *
5  * All rights reserved not granted herein.
6  *
7  * Limited License.
8  *
9  * Texas Instruments Incorporated grants a world-wide, royalty-free, non-exclusive
10  * license under copyrights and patents it now or hereafter owns or controls to make,
11  * have made, use, import, offer to sell and sell ("Utilize") this software subject to the
12  * terms herein. With respect to the foregoing patent license, such license is granted
13  * solely to the extent that any such patent is necessary to Utilize the software alone.
14  * The patent license shall not apply to any combinations which include this software,
15  * other than combinations with devices manufactured by or for TI ("TI Devices").
16  * No hardware patent is licensed hereunder.
17  *
18  * Redistributions must preserve existing copyright notices and reproduce this license
19  * (including the above copyright notice and the disclaimer and (if applicable) source
20  * code license limitations below) in the documentation and/or other materials provided
21  * with the distribution
22  *
23  * Redistribution and use in binary form, without modification, are permitted provided
24  * that the following conditions are met:
25  *
26  * * No reverse engineering, decompilation, or disassembly of this software is
27  * permitted with respect to any software provided in binary form.
28  *
29  * * any redistribution and use are licensed by TI for use only with TI Devices.
30  *
31  * * Nothing shall obligate TI to provide you with source code for the software
32  * licensed and provided to you in object code.
33  *
34  * If software source code is provided to you, modification and redistribution of the
35  * source code are permitted provided that the following conditions are met:
36  *
37  * * any redistribution and use of the source code, including any resulting derivative
38  * works, are licensed by TI for use only with TI Devices.
39  *
40  * * any redistribution and use of any object code compiled from the source code
41  * and any resulting derivative works, are licensed by TI for use only with TI Devices.
42  *
43  * Neither the name of Texas Instruments Incorporated nor the names of its suppliers
44  *
45  * may be used to endorse or promote products derived from this software without
46  * specific prior written permission.
47  *
48  * DISCLAIMER.
49  *
50  * THIS SOFTWARE IS PROVIDED BY TI AND TI'S LICENSORS "AS IS" AND ANY EXPRESS
51  * OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
52  * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
53  * IN NO EVENT SHALL TI AND TI'S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT,
54  * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
55  * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
56  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY
57  * OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE
58  * OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED
59  * OF THE POSSIBILITY OF SUCH DAMAGE.
60  *
61  */
62 
63 #ifndef HWA_VPAC_LDC_H_
64 #define HWA_VPAC_LDC_H_
65 
66 #include <VX/vx.h>
67 #include <VX/vx_kernels.h>
68 
69 #ifdef __cplusplus
70 extern "C" {
71 #endif
72 
81 #define TIVX_KERNEL_VPAC_LDC_NAME "com.ti.hwa.vpac_ldc"
82 
86 #define TIVX_KERNEL_VPAC_LDC2_NAME "com.ti.hwa.vpac_ldc2"
87 
88 
89 /*********************************
90  * VPAC_LDC Control Commands
91  *********************************/
92 
99 #define TIVX_VPAC_LDC_CMD_SET_READ_BW_LIMIT_PARAMS (0x10000000u)
100 
111 #define TIVX_VPAC_LDC_CMD_SET_BIT_DEPTH_CONV_LUT_PARAMS (0x10000001u)
112 
127 #define TIVX_VPAC_LDC_CMD_GET_ERR_STATUS (0x10000002u)
128 
140 #define TIVX_VPAC_LDC_CMD_SET_LDC_PARAMS (0x10000003u)
141 
145 #define TIVX_VPAC_LDC_CMD_GET_PSA_STATUS (0x10000004u)
146 
162 #define TIVX_VPAC_LDC_CMD_SET_LDC_DCC_PARAMS (0x30000000u)
163 
164 #if defined (LDRA_COVERAGE)
165 
168 #define TIVX_VPAC_CMD_GET_COVERAGE_START (0x10000005u)
169 #endif /* LDRA_COVERAGE */
170 
174 #define TIVX_VPAC_LDC_CMD_ENABLE_ERROR_EVENTS (0x10000006u)
175 
181 #define TIVX_VPAC_LDC_CMD_ENABLE_VPAC_SAFETY_MECHANISM (0x10000007u)
182 
183 /*********************************
184  * VPAC_LDC Defines
185  *********************************/
186 
194 #define TIVX_VPAC_LDC_ALIGN_LSB (0U)
195 
196 #define TIVX_VPAC_LDC_ALIGN_MSB (1U)
197 
199 #define TIVX_VPAC_LDC_INTERPOLATION_BICUBIC (0U)
200 
201 #define TIVX_VPAC_LDC_INTERPOLATION_BILINEAR (1U)
202 
204 #define TIVX_VPAC_LDC_MODE_LUMA_ONLY (0U)
205 
206 #define TIVX_VPAC_LDC_MODE_CHROMA_ONLY (1U)
207 
208 #if defined(VPAC3) || defined(VPAC3L)
209 
210 #define TIVX_VPAC_LDC_CONTINUOUS_MODE_ONE_SHOT (0U)
211 
212 #define TIVX_VPAC_LDC_CONTINUOUS_MODE_CONTINUOUS (1U)
213 #endif
214 
222 #define TIVX_VPAC_LDC_CALC_MESH_LINE_OFFSET(width, subsample_factor) \
223  ((((((width)/(subsample_factor))+1) + 15U) & ~15U) * (4U))
224 
226 #define TIVX_VPAC_LDC_BIT_DEPTH_CONV_LUT_SIZE (513u)
227 
230 #define TIVX_VPAC_LDC_PIX_BLK_OUTOFBOUND_ERR_STATUS (0x1u)
231 
233 #define TIVX_VPAC_LDC_MESH_BLK_OUTOFBOUND_ERR_STATUS (0x2u)
234 
235 #define TIVX_VPAC_LDC_PIX_MEM_OVF_ERR_STATUS (0x4u)
236 
237 #define TIVX_VPAC_LDC_MESH_MEM_OVF_ERR_STATUS (0x8u)
238 
239 #define TIVX_VPAC_LDC_PIX_FRM_OUTOFBOUND_ERR_STATUS (0x10u)
240 
241 #define TIVX_VPAC_LDC_SZ_OVF_ERR_STATUS (0x20u)
242 
243 #define TIVX_VPAC_LDC_SL2_WR_ERR_STATUS (0x80u)
244 
245 #define TIVX_VPAC_LDC_RD_ERR_STATUS (0x100u)
246 
247 #define TIVX_VPAC_LDC_WDTIMER_ERR (0x40000000U)
248 
249 #define TIVX_VPAC_LDC_ALL_ERR_EVENTS ( \
250  TIVX_VPAC_LDC_PIX_BLK_OUTOFBOUND_ERR_STATUS | \
251  TIVX_VPAC_LDC_MESH_BLK_OUTOFBOUND_ERR_STATUS | \
252  TIVX_VPAC_LDC_PIX_MEM_OVF_ERR_STATUS | \
253  TIVX_VPAC_LDC_MESH_MEM_OVF_ERR_STATUS | \
254  TIVX_VPAC_LDC_PIX_FRM_OUTOFBOUND_ERR_STATUS | \
255  TIVX_VPAC_LDC_SZ_OVF_ERR_STATUS | \
256  TIVX_VPAC_LDC_SL2_WR_ERR_STATUS | \
257  TIVX_VPAC_LDC_RD_ERR_STATUS | \
258  TIVX_VPAC_LDC_WDTIMER_ERR \
259 )
260 
262 #define TIVX_VPAC_LDC_WDTIMER_DISABLE (0u)
263 
264 #define TIVX_VPAC_LDC_WDTIMER_ENABLE (1u)
265 
266 #define TIVX_VPAC_LDC_WDTIMER_64K_CYCLES (0u)
267 
268 #define TIVX_VPAC_LDC_WDTIMER_128K_CYCLES (1u)
269 
270 #define TIVX_VPAC_LDC_SET_PARAMS_WARP_MATRIX_IDX (0u)
271 
272 #define TIVX_VPAC_LDC_DEF_BLOCK_WIDTH (64u)
273 #define TIVX_VPAC_LDC_DEF_BLOCK_HEIGHT (64u)
274 #define TIVX_VPAC_LDC_DEF_PIXEL_PAD (0u)
275 
276 /* Maximum number of outputs supported in LDC */
277 #define TIVX_VPAC_LDC_MAX_OUTPUT (2u)
278 
279 /*********************************
280  * VPAC_LDC STRUCTURES
281  *********************************/
282 
289 typedef struct {
291  uint32_t enable;
293  uint32_t out_block_width;
297  uint32_t pixel_pad;
299 
306 typedef struct {
308  uint32_t reg_width[3];
310  uint32_t reg_height[3];
314 
321 typedef struct {
322 
327 
332 
339 typedef struct {
345 
348  uint32_t init_x;
351  uint32_t init_y;
352 
364  uint32_t yc_mode;
365 
367  uint32_t dcc_camera_id;
368  #if defined(VPAC3) || defined(VPAC3L)
369 
374  uint32_t in_img0_yc_mode;
378  uint32_t in_img1_yc_mode;
379  #endif
380 
412  uint32_t enable_psa;
413 #if defined(VPAC3) || defined(VPAC3L)
414 
421  uint32_t continuous_mode;
422 #endif
423 
431 
432 
441 typedef struct {
457  uint32_t tag_count;
469 
479 typedef struct {
483  uint32_t input_bits;
487  uint32_t output_bits;
492 
498 typedef struct {
504  uint32_t psa_values[TIVX_VPAC_LDC_MAX_OUTPUT];
505 
511  uint64_t timestamp;
513 
537 typedef struct {
538 
539  /* This flag will be used to control the reconfig of Registers safety mechanism feature */
540  uint32_t enable_reconfig_and_reinit_Reg;
541 
542  /* This flag will be used to control the status register validation safety mechanism feature */
543  uint32_t enable_status_reg_validation;
544 
545  /* This flag will be used to enable configuration register readback validation safety mechanism feature */
546  uint32_t enable_readback_config_registers;
547 
549 
555 #define TIVX_VPAC_LDC_REG_VALIDATE_FAILURE_STATUS_REG ((int32_t) 0x80000001U)
556 
561 #define TIVX_VPAC_LDC_REG_VALIDATE_FAILURE_CONFIG_REG ((int32_t) 0x80000002U)
562 
570 typedef struct {
585  uint32_t err_intr_stat;
588  uint64_t timestamp;
590 
591 /*********************************
592  * Function Prototypes
593  *********************************/
594 
600 
601 
607 
608 
702 VX_API_ENTRY vx_node VX_API_CALL tivxVpacLdcNode(vx_graph graph,
703  vx_user_data_object configuration,
704  vx_matrix warp_matrix,
705  vx_user_data_object region_prms,
706  vx_user_data_object mesh_prms,
707  vx_image mesh_img,
708  vx_user_data_object dcc_db,
709  vx_image in_img,
710  vx_image out0_img,
711  vx_image out1_img);
826 VX_API_ENTRY vx_node VX_API_CALL tivxVpacLdcNode2(vx_graph graph,
827  vx_user_data_object configuration,
828  vx_matrix warp_matrix,
829  vx_user_data_object region_prms,
830  vx_user_data_object mesh_prms,
831  vx_image mesh_img,
832  vx_user_data_object dcc_db,
833  vx_image in0_img,
834  vx_image out0_img,
835  vx_image out1_img,
836  vx_image in1_img,
837  vx_image out2_img,
838  vx_image out3_img);
847 
856 
865 
875 
884 
894 
895 #ifdef __cplusplus
896 }
897 #endif
898 
899 #endif /* HWA_VPAC_LDC_H_ */
900 
901 
struct _vx_image * vx_image
The region_params data structure used by the TIVX_KERNEL_VPAC_LDC kernel.
Definition: hwa_vpac_ldc.h:289
The remap params structure used by the TIVX_KERNEL_VPAC_LDC kernel. Passed as argument to TIVX_VPAC_L...
Definition: hwa_vpac_ldc.h:479
#define TIVX_VPAC_LDC_BIT_DEPTH_CONV_LUT_SIZE
Definition: hwa_vpac_ldc.h:226
void tivx_vpac_ldc_region_params_init(tivx_vpac_ldc_region_params_t *prms)
Function to initialize LDC Region parameters.
uint32_t luma_interpolation_type
Definition: hwa_vpac_ldc.h:344
void tivxUnRegisterHwaTargetVpacLdcKernels(void)
Function to un-register HWA Kernels on the vpac_ldc Target.
VX_API_ENTRY vx_node VX_API_CALL tivxVpacLdcNode2(vx_graph graph, vx_user_data_object configuration, vx_matrix warp_matrix, vx_user_data_object region_prms, vx_user_data_object mesh_prms, vx_image mesh_img, vx_user_data_object dcc_db, vx_image in0_img, vx_image out0_img, vx_image out1_img, vx_image in1_img, vx_image out2_img, vx_image out3_img)
[Graph] Creates a VPAC_LDC Node. This node takes at most 2 single plane inputs and generate at most 4...
void tivx_vpac_ldc_mesh_params_init(tivx_vpac_ldc_mesh_params_t *prms)
Function to initialize LDC Mesh parameters.
The configuration data structure used by the TIVX_KERNEL_VPAC_LDC kernel.
Definition: hwa_vpac_ldc.h:339
The alternative region_params data structure used by the TIVX_KERNEL_VPAC_LDC kernel.
Definition: hwa_vpac_ldc.h:306
Structure to hold PSA timestamp data.
Definition: hwa_vpac_ldc.h:498
void tivx_vpac_ldc_multi_region_prms_init(tivx_vpac_ldc_multi_region_params_t *prms)
Function to initialize LDC Multi Region parameters.
uint64_t timestamp
Timestamp value.
Definition: hwa_vpac_ldc.h:511
Safety parameters structure for VPAC LDC.
Definition: hwa_vpac_ldc.h:537
void tivx_vpac_ldc_safety_mech_prms_init(tivx_vpac_ldc_safety_mechanism_params_t *prms)
Function to initialize LDC safety mechanism parameters with default values.
struct _vx_user_data_object * vx_user_data_object
The User Data Object. User Data Object is a strongly-typed container for other data structures...
Error info structure attached to a node&#39;s VX_EVENT_NODE_ERROR event via tivxSetTargetKernelInstanceEr...
Definition: hwa_vpac_ldc.h:570
void tivx_vpac_ldc_bandwidth_prms_init(tivx_vpac_ldc_bandwidth_params_t *prms)
Function to initialize Bandwidth limiter parameters.
struct _vx_graph * vx_graph
struct _vx_node * vx_node
VX_API_ENTRY vx_node VX_API_CALL tivxVpacLdcNode(vx_graph graph, vx_user_data_object configuration, vx_matrix warp_matrix, vx_user_data_object region_prms, vx_user_data_object mesh_prms, vx_image mesh_img, vx_user_data_object dcc_db, vx_image in_img, vx_image out0_img, vx_image out1_img)
[Graph] Creates a VPAC_LDC Node.
The bandwidth params structure used by the TIVX_KERNEL_VPAC_LDC kernel. Passed as argument to TIVX_VP...
Definition: hwa_vpac_ldc.h:441
uint32_t wdtimer_timeout_cycles
Definition: hwa_vpac_ldc.h:429
struct _vx_matrix * vx_matrix
void tivxRegisterHwaTargetVpacLdcKernels(void)
Function to register HWA Kernels on the vpac_ldc Target.
vx_status(* VX_API_CALL)(vx_reference *ref)
Callback type used to register release callbacks from object derived from references.
Definition: vx_reference.h:56
The mesh data structure in the configuration data structure used by the TIVX_KERNEL_VPAC_LDC kernel...
Definition: hwa_vpac_ldc.h:321
void tivx_vpac_ldc_params_init(tivx_vpac_ldc_params_t *prms)
Function to initialize LDC parameters with the default values.