TIOVX User Guide
vx_khr_user_data_object.h File Reference

The OpenVX User Data Object extension API. More...

#include <VX/vx.h>

Go to the source code of this file.

Macros

#define VX_TYPE_USER_DATA_OBJECT   0x816
 The object type enumeration for user data object. More...
 

Typedefs

typedef struct _vx_user_data_object * vx_user_data_object
 The User Data Object. User Data Object is a strongly-typed container for other data structures.
 

Enumerations

enum  vx_user_data_object_attribute_e {
  VX_USER_DATA_OBJECT_NAME = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_USER_DATA_OBJECT) + 0x0,
  VX_USER_DATA_OBJECT_SIZE = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_USER_DATA_OBJECT) + 0x1,
  VX_USER_DATA_OBJECT_VALID_SIZE = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_USER_DATA_OBJECT) + 0x2
}
 The user data object attributes. More...
 

Functions

VX_API_ENTRY vx_user_data_object VX_API_CALL vxCreateUserDataObject (vx_context context, const vx_char *type_name, vx_size size, const void *ptr)
 Creates a reference to a User Data Object. More...
 
VX_API_ENTRY vx_user_data_object VX_API_CALL vxCreateVirtualUserDataObject (vx_graph graph, const vx_char *type_name, vx_size size)
 Creates an opaque reference to a virtual User Data Object with no direct user access. More...
 
VX_API_ENTRY vx_status VX_API_CALL vxReleaseUserDataObject (vx_user_data_object *user_data_object)
 Releases a reference of a User data object. The object may not be garbage collected until its total reference count is zero. After returning from this function the reference is zeroed. More...
 
VX_API_ENTRY vx_status VX_API_CALL vxQueryUserDataObject (vx_user_data_object user_data_object, vx_enum attribute, void *ptr, vx_size size)
 Queries the User data object for some specific information. More...
 
VX_API_ENTRY vx_status VX_API_CALL vxSetUserDataObjectAttribute (vx_user_data_object user_data_object, vx_enum attribute, const void *ptr, vx_size size)
 Sets an attribute in the User data object. More...
 
VX_API_ENTRY vx_status VX_API_CALL vxCopyUserDataObject (vx_user_data_object user_data_object, vx_size offset, vx_size size, void *user_ptr, vx_enum usage, vx_enum user_mem_type)
 Allows the application to copy a subset from/into a user data object. More...
 
VX_API_ENTRY vx_status VX_API_CALL vxMapUserDataObject (vx_user_data_object user_data_object, vx_size offset, vx_size size, vx_map_id *map_id, void **ptr, vx_enum usage, vx_enum mem_type, vx_uint32 flags)
 Allows the application to get direct access to a subset of the user data object. More...
 
VX_API_ENTRY vx_status VX_API_CALL vxUnmapUserDataObject (vx_user_data_object user_data_object, vx_map_id map_id)
 Unmap and commit potential changes to a user data object subset that was previously mapped. Unmapping a user data object subset invalidates the memory location from which the subset could be accessed by the application. Accessing this memory location after the unmap function completes is implementation specific. More...
 

Detailed Description

The OpenVX User Data Object extension API.

Definition in file vx_khr_user_data_object.h.

Macro Definition Documentation

◆ VX_TYPE_USER_DATA_OBJECT

#define VX_TYPE_USER_DATA_OBJECT   0x816

The object type enumeration for user data object.

A vx_user_data_object.

Definition at line 43 of file vx_khr_user_data_object.h.

Enumeration Type Documentation

◆ vx_user_data_object_attribute_e

The user data object attributes.

Enumerator
VX_USER_DATA_OBJECT_NAME 

The type name of the user data object. Read-only. Use a vx_char[VX_MAX_REFERENCE_NAME] array.

VX_USER_DATA_OBJECT_SIZE 

The number of bytes in the user data object. Read-only. Use a vx_size parameter.

VX_USER_DATA_OBJECT_VALID_SIZE 

The number of valid bytes in the user data object. Must be less than or equal to the value of VX_USER_DATA_OBJECT_SIZE. By default, upon object creation, this value is set to be equal to VX_USER_DATA_OBJECT_SIZE, and may be modified by either the application or a node connected to this object. Read-write. Use a vx_size parameter.

Definition at line 48 of file vx_khr_user_data_object.h.

Function Documentation

◆ vxCreateUserDataObject()

VX_API_ENTRY vx_user_data_object VX_API_CALL vxCreateUserDataObject ( vx_context  context,
const vx_char type_name,
vx_size  size,
const void *  ptr 
)

Creates a reference to a User Data Object.

User data objects can be used to pass a user kernel defined data structure or blob of memory as a parameter to a user kernel.

Parameters
[in]contextThe reference to the overall Context.
[in]type_namePointer to the '\0' terminated string that identifies the type of object. The string is copied by the function so that it stays the property of the caller. The length of the string shall be lower than VX_MAX_REFERENCE_NAME bytes. The string passed here is what shall be returned when passing the VX_USER_DATA_OBJECT_NAME attribute enum to the vxQueryUserDataObject function. In the case where NULL is passed to type_name, then the query of the VX_USER_DATA_OBJECT_NAME attribute enum will return a single character '\0' string.
[in]sizeThe number of bytes required to store this instance of the user data object.
[in]ptrThe pointer to the initial value of the user data object. If NULL, then entire size bytes of the user data object is initialized to all 0s, otherwise, size bytes is copied into the object from ptr to initialize the object
Returns
A user data object reference vx_user_data_object. Any possible errors preventing a successful creation should be checked using vxGetStatus.

◆ vxCreateVirtualUserDataObject()

VX_API_ENTRY vx_user_data_object VX_API_CALL vxCreateVirtualUserDataObject ( vx_graph  graph,
const vx_char type_name,
vx_size  size 
)

Creates an opaque reference to a virtual User Data Object with no direct user access.

Virtual User Data Objects are useful when the User Data Object is used as internal graph edge. Virtual User Data Objects are scoped within the parent graph only.

Parameters
[in]graphThe reference to the parent graph.
[in]type_namePointer to the '\0' terminated string that identifies the type of object. The string is copied by the function so that it stays the property of the caller. The length of the string shall be lower than VX_MAX_REFERENCE_NAME bytes. The string passed here is what shall be returned when passing the VX_USER_DATA_OBJECT_NAME attribute enum to the vxQueryUserDataObject function. In the case where NULL is passed to type_name, then the query of the VX_USER_DATA_OBJECT_NAME attribute enum will return a single character '\0' string.
[in]sizeThe number of bytes required to store this instance of the user data object.
Returns
A user data object reference vx_user_data_object. Any possible errors preventing a successful creation should be checked using vxGetStatus.

◆ vxReleaseUserDataObject()

VX_API_ENTRY vx_status VX_API_CALL vxReleaseUserDataObject ( vx_user_data_object user_data_object)

Releases a reference of a User data object. The object may not be garbage collected until its total reference count is zero. After returning from this function the reference is zeroed.

Parameters
[in]user_data_objectThe pointer to the User Data Object to release.
Returns
A vx_status_e enumeration.
Return values
VX_SUCCESSNo errors.
VX_ERROR_INVALID_REFERENCEIf user_data_object is not a vx_user_data_object.

◆ vxQueryUserDataObject()

VX_API_ENTRY vx_status VX_API_CALL vxQueryUserDataObject ( vx_user_data_object  user_data_object,
vx_enum  attribute,
void *  ptr,
vx_size  size 
)

Queries the User data object for some specific information.

Parameters
[in]user_data_objectThe reference to the User data object.
[in]attributeThe attribute to query. Use a vx_user_data_object_attribute_e.
[out]ptrThe location at which to store the resulting value.
[in]sizeThe size in bytes of the container to which ptr points.
Returns
A vx_status_e enumeration.
Return values
VX_SUCCESSNo errors; any other value indicates failure.
VX_ERROR_INVALID_REFERENCEuser_data_object is not a valid vx_user_data_object reference.
VX_ERROR_NOT_SUPPORTEDIf the attribute is not a value supported on this implementation.
VX_ERROR_INVALID_PARAMETERSIf any of the other parameters are incorrect.

◆ vxSetUserDataObjectAttribute()

VX_API_ENTRY vx_status VX_API_CALL vxSetUserDataObjectAttribute ( vx_user_data_object  user_data_object,
vx_enum  attribute,
const void *  ptr,
vx_size  size 
)

Sets an attribute in the User data object.

Parameters
[in]user_data_objectThe reference to the User data object.
[in]attributeThe attribute to set. Use a vx_user_data_object_attribute_e.
[in]ptrThe pointer to the data to which to set the attribute.
[in]sizeThe size in bytes of the data to which ptr points.
Returns
A vx_status_e enumeration.
Return values
VX_SUCCESSNo errors; any other value indicates failure.
VX_ERROR_INVALID_REFERENCEuser_data_object is not a valid vx_user_data_object reference.
VX_ERROR_NOT_SUPPORTEDIf the attribute is not a value supported on this implementation.
VX_ERROR_INVALID_PARAMETERSIf any of the other parameters are incorrect.

◆ vxCopyUserDataObject()

VX_API_ENTRY vx_status VX_API_CALL vxCopyUserDataObject ( vx_user_data_object  user_data_object,
vx_size  offset,
vx_size  size,
void *  user_ptr,
vx_enum  usage,
vx_enum  user_mem_type 
)

Allows the application to copy a subset from/into a user data object.

Parameters
[in]user_data_objectThe reference to the user data object that is the source or the destination of the copy.
[in]offsetThe byte offset into the user data object to copy.
[in]sizeThe number of bytes to copy. The size must be within the bounds of the user data object: 0 <= (offset + size) <= size of the user data object. If zero, then copy until the end of the object.
[in]user_ptrThe address of the memory location where to store the requested data if the copy was requested in read mode, or from where to get the data to store into the user data object if the copy was requested in write mode. The accessible memory must be large enough to contain the specified size.
[in]usageThis declares the effect of the copy with regard to the user data object using the vx_accessor_e enumeration. Only VX_READ_ONLY and VX_WRITE_ONLY are supported:
  • VX_READ_ONLY means that data are copied from the user data object into the user memory.
  • VX_WRITE_ONLY means that data are copied into the user data object from the user memory.
[in]user_mem_typeA vx_memory_type_e enumeration that specifies the memory type of the memory referenced by the user_addr.
Returns
A vx_status_e enumeration.
Return values
VX_ERROR_OPTIMIZED_AWAYThis is a reference to a virtual user data object that cannot be accessed by the application.
VX_ERROR_INVALID_REFERENCEThe user_data_object reference is not actually a user data object reference.
VX_ERROR_INVALID_PARAMETERSAnother parameter is incorrect.

◆ vxMapUserDataObject()

VX_API_ENTRY vx_status VX_API_CALL vxMapUserDataObject ( vx_user_data_object  user_data_object,
vx_size  offset,
vx_size  size,
vx_map_id map_id,
void **  ptr,
vx_enum  usage,
vx_enum  mem_type,
vx_uint32  flags 
)

Allows the application to get direct access to a subset of the user data object.

Parameters
[in]user_data_objectThe reference to the user data object that contains the subset to map.
[in]offsetThe byte offset into the user data object to map.
[in]sizeThe number of bytes to map. The size must be within the bounds of the user data object: 0 <= (offset + size) <= size of the user data object. If zero, then map until the end of the object.
[out]map_idThe address of a vx_map_id variable where the function returns a map identifier.
[out]ptrThe address of a pointer that the function sets to the address where the requested data can be accessed. The returned (*ptr) address is only valid between the call to the function and the corresponding call to vxUnmapUserDataObject.
[in]usageThis declares the access mode for the user data object subset, using the vx_accessor_e enumeration.
  • VX_READ_ONLY: after the function call, the content of the memory location pointed by (*ptr) contains the user data object subset data. Writing into this memory location is forbidden and its behavior is implementation specific.
  • VX_READ_AND_WRITE : after the function call, the content of the memory location pointed by (*ptr) contains the user data object subset data; writing into this memory is allowed only for the location of data and will result in a modification of the affected data in the user data object once the subset is unmapped.
  • VX_WRITE_ONLY: after the function call, the memory location pointed by (*ptr) contains undefined data; writing to all data in the subset is required prior to unmapping. Data values not written by the application before unmap may be defined differently in different implementations after unmap, even if they were well defined before map.
[in]mem_typeA vx_memory_type_e enumeration that specifies the type of the memory where the user data object subset is requested to be mapped.
[in]flagsAn integer that allows passing options to the map operation. Use the vx_map_flag_e enumeration.
Returns
A vx_status_e enumeration.
Return values
VX_ERROR_OPTIMIZED_AWAYThis is a reference to a virtual user data object that cannot be accessed by the application.
VX_ERROR_INVALID_REFERENCEThe user_data_object reference is not actually a user data object reference.
VX_ERROR_INVALID_PARAMETERSAn other parameter is incorrect.
Postcondition
vxUnmapUserDataObject with same (*map_id) value.

◆ vxUnmapUserDataObject()

VX_API_ENTRY vx_status VX_API_CALL vxUnmapUserDataObject ( vx_user_data_object  user_data_object,
vx_map_id  map_id 
)

Unmap and commit potential changes to a user data object subset that was previously mapped. Unmapping a user data object subset invalidates the memory location from which the subset could be accessed by the application. Accessing this memory location after the unmap function completes is implementation specific.

Parameters
[in]user_data_objectThe reference to the user data object to unmap.
[in]map_idThe unique map identifier that was returned when calling vxMapUserDataObject .
Returns
A vx_status_e enumeration.
Return values
VX_ERROR_INVALID_REFERENCEThe user_data_object reference is not actually a user data object reference.
VX_ERROR_INVALID_PARAMETERSAnother parameter is incorrect.
Precondition
vxMapUserDataObject returning the same map_id value