![]() |
SDL API Guide for J721E
|
DCC Operation Mode | |
| typedef uint32_t | SDL_DCC_mode |
| Enum to select the DCC Operation Mode. More... | |
| #define | SDL_DCC_MODE_SINGLE_SHOT_1 (DCC_DCCGCTRL_SINGLESHOT_MODE1) |
| #define | SDL_DCC_MODE_SINGLE_SHOT_2 (DCC_DCCGCTRL_SINGLESHOT_MODE2) |
| #define | SDL_DCC_MODE_CONTINUOUS (DCC_DCCGCTRL_SINGLESHOT_DISABLE) |
DCC Clock source of COUNT0 | |
| typedef uint32_t | SDL_DCC_clkSrc0 |
| Enum to select the COUNT0 clock source. More... | |
| #define | SDL_DCC_CLK0_SRC_CLOCK0_0 (DCC_DCCCLKSRC0_CLKSRC0_0) |
| #define | SDL_DCC_CLK0_SRC_CLOCK0_1 (DCC_DCCCLKSRC0_CLKSRC0_1) |
| #define | SDL_DCC_CLK0_SRC_CLOCK0_2 (DCC_DCCCLKSRC0_CLKSRC0_2) |
DCC Clock source of COUNT1 | |
| typedef uint32_t | SDL_DCC_clkSrc1 |
| Enum to select the COUNT1 clock source. More... | |
| #define | SDL_DCC_CLK1_SRC_CLOCK1 (DCC_DCCCLKSRC1_CLKSRC_0) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC0 (DCC_DCCCLKSRC1_CLKSRC_1) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC1 (DCC_DCCCLKSRC1_CLKSRC_2) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC2 (DCC_DCCCLKSRC1_CLKSRC_3) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC3 (DCC_DCCCLKSRC1_CLKSRC_4) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC4 (DCC_DCCCLKSRC1_CLKSRC_5) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC5 (DCC_DCCCLKSRC1_CLKSRC_6) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC6 (DCC_DCCCLKSRC1_CLKSRC_7) |
| #define | SDL_DCC_CLK1_SRC_CLOCKSRC7 (DCC_DCCCLKSRC1_CLKSRC_8) |
| #define | SDL_DCC_CLK1_SRC_FICLK (DCC_DCCCLKSRC1_CLKSRC_OTHER) |
DCC Interrupt type | |
| typedef uint32_t | SDL_DCC_intrType |
| Enum for DCC interrupts. More... | |
| #define | SDL_DCC_INTERRUPT_ERR (0x0U) |
| #define | SDL_DCC_INTERRUPT_DONE (0x1U) |
| #define SDL_DCC_MODE_SINGLE_SHOT_1 (DCC_DCCGCTRL_SINGLESHOT_MODE1) |
Stop counting when counter0 and valid0 both reach zero
| #define SDL_DCC_MODE_SINGLE_SHOT_2 (DCC_DCCGCTRL_SINGLESHOT_MODE2) |
Stop counting when counter1 reaches zero
| #define SDL_DCC_MODE_CONTINUOUS (DCC_DCCGCTRL_SINGLESHOT_DISABLE) |
Continuously repeat (until error)
| #define SDL_DCC_CLK0_SRC_CLOCK0_0 (DCC_DCCCLKSRC0_CLKSRC0_0) |
SYS_CLK1 is selected as source for COUNT0
| #define SDL_DCC_CLK0_SRC_CLOCK0_1 (DCC_DCCCLKSRC0_CLKSRC0_1) |
SYS_CLK2 is selected as source for COUNT0
| #define SDL_DCC_CLK0_SRC_CLOCK0_2 (DCC_DCCCLKSRC0_CLKSRC0_2) |
XREF_CLK is selected as source for COUNT0
| #define SDL_DCC_CLK1_SRC_CLOCK1 (DCC_DCCCLKSRC1_CLKSRC_0) |
TEST_CLK1 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC0 (DCC_DCCCLKSRC1_CLKSRC_1) |
TEST_CLK0 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC1 (DCC_DCCCLKSRC1_CLKSRC_2) |
TEST_CLK1 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC2 (DCC_DCCCLKSRC1_CLKSRC_3) |
TEST_CLK2 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC3 (DCC_DCCCLKSRC1_CLKSRC_4) |
TEST_CLK3 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC4 (DCC_DCCCLKSRC1_CLKSRC_5) |
TEST_CLK4 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC5 (DCC_DCCCLKSRC1_CLKSRC_6) |
TEST_CLK5 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC6 (DCC_DCCCLKSRC1_CLKSRC_7) |
TEST_CLK6 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC7 (DCC_DCCCLKSRC1_CLKSRC_8) |
TEST_CLK7 is selected as source for COUNT1
| #define SDL_DCC_CLK1_SRC_FICLK (DCC_DCCCLKSRC1_CLKSRC_OTHER) |
OTHER_CLK is selected as source for COUNT1
| #define SDL_DCC_INTERRUPT_ERR (0x0U) |
The error signal
| #define SDL_DCC_INTERRUPT_DONE (0x1U) |
Done interrupt signal
| typedef uint32_t SDL_DCC_mode |
Enum to select the DCC Operation Mode.
DCC can either operate in single shot or continuous mode.
| typedef uint32_t SDL_DCC_clkSrc0 |
Enum to select the COUNT0 clock source.
| typedef uint32_t SDL_DCC_clkSrc1 |
Enum to select the COUNT1 clock source.
| typedef uint32_t SDL_DCC_intrType |
Enum for DCC interrupts.
| enum SDL_DCC_Inst |