![]() |
MCUSW
|
This document details AUTOSAR BSW Flash module implementation
The Flash Driver provides services for reading, writing, erasing flash memory and Execute-in-Place (XIP) mode for external Flash Device.
The driver supports the following devices:
| Device | Flash Protocol | Boards supported |
| MT35XU512ABA1G12 | OSPI | J721E |
| S28HS512T | XSPI | J721S2, J7200, J784S4, J742S2 |
| MT25QU512ABB | QSPI | J721S2 |
The main tasks of the FLS driver are:
Please refer the Flash design, which is included as part of CSP.
The Fls Module uses internal OSPI peripheral as the serial bus to transfer data to and from the attached flash device.
Programming of clock source for the flash, is beyond the scope of this document. The Clock programming is taken care by the test application.
1 Fls instance is supported by this driver implementation.
The Fls Driver implementation supports multiple configuration variants (refer section Introduction), the driver expects generated Fls_Cfg.h to be present as (Configuration Folder Structure). Please refer (Build) to specify path to generated configuration. The associated Fls configuration generated files Fls_Cfg.c, and Fls_PBcfg.c to be present as shown (Configuration Folder Structure)
The Flash (FLS) driver in the MCAL layer interacts with various types of NOR flash memory devices. To maintain modularity and enhance portability across different hardware platforms, the board layer has been introduced.
The board layer resides separately at: mcusw/mcal_drv/mcal/board
The board layer for the FLS driver contains hardware-specific implementations, configurations, and command sequences necessary to interact directly with flash memory devices. By isolating board-specific details from the generic FLS driver logic, we achieve:
The board layer consists of the following important files for flash functionality:
| File Name | Description |
|---|---|
Fls_Brd_Nor_Ospi.c | Board-specific implementation for NOR flash using OSPI protocol |
Fls_Brd_Nor_Qspi.c | NOR flash interactions via QSPI interface |
Fls_Brd_Nor_Xspi.c | XSPI-based flash access and command sequencing |
Fls_Brd_Nor.c | SPI command patterns specific to flash operations |
nor_spi_patterns.c, nor_spi_phy_tune.c | PHY-level tuning and adjustments for stable flash interactions |
The board layer takes care of:
When adding a custom flash device, users may need to modify or extend the board layer code according to the specifications provided in the flash datasheet. This could involve:
Note: The board layer implementation is not qualified for functional safety.
The current driver supports the following protocols for custom flash devices:
Ensure the correct protocol is selected based on the flash device’s capabilities.
The FlsMemConfiguration section of the EB Tresos configurator allows the user to define custom flash devices. Key fields and their descriptions for custom flash configuration include:
FLS_NORFLS_OSPI67108864 (64KB)4096 (4KB)4096 (4KB) for hybrid sectors.FlsNORUniformSectorSize. It will default to FlsNORUniformSectorSize which represents the regular sector size.0x4000000 (64MB)0x100 (256B)0xFF.0xC7 for supported devices, 0U if unsupported.0x01 for supported devices, 0U if unsupported.In addition to the above, other fields are also present in the configuration, such as commands for read, write, and specific flash operations, which are similarly defined for supported and unsupported devices. Above is the description of some key fields.
Ensure all relevant commands are defined according to the flash device’s datasheet.
This section explains the purpose and structure of the sectorList[] configuration used in the Flash (FLS) Driver module, following AUTOSAR standards. This configuration is typically set up in EB Tresos and consumed by the FLS driver during runtime to manage flash memory operations.
The sectorList[] is an array of Fls_SectorType structures. Each element describes a block of flash memory with a common configuration, allowing the driver to correctly interpret fl layout and perform operations like read, write, and erase.
| Field Name | Type | Description |
|---|---|---|
sectorStartaddress | uint32 | Start address (in flash address space) of the first sector in this configuration block. It must be aligned to the corresponding sectorSize. |
sectorSize | uint32 | Size (in bytes) of one sector in this configuration block. It may vary between configurations in case of hybrid sector layout. |
sectorPageSize | uint32 | Page size (in bytes) of the sector. This is the granularity used for programming (writing) operations. This is typically constant for a given flash device. |
numberOfSectors | uint32 | Number of contiguous sectors with identical configuration starting at sectorStartaddress. |
In EB Tresos, users should:
FlsSectorList entries.Tip: Uniform sectors can be defined with one entry. Hybrid sector layouts (e.g., small boot sectors + large data sectors) require multiple entries.
During runtime, the FLS driver uses sectorList[] to:
The driver internally stores sectorList[] in Fls_DrvObj.sectorList[] and determines the active configuration using Fls_DetermineSectorCfgIndex().
The image below illustrates the Custom Flash Configuration in the EB Tresos tool, where the user can define parameters such as the NOR device type, protocol mode, sector sizes, and various command configurations. These fields allow seamless integration and customization of external flash devices by configuring the appropriate values for each field.
The driver uses two primary configuration files:
Above file is generated based on the configuration fields set in the configurator. Ensure that file is included correctly in the build path to avoid errors.
Sector Size Configuration In the FLS driver configuration, two key fields help in defining the size of sectors in the flash memory:
NOR_UNIFORM_SECTOR_SIZE: This field represents the size of the sectors when the flash uses a regular or uniform sector size throughout the memory. If the flash device has consistent sector sizes across the entire memory, this parameter is used to define the sector size.
Example:
In such cases, the flash memory has uniform sectors of 64KB, and this value will be used for erasing, writing, and reading operations. The system will rely on this parameter alone to manage sector-related operations.
Example
Protocol Configuration
Current FLS driver uses OSPI, XSPI, and QSPI protocol modes and supports the three NOR Flash devices for all devices (MT35XU512ABA1G12, S28HS512T, and MT25QU512ABB).
If variation to the supported features are needed, user will need to take care to modify the driver to accommodate changes.
Fls_Cfg.c.Fls_Cfg.c or Fls_PBcfg.c. Since a single flash device can be used in runtime, driver will detect the flash used during the Fls_init and use that flash configured in the driver. Although detecting the flash device used during the runtime is taken care in the driver, the user needs to ensure the flash commands are configured properly during the configuration.As the Fls driver supports different flash protocols, and the configuration differs based on the selected protocol:
NOR_BLOCK_SIZE parameter is used when configuring devices with the XSPI protocol. The block size value defines the erase unit size for the flash memory.NOR_SECTOR_SIZE parameter is utilized. This configuration reflects the sector size used for read, write, and erase operations specific to these protocols.(When configuring flash devices using the FlsMemConfiguration field, ensure that the correct protocol is set so that the driver can apply the appropriate block or sector sizes based on the selected flash type.)
Handling Flash Operations
The driver supports the following operations for custom flash devices:
Error Handling for Custom Flash Devices
When integrating custom flash devices, pay attention to the following error handling mechanisms:
0U in the configuration to avoid operation failure.Key Considerations
When configuring a custom flash device, ensure the following:
FlsNORCmdPageProg, FlsNORCmdSecErase) are supported by the custom flash. Unsupported commands should be set to 0U.0xFF for erased data. Ensure the FlsNORErasedData is correctly set.0U, and the driver will fall back on the regular FlsNORUniformSectorSize.The FLS driver incorporates safety checks to ensure data integrity and proper operation across supported flash devices. These checks include boundary verifications for uniform and hybrid sector sizes, valid address alignment, and command execution correctness. Although the driver is thoroughly tested and verified for the following flash devices:
It is important to note that when adding custom flash devices, these safety mechanisms will ensure that the driver performs appropriate validations during read, write, and erase operations. While custom devices can be configured, it is critical to refer to the device's datasheet to ensure proper configuration of commands, sizes, and addressing modes. For any device not listed here, ensure that it adheres to similar specifications to the tested devices to maintain the driver's integrity and safety standards.
Note: For detailed descriptions of all configurable parameters, refer to the design document provided in the CSP package. The document is located at: "$(MCAL_INSTALL_PATH)/mcusw/csp"
The following section details on the unsupported features and additional features added.
This parameter is the switch between Direct Access Mode (DAC) and Indirect Access Mode (INDAC) used by the OSPI module to communicate with the Flash Device. The Flash will be memory mapped when running in DAC mode, and execution in place will happen directly from flash memory. In INDAC mode, data transfer between system memory and external flash occurs through the internal SRAM.
This parameter is the switch to turn on or off XIP mode. Only XIP Read mode is supported in current driver. XIP mode will only be functional in DAC mode of operation.
This parameter defines the Clock Speed for the OSPI peripheral. The supported clock speeds are as follows:
This parameter is the switch between Double Transfer Rate (DTR) and Single Transfer Rate (STR) for OSPI Flash.
This parameter is the switch to turn on and off PHY mode.
This parameter defines the Block size for the OSPI peripheral. The parameter shall be obtained as the base-2 logarithm of sectorSize.
For example: if the sectorSize is 262144 then, blockSize = log2(262144) = 18
Following features outlined in Specification are not supported:
In compliance with project-specific requirements, the FlsSectorList field has been removed from the configurator. Instead, the flash-related information, such as sector size, block size, and page size, is now defined through the fields in FlsMemConfiguration. These fields include:
This deviation from the AUTOSAR specification ensures a more streamlined and flexible configuration for flash devices. The use of the FlsMemConfiguration fields allows for easier integration of custom flash devices while maintaining necessary safety and validation checks.
By using these parameters, the driver automatically detects the flash used in runtime during the Fls_Init by reading and comparing the Flash device and manufacturer Id. The driver will use the commands specific to that flash instance. This modification allows support for multiple custom flash devices while still adhering to core safety mechanisms, even though it deviates from the strict AUTOSAR spec implementation. Refer section (refer section Configuration) for custom flash addition.
With the introduction of multi-flash support, existing customers must adjust their configurations to align with the new structure. Follow the steps below to transition smoothly:
FlsMemConfiguration and add all flash specific commands for each flash devices.Fls_Cfg.c.FlsMemConfiguration field in the EB Tresos configurator to define flash parameters such as:Fls_Cfg.c. The driver will detect the flash used in the application and use the configured commands specific to that flash in the driver.Fls_Brd_Nor.c) reference the new flash specific commands and settings.FlsMemConfiguration within EB Tresos.Fls_Cfg.c for any custom commands or configurations.FlsMemConfiguration field.Fls_Cfg.c.As noted from the previous MCAL implementation, some of the critical configuration registers could potentially be corrupted by other entities (s/w or h/w). One of the recommended detection methods would be to periodically read-back the configuration and confirm configuration is consistent. The service API defined below shall be implemented to enable this detection
| Description | Comments | |
| Service Name | Ospi_RegisterReadback | Can potentially be turned OFF (Refer to Design Document provided in CSP) |
| Syntax | Ospi_RegisterReadback( P2VAR(CSL_ospi_flash_cfgRegs, AUTOMATIC, SPI_APPL_DATA) RegRbPtr) | E_OK: Register read back has been done, E_NOT_OK: Register read back failed |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | None | |
| Parameters out | RegRbPtr | Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK. |
| Return Value | Std_ReturnType | E_OK, E_NOT_OK |
This API Enable Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrEnable | Fls_dataOverflowUnderflowIntrEnable Enable Under/Overflow Interrupts of the hardware unit |
| Syntax | Fls_dataOverflowUnderflowIntrEnable(uint32 intrFlag) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Enable flag for Underflow=2U Interrupt Enable flag for Overflow=128U |
| Parameters out | NA | |
| Return Value | Std_ReturnType | E_OK: Interrupt Enabled E_NOT_OK: Interrupt Enable failed |
This API Disable Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrDisable | Spi_dataOverflowUnderflowIntrDisable Disable Under/Overflow Interrupts of the hardware unit and returns the status. |
| Syntax | Fls_dataOverflowUnderflowIntrDisable(uint32 intrFlag) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Disable flag for Underflow=2U Interrupt Disable flag for Overflow=128U |
| Parameters out | NA | |
| Return Value | Std_ReturnType | E_OK: Interrupt Disabled E_NOT_OK: Interrupt Disabled failed |
This API gets status of Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrGetStatus | Fls_dataOverflowUnderflowIntrGetStatus gets status of Under/Overflow Interrupts of the hardware unit |
| Syntax | Fls_dataOverflowUnderflowIntrGetStatus(uint32 intFlags) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Enable flag |
| Parameters out | NA | |
| Return Value | ospiIrqstatus | OSPI_NO_EVENT: No underflow event OSPI_EVENT_PENDING: Underflow Event OSPI_STATUS_READ_FAIL: Status read fail |
This API clear Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrStatusClear | Fls_dataOverflowUnderflowIntrStatusClear clear Under/Overflow Interrupts of the hardware unit and returns the status. |
| Syntax | Fls_dataOverflowUnderflowIntrStatusClear(uint32 intrFlag) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Enable flag for Underflow=2U Interrupt Enable flag for Overflow=128U |
| Parameters out | NA | |
| Return Value | Std_ReturnType | E_OK: Interrupt status clears E_NOT_OK: Interrupt status clear failed |
The driver can have unexpected behavior and loss of functionality if unsupported values are passed into configurator or unsupported combinations are used. Below is a list of such constraints.
Note: Only one OSPI instance (OSPI_0 or OSPI_1) is supported at a time.
The Driver does not register any interrupt service routine(ISR), it’s expected that consumer of this driver registers the required interrupt handler.
The interrupt number associated with instance of the Fls is detailed in TRM. Please refer FlsApp_InterruptConfig() in fls_app_intr test application for reference.
Please note that interrupt implementation is only available when running with INDAC mode. BlankCheck and Compare APIs are not supported with interrupt mode.
The driver doesn't configure the functional clock and power for the Fls modules. It's expected that secondary boot loader(SBL) power-up the required modules. Please refer SBL documentation.
There PHY algorthm used in J7200, J721E, J721S2, and J784S4,J742S2 are based on calibration algorithm. QSPI device on J721S2 do not have PHY tune as of now.
The Phy tune data vector must first be flashed into the last sector of flash memory, and then during first read operation, Phy tune will be calibrated.
The example application can be used as reference for this.
Some restrictions that Fls driver has right now with respect to the SoC:
J721S2 support both XSPI flash device (s28hs512t) and QSPI flash device (mt25qu512abb). The build command "FLS_PROTOCOL=qspi" and "FLS_PROTOCOL=ospi" is used to differentiate between using XSPI vs QSPI flash device. example/Fls/QSPI_Cfg has QSPI configuration files. Currently only one flash device can be used at a time on J721S2.
Refer to Build and Running the Application for QSPI build instructions.
Refer to Configuration Folder Structure for QSPI configuration folder
Please follow steps detailed in section (Build) to build library or example. Please note that OSPI Boot mode is not applicable for Fls module.
The below Fls Test Applications are available:
Please refer to Configuration Folder Structure on which of the three configuration folders each Fls Test Apllication uses.
Note: Please do a clean build (make -s allclean) when a different configuration folder is used. Each configuration folder header files have different define values.
M35XU512_4BYTE_ADDRESSING Flash in the configurator under FlsMemConfiguration field.Note: SDR mode does not support Phy Tune
Please follow steps detailed in section (Build) to build example
Poll Mode - Storage Mode
Test Applications fls_app_dac and fls_app_indac will run as packaged, just build and the executable will be generated.
Interrupt Mode - Storage Mode
Build fls_app_intr and run. Uses different configuration files than Poll Mode, so please build this application on a clean build.
This implementation depends on the DET in order to report development errors and can be turned OFF. Refer section (Development Error Reporting) for detailed error codes.
This implementation requires one level of exclusive access to guard critical sections. Invokes SchM_Enter_Fls_FLS_EXCLUSIVE_AREA_0 (), SchM_Exit_Fls_FLS_EXCLUSIVE_AREA_0 () to enter critical section and exit.
In the example implementation (Driver File Structure SchM_Fls.c) , all the interrupts on CPU are disabled. However, disabling of the enabled Fls interrupt should suffice.
This implementation depends on MemIf module and uses its imported types such as MemIf_JobResultType, MemIf_ModeType and MemIf_StatusType.
This implementation depends on Fee module for callback notification to notify the module environment about job end and job error.
Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface (Fls.h) lists the SID.
| Type of Error | Related Error code | Value (Hex) |
| API service called with wrong parameter | FLS_E_PARAM_CONFIG | 0x01 |
| API service called with wrong parameter | FLS_E_PARAM_ADDRESS | 0x02 |
| API service called with wrong parameter | FLS_E_PARAM_LENGTH | 0x03 |
| API service called with wrong parameter | FLS_E_PARAM_DATA | 0x04 |
| API service used without module initialization | FLS_E_UNINIT | 0x05 |
| API called when module is busy | FLS_E_BUSY | 0x06 |
| API called with a Null Pointer | FLS_E_PARAM_POINTER | 0x0A |
Transient errors are reported to the DET using the service Det_reportDetTransientFault(). The driver interface (Fls.h) lists the SID.
| Type of Error | Related Error code | Value (Hex) |
| Flash Erase Failed in HW | FLS_E_ERASE_FAILED | 0x01 |
| Flash Write Failed in HW | FLS_E_WRITE_FAILED | 0x02 |
| Flash Read Failed in HW | FLS_E_READ_FAILED | 0x03 |
| Flash Compare Failed in HW | FLS_E_COMPARE_FAILED | 0x04 |
| Expected HW ID not matched | FLS_E_UNEXPECTED_FLASH_ID | 0x05 |
The AUTOSAR BSW Flash Driver specification details the APIs required for Flash Driver. Please refer to (Refer to Design Document provided in CSP) for detailed API description.
Refer API Documentation for details
The example application demonstrates use of Fls module, the list below identifies key steps performed in the example. The configuration file is present at (Configuration Folder Structure).
Polled Storage Mode (fls_app_dac and fls_app_indac)
Interrupt Storage Mode (fls_app_intr)
Performance Measurements
FLS_APP_DAC:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_DAC:
Running on J7 ES
FLS_APP_DAC: OSPI0 controller will be configured for OSPI/XSPI flash
FLS_APP_DAC: FLS spi_test Initiating and Starting.
FLS_APP_DAC: Variant - Pre Compile being used !!!
FLS_APP_DAC: Configuring Clocks.
FLS_APP_DAC: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 10
SW Minor Version : 0
SW Patch Version : 0
FLS_APP_DAC: DATA SIZE TEST is 0x100000
FLS_APP_DAC: Offset is 0x0
FLS_APP_DAC:
*****************Writing PHY Tune Data to last sector in memory*****************
FLS_APP_DAC: Erasing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Blank Checking
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Writing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Write 1048576 bytes at transfer rate 107557 Kbps
FLS_APP_DAC: Comparing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
*************************Writing PHY Tune Data complete*************************
FLS_APP_DAC: Erasing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Blank Checking
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Writing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Write 1048576 bytes at transfer rate 2533 Kbps
FLS_APP_DAC: Reading
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Read 1048576 bytes at transfer rate 40725 Kbps
FLS_APP_DAC: Comparing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Reading
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Read 1048576 bytes at transfer rate 41341 Kbps
FLS_APP_DAC: All tests have passed! FLS_APP_INDAC:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_INDAC:
Running on J7 ES
FLS_APP_INDAC: OSPI0 controller will be configured for OSPI/XSPI flash
FLS_APP_INDAC: FLS spi_test Initiating and Starting.
FLS_APP_INDAC: Variant - Pre Compile being used !!!
FLS_APP_INDAC: Configuring Clocks.
FLS_APP_INDAC: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 10
SW Minor Version : 0
SW Patch Version : 0
FLS_APP_INDAC: DATA SIZE TEST is 0x100000
FLS_APP_INDAC: Offset is 0x0
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Blank Checking
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Writing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8912 Kbps
FLS_APP_INDAC: Cancel while Erasing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Cancel while Writing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 53350 Kbps
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Comparing.Expected to fail as data is erased.
FLS_APP_INDAC: Job Processing in Progress.
Det Error reported
Module ID 92
Instance ID 0
SID 8
Error ID 8
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Cancel while Comparing.Expected to fail as data is erased.
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Writing to compare again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8911 Kbps
FLS_APP_INDAC: Comparing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Reading
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 44758 Kbps
FLS_APP_INDAC: Cancel while Reading
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 53349 Kbps
FLS_APP_INDAC:
.......................Changing mode to DAC.......................
FLS_APP_INDAC: Reading
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 20022 Kbps
FLS_APP_INDAC: Comparing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
....................Changing mode to INDAC.....................
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Blank Checking
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Writing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8913 Kbps
FLS_APP_INDAC: Reading
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 44756 Kbps
FLS_APP_INDAC: Comparing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Cancel Erase Job
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Blank Checking after erase cancel-----Expect to fail
FLS_APP_INDAC: Job Processing in Progress.
Det Error reported
Module ID 92
Instance ID 0
SID 10
Error ID 7
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Erasing again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Blank Checking after erase again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Cancel after Writing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 53350 Kbps
FLS_APP_INDAC: Comparing after write cancel---Expect to fail
FLS_APP_INDAC: Job Processing in Progress.
Det Error reported
Module ID 92
Instance ID 0
SID 8
Error ID 8
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Writing again. Will pass
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8914 Kbps
FLS_APP_INDAC: Comparing.Expected to pass since write passed.
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Writing.
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8913 Kbps
FLS_APP_INDAC: Cancel while Reading
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 53349 Kbps
FLS_APP_INDAC: Reading again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 44751 Kbps
FLS_APP_INDAC: Cancel while Comparing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Comparing again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Changing mode to DAC
FLS_APP_INDAC: FLS SPI TEST DONE!
FLS_APP_INDAC: Ospi configuration Register Readback values
FLS_APP_INDAC: CONFIG_REG : 0x81783881
FLS_APP_INDAC: DEV_INSTR_RD_CONFIG_REG : 0x1e03339d
FLS_APP_INDAC: DEV_INSTR_WR_CONFIG_REG : 0x33082
FLS_APP_INDAC: DEV_DELAY_REG : 0x300000a
FLS_APP_INDAC: DEV_SIZE_CONFIG_REG : 0x111003
FLS_APP_INDAC: SRAM_PARTITION_CFG_REG : 0x3f
FLS_APP_INDAC: DMA_PERIPH_CONFIG_REG : 0x0
FLS_APP_INDAC: MODE_BIT_CONFIG_REG : 0x200
FLS_APP_INDAC: TX_THRESH_REG : 0x1
FLS_APP_INDAC: RX_THRESH_REG : 0x1
FLS_APP_INDAC: PHY_CONFIGURATION_REG : 0x2d0021
FLS_APP_INDAC: All tests have passed! FLS_APP_INTR:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_INTR: OSPI0 controller will be configured for OSPI/XSPI flash
FLS_APP_INTR: FLS spi_test Initiating and Starting.
FLS_APP_INTR: Configuring Interrupt.
FLS_APP_INTR: Variant - Pre Compile being used !!!
FLS_APP_INTR: Configuring Clocks.
FLS_APP_INTR: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 10
SW Minor Version : 0
SW Patch Version : 0
FLS_APP_INTR: DATA SIZE TEST is 0x100000
FLS_APP_INTR: Offset is 0x0
FLS_APP_INTR: Erasing
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR: Manual comparing erased data
FLS_APP_INTR: Calling Read to manually compare
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58417 Kbps
FLS_APP_INTR: Manual Comparing is Correct
FLS_APP_INTR: Cancel while Writing
FLS_APP_INTR: Cancel job Processing in Progress.
FLS_APP_INTR: Error is expected as we are cancelling the operation.
FLS_APP_INTR: Job Ends: ERROR
FLS_APP_INTR:
Write 1048576 bytes at transfer rate 55448 Kbps
FLS_APP_INTR: Cancel while Reading
FLS_APP_INTR: Cancel job Processing in Progress.
FLS_APP_INTR: Error is expected as we are cancelling the operation.
FLS_APP_INTR: Job Ends: ERROR
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 56766 Kbps
FLS_APP_INTR: Erasing
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR: Manual comparing erased data
FLS_APP_INTR: Calling Read to manually compare
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58439 Kbps
FLS_APP_INTR: Manual Comparing is Correct
FLS_APP_INTR: Writing Again without Cancel
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Write 1048576 bytes at transfer rate 13121 Kbps
FLS_APP_INTR: Reading without cancel
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58452 Kbps
FLS_APP_INTR: Manual Comparing written data
FLS_APP_INTR: Calling Read to manually compare
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58433 Kbps
FLS_APP_INTR: Manual Comparing is Correct
FLS_APP_INTR:
Changing mode to DAC
FLS_APP_INTR: FLS SPI TEST DONE!
FLS_APP_INTR: Ospi configuration Register Readback values
FLS_APP_INTR: CONFIG_REG : 0x81783881
FLS_APP_INTR: DEV_INSTR_RD_CONFIG_REG : 0x1e03339d
FLS_APP_INTR: DEV_INSTR_WR_CONFIG_REG : 0x33082
FLS_APP_INTR: DEV_DELAY_REG : 0x300000a
FLS_APP_INTR: DEV_SIZE_CONFIG_REG : 0x111003
FLS_APP_INTR: SRAM_PARTITION_CFG_REG : 0x3f
FLS_APP_INTR: DMA_PERIPH_CONFIG_REG : 0x0
FLS_APP_INTR: MODE_BIT_CONFIG_REG : 0x200
FLS_APP_INTR: TX_THRESH_REG : 0x1
FLS_APP_INTR: RX_THRESH_REG : 0x1
FLS_APP_INTR: PHY_CONFIGURATION_REG : 0x2d0021
FLS_APP_INTR: All tests have passed! FLS_APP_XIP:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_XIP:
Running on J7 ES
FLS_APP_XIP: FLS spi_test Initiating and Starting.
FLS_APP_XIP: Variant - Pre Compile being used !!!
FLS_APP_XIP: Configuring Clocks.
FLS_APP_XIP: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 1
SW Minor Version : 2
SW Patch Version : 1
FLS_APP_XIP: DATA SIZE TEST is 0x1000
FLS_APP_XIP: Offset is 0x0
FLS_APP_XIP: Erasing
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Blank Checking
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Writing
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Calling XIP app
MCU1_0 running
MCU1_0 reports: All tests have passed
FLS_APP_XIP: Returning from XIP app, returned value is 0xFEEDFACE
FLS_APP_XIP: Reading
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Comparing
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: DONE!