EthFw Release Notes
Version: 11.01.00.06
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- What's New
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Known Issues
- Dependencies
- Technical Support
- Package Versioning
Introduction
This release notes provides important information that will assist you in using the EthFw component. This document provides the product information and known issues with respect to EthFw software component. The EthFw component consists of firmware for Ethernet switch, profiling tools and demos/applications for J721E, J7200, J784S4 and J742S2 silicon platforms.
Licensing
Refer to Processor SDK RTOS top-level manifest.
Getting Started
The Ethernet Firmware User's Guide provides the documentation and references necessary to run EthFw demos and begin development on TI's platforms.
Documentation
Refer to following documentation for further details:
| Ethernet Firmware User Guide | Build instructions, Demos | [HTML] |
| Ethernet Firmware API Guide | API Guide | [HTML] |
Upgrade and Compatibility Information
Users moving from SDK 8.2 or older to SDK 8.6 must refer to the Porting Guide document which describes how the board initialization routines have been restructured.
VLAN configuration parameter from static shared multicast table has been removed.
Exclusive multicast address is considered to be exclusive irrespective of VLAN. In case when client registers exclusive multicast in a VLAN, VLAN provided will be ignored and it will be registered only based on multicast address. Any other client registering the same multicast address (even with different VLAN) will result an error from EthFw.
Device Support
Below table shows device support for EthFw.| SoC | HOST (OS) | Target (OS) | Test Platform |
| J721E | Linux | FreeRTOS, SafeRTOS | J721E EVM with GESI and QSGMII Daughter Boards |
| J7200 | Linux | FreeRTOS, SafeRTOS | J7200 EVM with QSGMII Daughter Board |
| J784S4 | Linux | FreeRTOS, SafeRTOS | J784S4 EVM with QSGMII Daughter Board |
Refer Processor SDK RTOS RTOS release notes for SDK device support.
Validation Information
This release was built and validated using the following tools. Refer to the EthFw User's Guide for additional instructions to install and setup the dependencies.Build Tools (included in Processor SDK)
- TI ARM CLANG: 4.0.1.LTS
- lwIP stack: 2.2.0
- FreeRTOS Kernel: 10.4.3
- SafeRTOS Kernel - see table below
| SoC | ISA | SafeRTOS package version |
| J721E | R5F | 009-005-199-024-219-005 |
| J7200 | R5F | 009-005-199-024-219-005 |
| J784S4 | R5F | 009-005-199-024-219-005 |
Fixed Issues
| Issue ID | Headline | Module | Reported in Release | Affected Platforms | Fixed in Release |
| ETHFW-2897 | ETHFW is suppressing build warnings | EthFw | 10.00.00.00 | J721E, J7200, J784S4 | 11.01.00 |
| ETHFW-3080 | Incorrect MAC Port Mask Provided to Clients | EthFw | 10.01.00.00 | J721E, J7200, J784S4 | 11.01.00 |
| ETHFW-3068 | EthFw: gPTP synch is not achieved post reset recovery | EthFw | 11.00.00.00 | J721E, J7200, J784S4 | 11.01.00 |
Known Issues and Limitations
| Issue ID | Headline | Module | Reported in Release | Affected Platforms | Workaround in this release |
| ETHFW-2088 | EthFW will get stuck waiting for link if link partner is not ready | Enet, EthFw | 08.04.00.00 | J721E, J7200, J784S4 | None. |
| ETHFW-2575 | CPSW error flags are not getting updated in UDMA host packet descriptor | EthFw | 09.02.00.00 | J721E, J7200, J784S4 | None. |
| ETHFW-2885 | Error Code For Error Packets Not Being Passed to Host CPU in CPSW9G/CPSW5G | Enet, EthFw | 10.00.00.00 | J721E, J7200, J721S2, J784S4 | None. |
| ETHFW-2586 | CPSW ALE Table Reads Return Incorrect Values After Prolonged Operation (>20M Runs) | Enet, EthFw | 09.00.00.00 | J721E, J7200, J721S2, J784S4 | Trigger CPSW ALE read twice before reading value. |
| ETHFW-3415 | EthFw ABI change breaks QNX io-sock driver for versions <= 11.0 | QNX Thin Client | 11.01.00.00 | J721E, J784S4 | None. |
Limitations
As J742S2 EVM E1 version does not provide any Enet board/connector, hence no functionality test has been done on J742S2-EVM. EthFw (built for J742S2) for CPSW_9G is validated on J784S4-EVM post applying a patch. Please refer to ETHFW J742S2 Testing section in ETHFW User's Guide for more details.
Note: The EthFW 11.1 release has an interface change that breaks the ABI with 11.0 or earlier versions of the QNX io-sock thin-client driver. For the driver to work
correctly, an update to the ABI interface header file (ethremotecfg.h) is required.
Don't hesitate to contact TI for further details or refer to
this e2e thread.
Please note that the TI 11.1 io-pkt thin client driver has been updated to accommodate this ABI change.
Dependencies
All Ethernet Firmware dependencies are also part of the SDK, please refer to the User's Guide for details.
Technical Support
For technical support and additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.
| Digit | Meaning | Description |
|---|---|---|
| 1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
| 2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
| 3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
| 4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p. |
Copyright 2023, Texas Instruments Incorporated