![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 148 of file DSPLIB_minerror_priv.h.
Data Fields | |
| pFxnDSPLIB_minerror_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_minerror_exec_cn and DSPLIB_minerror_exec_ci. More... | |
| uint32_t | vecInSize |
| Size of input data DSPLIB_minerror_init that will be retrieved and used by DSPLIB_minerror_exec More... | |
| uint32_t | errCoefsSize |
| Size of error coefficients vector More... | |
| uint32_t | strideIn |
| int32_t | mainLoopCount |
| uint8_t | bufPblock [DSPLIB_MINERROR_IXX_IXX_OXX_PBLOCK_SIZE] |
| pFxnDSPLIB_minerror_exec DSPLIB_minerror_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_minerror_exec_cn and DSPLIB_minerror_exec_ci.
Definition at line 152 of file DSPLIB_minerror_priv.h.
| uint32_t DSPLIB_minerror_PrivArgs::vecInSize |
Size of input data DSPLIB_minerror_init that will be retrieved and used by DSPLIB_minerror_exec
Definition at line 156 of file DSPLIB_minerror_priv.h.
| uint32_t DSPLIB_minerror_PrivArgs::errCoefsSize |
Size of error coefficients vector
Definition at line 158 of file DSPLIB_minerror_priv.h.
| uint32_t DSPLIB_minerror_PrivArgs::strideIn |
Definition at line 159 of file DSPLIB_minerror_priv.h.
| int32_t DSPLIB_minerror_PrivArgs::mainLoopCount |
Definition at line 160 of file DSPLIB_minerror_priv.h.
| uint8_t DSPLIB_minerror_PrivArgs::bufPblock[DSPLIB_MINERROR_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 162 of file DSPLIB_minerror_priv.h.