![]() |
DSPLIB User Guide
|
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_minerror.
Definition in file DSPLIB_minerror_priv.h.
Go to the source code of this file.
Data Structures | |
| struct | DSPLIB_minerror_PrivArgs |
| Structure that is reserved for internal use by the kernel. More... | |
Macros | |
| #define | DSPLIB_MINERROR_IXX_IXX_OXX_PBLOCK_SIZE (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t)) |
| Macro to define the size of bufPblock array of DSPLIB_minerror_PrivArgs structure. More... | |
Typedefs | |
| typedef DSPLIB_STATUS(* | pFxnDSPLIB_minerror_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pErrCoefs, const int *restrict pMaxIndex, const void *restrict pMaxVal) |
| This is a function pointer type that conforms to the declaration of DSPLIB_minerror_exec_ci and DSPLIB_minerror_exec_cn. More... | |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_minerror_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsErrCoefs, const DSPLIB_bufParams1D_t *bufParamsOutIndex, const DSPLIB_bufParams1D_t *bufParamsOutVal, const DSPLIB_minerror_InitArgs *pKerInitArgs) |
| This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_init. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_minerror_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pErrCoefs, const int *restrict pMaxIndex, const void *restrict pMaxVal) |
| This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_exec. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_minerror_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pErrCoefs, const int *restrict pMaxIndex, const void *restrict pMaxVal) |
| This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_exec. More... | |
| DSPLIB_STATUS | DSPLIB_minerror_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsErrCoefs, const int *pMaxIndex, const void *pMaxVal) |
| This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_init. More... | |
| #define DSPLIB_MINERROR_IXX_IXX_OXX_PBLOCK_SIZE (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t)) |
Macro to define the size of bufPblock array of DSPLIB_minerror_PrivArgs structure.
Definition at line 39 of file DSPLIB_minerror_priv.h.
| typedef DSPLIB_STATUS(* pFxnDSPLIB_minerror_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pErrCoefs, const int *restrict pMaxIndex, const void *restrict pMaxVal) |
This is a function pointer type that conforms to the declaration of DSPLIB_minerror_exec_ci and DSPLIB_minerror_exec_cn.
Definition at line 45 of file DSPLIB_minerror_priv.h.
| DSPLIB_STATUS DSPLIB_minerror_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsErrCoefs, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOutIndex, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOutVal, | ||
| const DSPLIB_minerror_InitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_init.
This function determines the configuration for the streaming engine and MMA hardware resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_minerror_exec_ci would be called later independently by the application. When DSPLIB_minerror_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_minerror_exec_ci does not lose cycles to determine the hardware configuration.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsErrCoefs | : Pointer to the structure containing error coefficients information of input buffer |
| [out] | pMaxIndex | : Pointer to the structure containing information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 63 of file DSPLIB_minerror_ci.cpp.
| DSPLIB_STATUS DSPLIB_minerror_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pErrCoefs, | ||
| const int *restrict | pMaxIndex, | ||
| const void *restrict | pMaxVal | ||
| ) |
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_exec.
The function uses streaming engine and C7x DSP to perform the minerror computation.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsErrCoefs | : Pointer to the structure containing error coefficients information of input buffer |
| [out] | bufParamsOutIndex | : Pointer to the structure containing information of ouput buffer |
| [out] | bufParamsOutVal | : Pointer to the structure containing information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
| DSPLIB_STATUS DSPLIB_minerror_exec_cn | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pErrCoefs, | ||
| const int *restrict | pMaxIndex, | ||
| const void *restrict | pMaxVal | ||
| ) |
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_exec.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pErrCoeff | : Pointer to buffer holding the error coefficient data |
| [out] | pMaxIndex | : Pointer to buffer holding the index to the element vector that resulted in the maximum dot product |
| [out] | pMaxVal | : Pointer to buffer holding the value of the maximum dot product |
| DSPLIB_STATUS DSPLIB_minerror_init_cn | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| DSPLIB_bufParams1D_t * | bufParamsErrCoefs, | ||
| const int * | pMaxIndex, | ||
| const void * | pMaxVal | ||
| ) |
This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minerror_init.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsErrCoefs | : Pointer to the structure containing error coefficients information of input buffer |
| [out] | bufParamsOutIndex | : Pointer to the structure containing information of ouput buffer |
| [out] | bufParamsOutVal | : Pointer to the structure containing information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |