SDL API Guide for J721E
sdl_esm_core.h File Reference

Go to the source code of this file.

Macros

#define SDL_MCU_ESM_HI_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_MCU_ESM0_ESM_INT_HI_LVL_0
 
#define SDL_MCU_ESM_LO_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_MCU_ESM0_ESM_INT_LOW_LVL_0
 
#define SDL_MCU_ESM_CFG_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_MCU_ESM0_ESM_INT_CFG_LVL_0
 
#define SDL_WKUP_ESM_HI_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_WKUP_ESM0_ESM_INT_HI_LVL_0
 
#define SDL_WKUP_ESM_LO_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_WKUP_ESM0_ESM_INT_LOW_LVL_0
 
#define SDL_WKUP_ESM_CFG_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_WKUP_ESM0_ESM_INT_CFG_LVL_0
 
#define SDL_MAIN_ESM_HI_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_ESM0_ESM_INT_HI_LVL_0
 
#define SDL_MAIN_ESM_LO_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_ESM0_ESM_INT_LOW_LVL_0
 
#define SDL_MAIN_ESM_CFG_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_ESM0_ESM_INT_CFG_LVL_0
 
#define SDL_ESM_MCU_R5_CORE0_SEC_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE0_ECC_CORRECTED_LEVEL_0
 
#define SDL_ESM_MCU_R5_CORE0_DED_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE0_ECC_UNCORRECTED_LEVEL_0
 
#define SDL_ESM_MCU_R5_CORE1_SEC_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE1_ECC_CORRECTED_LEVEL_0
 
#define SDL_ESM_MCU_R5_CORE1_DED_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE1_ECC_UNCORRECTED_LEVEL_0
 
#define SDL_ESM_MAIN_ESM_ERROR_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_GLUELOGIC_ESM_MAIN_ERR_GLUE_ERR_I_N_0
 

Macro Definition Documentation

◆ SDL_MCU_ESM_HI_INTNO

#define SDL_MCU_ESM_HI_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_MCU_ESM0_ESM_INT_HI_LVL_0

◆ SDL_MCU_ESM_LO_INTNO

#define SDL_MCU_ESM_LO_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_MCU_ESM0_ESM_INT_LOW_LVL_0

◆ SDL_MCU_ESM_CFG_INTNO

#define SDL_MCU_ESM_CFG_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_MCU_ESM0_ESM_INT_CFG_LVL_0

◆ SDL_WKUP_ESM_HI_INTNO

#define SDL_WKUP_ESM_HI_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_WKUP_ESM0_ESM_INT_HI_LVL_0

◆ SDL_WKUP_ESM_LO_INTNO

#define SDL_WKUP_ESM_LO_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_WKUP_ESM0_ESM_INT_LOW_LVL_0

◆ SDL_WKUP_ESM_CFG_INTNO

#define SDL_WKUP_ESM_CFG_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_WKUP_ESM0_ESM_INT_CFG_LVL_0

◆ SDL_MAIN_ESM_HI_INTNO

#define SDL_MAIN_ESM_HI_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_ESM0_ESM_INT_HI_LVL_0

◆ SDL_MAIN_ESM_LO_INTNO

#define SDL_MAIN_ESM_LO_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_ESM0_ESM_INT_LOW_LVL_0

◆ SDL_MAIN_ESM_CFG_INTNO

#define SDL_MAIN_ESM_CFG_INTNO   SDLR_MCU_R5FSS0_CORE0_INTR_ESM0_ESM_INT_CFG_LVL_0

◆ SDL_ESM_MCU_R5_CORE0_SEC_INT

#define SDL_ESM_MCU_R5_CORE0_SEC_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE0_ECC_CORRECTED_LEVEL_0

◆ SDL_ESM_MCU_R5_CORE0_DED_INT

#define SDL_ESM_MCU_R5_CORE0_DED_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE0_ECC_UNCORRECTED_LEVEL_0

◆ SDL_ESM_MCU_R5_CORE1_SEC_INT

#define SDL_ESM_MCU_R5_CORE1_SEC_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE1_ECC_CORRECTED_LEVEL_0

◆ SDL_ESM_MCU_R5_CORE1_DED_INT

#define SDL_ESM_MCU_R5_CORE1_DED_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_MCU_R5FSS0_CORE1_ECC_UNCORRECTED_LEVEL_0

◆ SDL_ESM_MAIN_ESM_ERROR_INT

#define SDL_ESM_MAIN_ESM_ERROR_INT   SDLR_MCU_ESM0_ESM_LVL_EVENT_GLUELOGIC_ESM_MAIN_ERR_GLUE_ERR_I_N_0