SDL API Guide for J721E
sdl Directory Reference

Directories

directory  dcc
 
directory  ecc
 
directory  esm
 
directory  lbist
 
directory  misc
 
directory  pbist
 
directory  r5
 
directory  rti
 
directory  tog
 
directory  vtm
 

Files

file  sdl_ccm.h [code]
 Header file contains enumerations, structure definitions and function.
 
file  sdl_dcc.h [code]
 This file contains the prototypes of the APIs present in the device abstraction layer file of DCC. This also contains some related macros.
 
file  sdl_ecc.h [code]
 Header file contains enumerations, structure definitions and function.
 
file  sdl/sdl_esm.h [code]
 This file contains the SDL ESM API's.
 
file  sdl_esm_core.h [code]
 
file  sdl_exception.h [code]
 Header file contains enumerations, structure definitions and function declarations for SDL EXCEPTION interface.
 
file  sdl_lbist.h [code]
 This file contains the SDL LBIST API's.
 
file  sdl_mcrc.h [code]
 This file contains the prototypes of the APIs present in the device abstraction layer file of MCRC. This also contains some related macros.
 
file  sdl_mpu.h [code]
 Header file contains enumerations, structure definitions and function.
 
file  sdl_msmc.h [code]
 This file contains the SDL-FL API's for MSMC Scrubbing Engine.
 
file  sdl_pbist.h [code]
 This file contains the SDL PBIST API's.
 
file  sdl_pok.h [code]
 This file contains the prototypes of the APIs present in the device abstraction layer file of POK. This also contains some related macros.
 
file  sdl_rat.h [code]
 Header file containing various enumerations, structure definitions and function declarations for the KSBUS RAT Ip. =
(C) Copyright 2016-2020, Texas Instruments, Inc.
 
file  sdl_rom_checksum.h [code]
 This file contains the SDL ROM Checksum API's.
 
file  sdl_tog.h [code]
 
file  sdl_vtm.h [code]
 This file contains the SDL VTM API's.