![]() |
PDK API Guide for J721E
|
I2C driver interface.
============================================================================
The I2C header file should be included in an application as follows:
The I2C driver operates as a master or a slave on a single-master I2C bus, in either I2C_MODE_BLOCKING or I2C_MODE_CALLBACK. In blocking mode, the task's execution is blocked during the I2C transaction. When the transfer has completed, code execution will resume. In callback mode, the task's execution is not blocked, allowing for other transactions to be queued up or to process some other code. When the transfer has completed, the I2C driver will call a user-specified callback function (from a HWI context).
The APIs in this driver serve as an interface to a typical TI-RTOS application. The specific peripheral implementations are responsible to create all the SYS/BIOS specific primitives to allow for thread-safe operation.
A I2C transaction with a I2C peripheral is started by calling I2C_transfer(). The details of the I2C transaction is specified with a I2C_Transaction data structure. This structure allows for any of the three types of transactions: Write, Read, or Write/Read. Each transfer is performed atomically with the I2C master or slave peripheral.
This module serves as the main interface for TI-RTOS applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to a I2C_FxnTable.
The I2C driver interface module is joined (at link time) to a NULL-terminated array of I2C_Config data structures named I2C_config. I2C_config is implemented in the application with each entry being an instance of a I2C peripheral. Each entry in I2C_config contains a:
The I2C driver interface produces log statements if instrumentation is enabled.
Go to the source code of this file.
Data Structures | |
struct | I2C_Transaction |
struct | I2C_Params |
I2C Parameters. More... | |
struct | I2C_FxnTable |
The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation. More... | |
struct | I2C_Config |
I2C Global configuration. More... | |
Macros | |
#define | I2C_CMD_RESERVED 32 |
#define | I2C_CMD_PROBE (0U) |
#define | I2C_CMD_SET_BUS_FREQUENCY (1U) |
#define | I2C_CMD_RECOVER_BUS (2U) |
#define | I2C_CMD_SMBUS_TYPE (3U) |
#define | I2C_STATUS_RESERVED (-((int32_t)32)) |
#define | I2C_STATUS_SUCCESS ((int32_t)(0)) |
Successful status code returned by I2C_control(). More... | |
#define | I2C_STATUS_ERROR (-((int32_t)1)) |
Generic error status code returned by I2C_control(). More... | |
#define | I2C_STATUS_UNDEFINEDCMD (-((int32_t)2)) |
An error status code returned by I2C_control() for undefined command codes. More... | |
#define | I2C_STS_SUCCESS ((int16_t)(1)) |
A status code returned by I2C_transfer(). More... | |
#define | I2C_STS_RESTART ((int16_t)(2)) |
A restart status code returned by I2C transfer callback. More... | |
#define | I2C_STS_ERR ((int16_t)(0)) |
A error status code returned by I2C_transfer(). More... | |
#define | I2C_STS_ERR_TIMEOUT (-(int16_t)(1)) |
A error status code returned by I2C_transfer(). More... | |
#define | I2C_STS_ERR_BUS_BUSY (-(int16_t)(2)) |
I2C bus busy error. More... | |
#define | I2C_STS_ERR_NO_ACK (-(int16_t)(3)) |
I2C no ack error when no acknowledgement is received. More... | |
#define | I2C_STS_ERR_ARBITRATION_LOST (-(int16_t)(4)) |
I2C Arbitration lost error. More... | |
#define | I2C_STS_ERR_ACCESS_ERROR (-(int16_t)(5)) |
I2C Bus Access error. More... | |
#define | I2C_STS_ERR_COMMAND_FAILURE (-(int16_t)(6)) |
I2C FW Command Access Failure. More... | |
#define | I2C_STS_ERR_INVALID_COMMAND (-(int16_t)(7)) |
I2C FW Invalid Command passed. More... | |
#define | I2C_TRANS_VALID_PARAM_MASTER_MODE (0x00000001U) |
I2C_TRANSACTION valid parameter bit fields. More... | |
#define | I2C_TRANS_VALID_PARAM_EXPAND_SA (0x00000002U) |
I2C transaction. More... | |
#define | I2C_WAIT_FOREVER (~((uint32_t)0U)) |
#define | I2C_MAX_CONFIG_CNT (14U) |
Typedefs | |
typedef struct I2C_Config_s * | I2C_Handle |
A handle that is returned from a I2C_open() call. More... | |
typedef void(* | I2C_CallbackFxn) (I2C_Handle handle, I2C_Transaction *msg, int16_t transferStatus) |
I2C callback function. More... | |
typedef void(* | I2C_CloseFxn) (I2C_Handle handle) |
A function pointer to a driver specific implementation of I2C_close(). More... | |
typedef int32_t(* | I2C_ControlFxn) (I2C_Handle handle, uint32_t cmd, void *arg) |
A function pointer to a driver specific implementation of I2C_control(). More... | |
typedef void(* | I2C_InitFxn) (I2C_Handle handle) |
A function pointer to a driver specific implementation of I2C_init(). More... | |
typedef I2C_Handle(* | I2C_OpenFxn) (I2C_Handle handle, const I2C_Params *params) |
A function pointer to a driver specific implementation of I2C_open(). More... | |
typedef int16_t(* | I2C_TransferFxn) (I2C_Handle handle, I2C_Transaction *transaction) |
A function pointer to a driver specific implementation of I2C_transfer(). More... | |
typedef I2C_Config | I2C_config_list[I2C_MAX_CONFIG_CNT] |
Enumerations | |
enum | I2C_TransferMode { I2C_MODE_BLOCKING, I2C_MODE_CALLBACK } |
I2C transfer mode. More... | |
enum | I2C_BitRate { I2C_100kHz = 0, I2C_400kHz = 1, I2C_1P0Mhz = 2, I2C_3P4Mhz = 3 } |
I2C bitRate. More... | |
Functions | |
void | I2C_close (I2C_Handle i2cHnd) |
Function to close a I2C peripheral specified by the I2C handle. More... | |
int32_t | I2C_control (I2C_Handle i2cHnd, uint32_t cmd, void *arg) |
Function performs implementation specific features on a given I2C_Handle. More... | |
void | I2C_init (void) |
Function to initializes the I2C module. More... | |
I2C_Handle | I2C_open (uint32_t idx, I2C_Params *params) |
Function to initialize a given I2C peripheral specified by the particular index value. The parameter specifies which mode the I2C will operate. More... | |
void | I2C_Params_init (I2C_Params *params) |
Function to initialize the I2C_Params struct to its defaults. More... | |
int16_t | I2C_transfer (I2C_Handle i2cHnd, I2C_Transaction *transaction) |
Function that handles the I2C transfer for SYS/BIOS. More... | |
void | I2C_transactionInit (I2C_Transaction *transaction) |