TIDL params structure.
More...
#include <j7_tidl.h>
TIDL params structure.
Definition at line 93 of file j7_tidl.h.
◆ config_checksum
vx_uint8 tivxTIDLJ7Params::config_checksum[TIVX_TIDL_J7_CHECKSUM_SIZE] |
Checksum placeholder for TIDL config params
Definition at line 95 of file j7_tidl.h.
◆ network_checksum
vx_uint8 tivxTIDLJ7Params::network_checksum[TIVX_TIDL_J7_CHECKSUM_SIZE] |
Checksum placeholder for TIDL network params
Definition at line 98 of file j7_tidl.h.
◆ compute_config_checksum
vx_uint32 tivxTIDLJ7Params::compute_config_checksum |
Flag to indicate if config params checksum is to be computed or not
Definition at line 101 of file j7_tidl.h.
◆ compute_network_checksum
vx_uint32 tivxTIDLJ7Params::compute_network_checksum |
Flag to indicate if network params checksum is to be computed or not
Definition at line 104 of file j7_tidl.h.
◆ ioBufDesc
sTIDL_IOBufDesc_t tivxTIDLJ7Params::ioBufDesc |
TIDL input/output buffer descriptor
Definition at line 107 of file j7_tidl.h.
◆ optimize_ivision_activation
vx_uint32 tivxTIDLJ7Params::optimize_ivision_activation |
Flag to enable optimization ivision alg activate, default it is disabled
Definition at line 110 of file j7_tidl.h.
The documentation for this struct was generated from the following file: