![]() |
PDK API Guide for J721E
|
IPC - Multiproc interface.
Go to the source code of this file.
Macros | |
#define | IPC_MP_INVALID_ID (0xFFFFFFFFU) |
Invalid processor id. More... | |
Functions | |
int32_t | Ipc_mpSetConfig (uint32_t selfId, uint16_t numProc, uint32_t procArry[IPC_MAX_PROCS]) |
Sets the multiproc configuration. More... | |
uint32_t | Ipc_mpGetId (const char *name) |
Gets the MultiProc id. More... | |
const char * | Ipc_mpGetName (uint32_t id) |
Gets the name of a processor. More... | |
uint16_t | Ipc_mpGetNumProcessors (void) |
Gets the number of processors. More... | |
uint32_t | Ipc_mpGetSelfId (void) |
Gets executing processor's MultiProc id. More... | |
const char * | Ipc_mpGetSelfName (void) |
Get the processor name for current processor. More... | |
uint32_t | Ipc_mpGetRemoteProcId (uint32_t coreIndex) |
Returns procId of the given index. More... | |