59 #include <ti/drv/ipc/soc/ipc_soc.h> 68 #define IPC_MP_INVALID_ID (0xFFFFFFFFU) 92 int32_t
Ipc_mpSetConfig(uint32_t selfId, uint16_t numProc, uint32_t procArry[IPC_MAX_PROCS]);
uint16_t Ipc_mpGetNumProcessors(void)
Gets the number of processors.
uint32_t Ipc_mpGetRemoteProcId(uint32_t coreIndex)
Returns procId of the given index.
uint32_t Ipc_mpGetSelfId(void)
Gets executing processor's MultiProc id.
const char * Ipc_mpGetName(uint32_t id)
Gets the name of a processor.
data types definitions for ipc module.
int32_t Ipc_mpSetConfig(uint32_t selfId, uint16_t numProc, uint32_t procArry[IPC_MAX_PROCS])
Sets the multiproc configuration.
const char * Ipc_mpGetSelfName(void)
Get the processor name for current processor.
uint32_t Ipc_mpGetId(const char *name)
Gets the MultiProc id.