![]() |
PDK API Guide for J721E
|
HWIP interface
Files | |
file | HwiP.h |
Hardware Interrupt module for the RTOS Porting Interface. | |
Data Structures | |
struct | HwiP_Params |
Basic HwiP Parameters. More... | |
Functions | |
void | HwiP_clearInterrupt (int32_t interruptNum) |
Function to clear a single interrupt. More... | |
HwiP_Handle | HwiP_create (int32_t interruptNum, HwiP_Fxn hwiFxn, const HwiP_Params *hwipParams) |
Function to create an interrupt on CortexM devices. More... | |
HwiP_Handle | HwiP_createDirect (int32_t interruptNum, HwiP_DirectFxn hwiFxn, const HwiP_Params *hwipParams) |
Function to create an interrupt using VIM direct registration. More... | |
HwiP_Status | HwiP_delete (HwiP_Handle hwiPhandle) |
Function to delete an interrupt on CortexM devices. More... | |
uintptr_t | HwiP_disable (void) |
Function to disable interrupts to enter a critical region. More... | |
void | HwiP_disableInterrupt (int32_t interruptNum) |
Function to disable a single interrupt. More... | |
void | HwiP_enableInterrupt (int32_t interruptNum) |
Function to enable a single interrupt. More... | |
void | HwiP_Params_init (HwiP_Params *hwipParams) |
Initialize params structure to default values. More... | |
void | HwiP_restore (uintptr_t key) |
Function to restore interrupts to exit a critical region. More... | |
HwiP_Handle | HwiP_getHandle (int32_t interruptNum) |
Function to get HwiP Handle from an interrupt number. More... | |
int32_t | HwiP_getEventId (int32_t interruptNum) |
Function to get the eventId associated with an interrupt number. More... | |
int32_t | HwiP_post (uint32_t interruptNum) |
Function to post the Hwi interrupt by software. More... | |
Typedefs | |
typedef void * | HwiP_Handle |
Opaque client reference to an instance of a HwiP. More... | |
typedef void(* | HwiP_Fxn) (uintptr_t arg) |
Prototype for the entry function for a hardware interrupt. More... | |
typedef void(* | HwiP_DirectFxn) (void) |
Prototype for the entry function for a hardware interrupt registered using HwiP_createDirect. More... | |
Enumerations | |
enum | HwiP_Status { HwiP_OK = 0, HwiP_FAILURE = (-(int32_t)1) } |
Status codes for HwiP APIs. More... | |
enum | OSAL_armGicTrigType_t { OSAL_ARM_GIC_TRIG_TYPE_LEVEL = 1, OSAL_ARM_GIC_TRIG_TYPE_EDGE = 2, OSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL = 3, OSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL = 4, OSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE = 5, OSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE = 6 } |
Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details. More... | |
Macros | |
#define | HWIP_USE_DEFAULT_PRIORITY (~((uint32_t)0)) |
#define HWIP_USE_DEFAULT_PRIORITY (~((uint32_t)0)) |
typedef void* HwiP_Handle |
Opaque client reference to an instance of a HwiP.
A HwiP_Handle returned from the HwiP_create represents that instance.
typedef void(* HwiP_Fxn) (uintptr_t arg) |
Prototype for the entry function for a hardware interrupt.
typedef void(* HwiP_DirectFxn) (void) |
Prototype for the entry function for a hardware interrupt registered using HwiP_createDirect.
enum HwiP_Status |
Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details.
void HwiP_clearInterrupt | ( | int32_t | interruptNum | ) |
Function to clear a single interrupt.
interruptNum | interrupt number to clear |
HwiP_Handle HwiP_create | ( | int32_t | interruptNum, |
HwiP_Fxn | hwiFxn, | ||
const HwiP_Params * | hwipParams | ||
) |
Function to create an interrupt on CortexM devices.
interruptNum | Interrupt Vector Id |
hwiFxn | entry function of the hardware interrupt |
hwipParams | Pointer to the instance configuration parameters. NULL denotes to use the default parameters. The HwiP default parameters are noted in HwiP_Params_init. |
HwiP_Handle HwiP_createDirect | ( | int32_t | interruptNum, |
HwiP_DirectFxn | hwiFxn, | ||
const HwiP_Params * | hwipParams | ||
) |
Function to create an interrupt using VIM direct registration.
interruptNum | Interrupt Vector Id |
hwiFxn | entry function of the hardware interrupt |
hwipParams | Pointer to the instance configuration parameters. NULL denotes to use the default parameters. The HwiP default parameters are noted in HwiP_Params_init. |
HwiP_Status HwiP_delete | ( | HwiP_Handle | hwiPhandle | ) |
Function to delete an interrupt on CortexM devices.
hwiPhandle | returned from the HwiP_create call |
uintptr_t HwiP_disable | ( | void | ) |
Function to disable interrupts to enter a critical region.
This function can be called multiple times.
For Non-OS case, it must unwound in the reverse order. For example
For FreeRTOS case, after the schedular had started the kernel keeps track of critical nesting count. So here the return key will be NULL.
void HwiP_disableInterrupt | ( | int32_t | interruptNum | ) |
Function to disable a single interrupt.
interruptNum | interrupt number to disable |
void HwiP_enableInterrupt | ( | int32_t | interruptNum | ) |
Function to enable a single interrupt.
interruptNum | interrupt number to enable |
void HwiP_Params_init | ( | HwiP_Params * | hwipParams | ) |
Initialize params structure to default values.
The default parameters are:
hwipParams | Pointer to the instance configuration parameters. |
void HwiP_restore | ( | uintptr_t | key | ) |
Function to restore interrupts to exit a critical region.
key | return from HwiP_disable |
HwiP_Handle HwiP_getHandle | ( | int32_t | interruptNum | ) |
Function to get HwiP Handle from an interrupt number.
interruptNum | the interrupt number |
int32_t HwiP_getEventId | ( | int32_t | interruptNum | ) |
Function to get the eventId associated with an interrupt number.
interruptNum | the interrupt number |
int32_t HwiP_post | ( | uint32_t | interruptNum | ) |
Function to post the Hwi interrupt by software.
interruptNum | the interrupt number |