SDL API Guide for J721E
SDL_ECC_InitConfig_t Struct Reference

Detailed Description

This structure defines the elements of ECC Init configuration.

Data Fields

uint32_t numRams
 
SDL_ECC_MemSubTypepMemSubTypeList
 

Field Documentation

◆ numRams

uint32_t SDL_ECC_InitConfig_t::numRams

Max number of memory sections ECC is enabled on R5F, the memory sections include ATCM, VIM, BTCM RAMs

◆ pMemSubTypeList

SDL_ECC_MemSubType* SDL_ECC_InitConfig_t::pMemSubTypeList

Pointer to list of Vector ID types of ECC enabled memory sections