![]() |
SDL API Guide for J721E
|
Structure containing the region configuration parameters. If application wants to do it's own MPU region configuration (override the default one), then it needs to define this variable and initialize that to desired values: Var: 'const SDL_ArmR5MpuRegionCfg gSdlR5MpuCfg[SDL_ARM_R5F_MPU_REGIONS_MAX]' With above application can have it's own MPU configuration, but MPU configuration will still happen at boot/startup time. Default configurations for MPU regions is present under file: "\src\startup\startup.c".
Data Fields | |
uint32_t | regionId |
uint32_t | enable |
uint32_t | baseAddr |
SDL_ArmR5MpuRegionSize | size |
uint32_t | subRegionEnable |
uint32_t | exeNeverControl |
uint32_t | accessPermission |
uint32_t | shareable |
uint32_t | cacheable |
uint32_t | cachePolicy |
uint32_t | memAttr |
uint32_t SDL_ArmR5MpuRegionCfg::regionId |
Region number to configure. Range: 0 to (SDL_ARM_R5F_MPU_REGIONS_MAX 1U)
uint32_t SDL_ArmR5MpuRegionCfg::enable |
Region enable control. 0: Memory region disabled. 1: Memory region enabled.
uint32_t SDL_ArmR5MpuRegionCfg::baseAddr |
Region base address: 32 bytes aligned.
SDL_ArmR5MpuRegionSize SDL_ArmR5MpuRegionCfg::size |
Region size Refer SDL_ArmR5MpuRegionSize
uint32_t SDL_ArmR5MpuRegionCfg::subRegionEnable |
Sub-region enable See SDL_ArmR5SubRegionDisable for details. Multiple sub-regions can disabled by ORing multiple masks from above
uint32_t SDL_ArmR5MpuRegionCfg::exeNeverControl |
Region execute control. 0: all instruction fetches enabled 1: no instruction fetches enabled
uint32_t SDL_ArmR5MpuRegionCfg::accessPermission |
Access permissions See SDL_ArmR5AccessPerm for more details
uint32_t SDL_ArmR5MpuRegionCfg::shareable |
Region share attribute. 0: non-shared 1: shared
uint32_t SDL_ArmR5MpuRegionCfg::cacheable |
Region cache control. FALSE: Memory region is non-cached. TRUE: Memory region is cached.
uint32_t SDL_ArmR5MpuRegionCfg::cachePolicy |
Inner and outer cache policy. This field is valid only if cacheable = TRUE See SDL_ArmR5CachePolicy for more details
uint32_t SDL_ArmR5MpuRegionCfg::memAttr |
Memory region attributes. This field is valid only if cacheable = FALSE See SDL_ArmR5MemAttr for more details