POK Configuration structure.
Definition: sdl_pok_def.h:478
int32_t SDL_porSetControl(SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_pokPorCfg_t *pPorCfg)
write the POR configuration for the specified POK control register
POK functionality of POR Configuration structure.
Definition: sdl_pok_def.h:525
SDL_wkup_ctrl_mmr_cfg0Regs SDL_wkupCtrlRegsBase_t
Definition: sdl_pok_def.h:407
int32_t SDL_pokSetControl(SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_POK_config *pPokCfg, SDL_POK_Inst instance)
write the POK configuration for the specified POK control register
void sdlGetErrSig(uint32_t id, SDL_POK_Inst *instance, uint32_t *esm_err_sig, bool *usePorCfgFlag)
int32_t SDL_pok_GetShiftsAndMasks(SDL_wkupCtrlRegsBase_t *pBaseAddress, SDL_POK_Inst instance, SDL_pokShiftsAndMasks_t *pShMasks)
Header file containing various enumerations, structure definitions and function declarations for the ...
int8_t SDL_POK_Inst
Definition: sdl_pok_def.h:420
int32_t SDL_pokGetControl(SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_POK_config *pPokCfg, SDL_pokVal_t *pPokVal, SDL_POK_Inst instance)
Read the POK configuration for the specified POK control register.
POK Configuration structure read value.
Definition: sdl_pok_def.h:500
Definition: sdl_pok_def.h:74