![]() |
SDL API Guide for J721E
|
Header file containing various enumerations, structure definitions and function declarations for the Power System modules such as POK/POR IP.
Go to the source code of this file.
POK types | |
This enumerator defines the possible POK module types | |
#define | SDL_TYPE_POK ((SDL_pok_type) 1U) |
#define | SDL_TYPE_POK_SA ((SDL_pok_type) 2U) |
typedef uint8_t | SDL_pok_type |
POK/POR hysteresIs types | |
This enumerator defines the possible hysteresis control values for the Power Subsystem modules | |
#define | SDL_PWRSS_SET_HYSTERESIS_DISABLE ((SDL_pwrss_hysteresis) 0U) |
#define | SDL_PWRSS_SET_HYSTERESIS_ENABLE ((SDL_pwrss_hysteresis) 1U) |
#define | SDL_PWRSS_GET_HYSTERESIS_VALUE ((SDL_pwrss_hysteresis) 2U) |
#define | SDL_PWRSS_HYSTERESIS_NO_ACTION ((SDL_pwrss_hysteresis) 3U) |
typedef uint8_t | SDL_pwrss_hysteresis |
POK/POR TRIM values | |
This enumerator defines the possible trim value for POK/POR modules Any value between 0 through 127 is valid TRIM value ------------------------------------------------------------------------— * * POK | Under Voltage | Over Voltage | * | Detection | Detection | Step Resolution * ----------- | --------------- | ---------------- | ---------------- * CORE_POK | 475mV - 1.35V | 725mV - 1.65V | 0.0125V * POK1.8 | 1.432V - 2.168V | 1.432V - 2.168V | 0.02V * POK3.3 | 2.625V - 3.975V | 2.625V - 3.975V | 0.0375V * * | |
#define | SDL_PWRSS_MAX_TRIM_VALUE ((SDL_pwrss_trim) 127U) |
#define | SDL_PWRSS_TRIM_NO_ACTION ((SDL_pwrss_trim) 128U) |
#define | SDL_PWRSS_GET_TRIM_VALUE ((SDL_pwrss_trim) 129U) |
#define | SDL_PWRSS_INVALID_TRIM_VALUE ((SDL_pwrss_trim) 255U) |
typedef uint8_t | SDL_pwrss_trim |
POK/POR Voltage detection modes | |
This enumerator defines the possible values of Voltage Detection modes | |
#define | SDL_PWRSS_SET_UNDER_VOLTAGE_DET_ENABLE ((SDL_pwrss_vd_mode) 0U) |
#define | SDL_PWRSS_SET_OVER_VOLTAGE_DET_ENABLE ((SDL_pwrss_vd_mode) 1U) |
#define | SDL_PWRSS_GET_VOLTAGE_DET_MODE ((SDL_pwrss_vd_mode) 2U) |
#define | SDL_PWRSS_VOLTAGE_DET_NO_ACTION ((SDL_pwrss_vd_mode) 3U) |
typedef uint8_t | SDL_pwrss_vd_mode |
POK detection status | |
This enumerator defines the POK Detection status values | |
#define | SDL_POK_DETECTION_DISABLED ((SDL_POK_detection_status) 0U) |
#define | SDL_POK_DETECTION_ENABLED ((SDL_POK_detection_status) 1U) |
typedef uint8_t | SDL_POK_detection_status |
POK detection values | |
This enumerator defines the POK Detection values | |
#define | SDL_POK_DETECTION_DISABLE ((SDL_POK_detection) 0U) |
#define | SDL_POK_DETECTION_ENABLE ((SDL_POK_detection) 1U) |
#define | SDL_POK_DETECTION_NO_ACTION ((SDL_POK_detection) 2U) |
#define | SDL_POK_GET_DETECTION_VALUE ((SDL_POK_detection) 3U) |
typedef uint8_t | SDL_POK_detection |
POK Enable Selection source Values | |
This enumerator defines the POK Enable selection source | |
#define | SDL_POK_ENSEL_HWTIEOFFS ((SDL_POK_enSelSrc) 0U) |
#define | SDL_POK_ENSEL_PRG_CTRL ((SDL_POK_enSelSrc) 1U) |
#define | SDL_POK_ENSEL_NO_ACTION ((SDL_POK_enSelSrc) 2U) |
#define | SDL_POK_GET_ENSEL_VALUE ((SDL_POK_enSelSrc) 3U) |
typedef uint8_t | SDL_POK_enSelSrc |
POK voltage threshold status | |
This enumerator defines the Voltage threshold status | |
#define | SDL_VOLTAGE_ABOVE_THRESHOLD ((SDL_POK_thrStatus) 0U) |
#define | SDL_VOLTAGE_BELOW_THRESHOLD ((SDL_POK_thrStatus) 1U) |
#define | SDL_VOLTAGE_GOOD ((SDL_POK_thrStatus) 2U) |
typedef uint8_t | SDL_POK_thrStatus |
POK trim selection values from HHV default or CTRL registers | |
This enumerator defines the trim selection values | |
#define | SDL_POR_TRIM_SELECTION_FROM_HHV_DEFAULT ((uint8_t) 0U) |
#define | SDL_POR_TRIM_SELECTION_FROM_CTRL_REGS ((uint8_t) 1U) |
#define | SDL_POR_TRIM_SELECTION_NO_CHANGE ((uint8_t) 2U) |
#define | SDL_POR_TRIM_SELECTION_GET_VALUE ((uint8_t) 3U) |
typedef uint8_t | SDL_por_trim_sel |
POR POR Override enable and set | |
This enumerator defines the override enable/set values | |
#define | SDL_POR_OVERRIDE_NOT_SET_DISABLE ((SDL_por_override) 0U) |
#define | SDL_POR_OVERRIDE_NOT_SET_ENABLE ((SDL_por_override) 1U) |
#define | SDL_POR_OVERRIDE_SET_DISABLE ((SDL_por_override) 2U) |
#define | SDL_POR_OVERRIDE_SET_ENABLE ((SDL_por_override) 3U) |
#define | SDL_POR_GET_OVERRIDE_VALUE ((SDL_por_override) 4U) |
#define | SDL_POR_SET_OVERRIDE_NO_CHANGE ((SDL_por_override) 5U) |
#define | SDL_OVERRIDE_SET_UNKNOWN ((SDL_por_override) 0xFFU) |
typedef uint8_t | SDL_por_override |
POR Module state values | |
This enumerator defines the POR Module State | |
#define | SDL_POR_MODULE_STATUS_FUNCTIONAL_MODE ((SDL_por_module_status) 0U) |
#define | SDL_POR_MODULE_STATUS_RESET_MODE ((SDL_por_module_status) 1U) |
typedef uint8_t | SDL_por_module_status |
POK POK ID values | |
This enumerator defines the possible POK module ID values on J721E | |
#define | SDL_FIRST_POK_ID (0) |
#define | SDL_POK_VDDA_PMIC_IN_ID (SDL_FIRST_POK_ID) |
#define | SDL_POK_VDD_CORE_UV_ID (1) |
#define | SDL_POK_VDDSHV_WKUP_GEN_UV_ID (2) |
#define | SDL_POK_VDD_CPU_UV_ID (3) |
#define | SDL_POK_VDDR_MCU_UV_ID (4) |
#define | SDL_POK_VMON_EXT_UV_ID (5) |
#define | SDL_POK_VDD_MCU_OV_ID (6) |
#define | SDL_POK_VDDR_CORE_UV_ID (7) |
#define | SDL_POK_VDDSHV_WKUP_GEN_OV_ID (8) |
#define | SDL_POK_VDD_CORE_OV_ID (9) |
#define | SDL_POK_VDDR_MCU_OV_ID (10) |
#define | SDL_POK_VDD_CPU_OV_ID (11) |
#define | SDL_POK_VDDR_CORE_OV_ID (12) |
#define | SDL_POK_VMON_EXT_OV_ID (13) |
#define | SDL_POR_POKHV_UV_ID (14) |
#define | SDL_POR_POKLV_UV_ID (15) |
#define | SDL_POR_POKHV_OV_ID (16) |
#define | SDL_LAST_POK_ID (SDL_POR_POKHV_OV_ID) |
typedef SDL_wkup_ctrl_mmr_cfg0Regs | SDL_wkupCtrlRegsBase_t |
typedef int8_t | SDL_POK_Inst |
Data Structures | |
struct | SDL_pokShiftsAndMasks_t |
struct | SDL_POK_config |
POK Configuration structure. More... | |
struct | SDL_pokVal_t |
POK Configuration structure read value. More... | |
struct | SDL_pokPorCfg_t |
POK functionality of POR Configuration structure. More... | |
struct | SDL_pokPorVal_t |
POK functionality of POR Value structure. More... | |
struct | SDL_pokPorStat_t |
POK functionality of POR Configuration structure. More... | |
Macros | |
POR POR Override index | |
#define | SDL_PORHV_OVERRIDE_INDEX (0U) |
#define | SDL_BGAP_OVERRIDE_INDEX (1U) |
#define | SDL_POKHV_OVERRIDE_INDEX (2U) |
#define | SDL_POKLVA_OVERRIDE_INDEX (3U) |
#define | SDL_POKLVB_OVERRIDE_INDEX (4U) |
#define | SDL_MAX_OVERRIDE_INDEX (5U) |