Go to the source code of this file.
|
void | sdlGetErrSig (uint32_t id, SDL_POK_Inst *instance, uint32_t *esm_err_sig, bool *usePorCfgFlag) |
|
int32_t | SDL_pok_GetShiftsAndMasks (SDL_wkupCtrlRegsBase_t *pBaseAddress, SDL_POK_Inst instance, SDL_pokShiftsAndMasks_t *pShMasks) |
|
int32_t | SDL_pokSetControl (SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_POK_config *pPokCfg, SDL_POK_Inst instance) |
| write the POK configuration for the specified POK control register More...
|
|
int32_t | SDL_pokGetControl (SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_POK_config *pPokCfg, SDL_pokVal_t *pPokVal, SDL_POK_Inst instance) |
| Read the POK configuration for the specified POK control register. More...
|
|
int32_t | SDL_porSetControl (SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_pokPorCfg_t *pPorCfg) |
| write the POR configuration for the specified POK control register More...
|
|
◆ sdlGetErrSig()
void sdlGetErrSig |
( |
uint32_t |
id, |
|
|
SDL_POK_Inst * |
instance, |
|
|
uint32_t * |
esm_err_sig, |
|
|
bool * |
usePorCfgFlag |
|
) |
| |
◆ SDL_pok_GetShiftsAndMasks()