![]() |
SDL API Guide for J721E
|
Functions | |
int32_t | SDL_ecc_aggrGetRevision (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t *pRev) |
int32_t | SDL_ecc_aggrGetNumRams (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t *pNumRams) |
int32_t | SDL_ecc_aggrReadEccRamReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t *pRegVal) |
int32_t | SDL_ecc_aggrReadEccRamWrapRevReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t *pRegVal) |
int32_t | SDL_ecc_aggrReadEccRamCtrlReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t *pRegVal) |
int32_t | SDL_ecc_aggrReadEccRamErrCtrlReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t *pRegVal) |
int32_t | SDL_ecc_aggrReadEccRamErrStatReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t *pRegVal) |
int32_t | SDL_ecc_aggrWriteEccRamReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t val) |
int32_t | SDL_ecc_aggrWriteEccRamCtrlReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t val) |
int32_t | SDL_ecc_aggrWriteEccRamErrCtrlReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t val) |
int32_t | SDL_ecc_aggrWriteEccRamErrStatReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t val) |
int32_t | SDL_ecc_aggrConfigEccRam (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEnable, bool bEccCheck, bool bEnableRMW) |
int32_t | SDL_ecc_aggrVerifyConfigEccRam (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEnable, bool bEccCheck, bool bEnableRMW) |
int32_t | SDL_ecc_aggrGetEccRamErrorStatus (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrEccRamErrorStatusInfo *pEccErrorStatus) |
int32_t | SDL_ecc_aggrForceEccRamError (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, const SDL_Ecc_AggrErrorInfo *pEccForceError) |
int32_t | SDL_ecc_aggrReadEDCInterconnectReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t *pRegVal) |
int32_t | SDL_ecc_aggrWriteEDCInterconnectReg (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t val) |
int32_t | SDL_ecc_aggrConfigEDCInterconnect (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEccCheck) |
int32_t | SDL_ecc_aggrVerifyConfigEDCInterconnect (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEccCheck) |
int32_t | SDL_ecc_aggrGetEDCInterconnectErrorStatus (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrEDCInterconnectErrorStatusInfo *pEccErrorStatus) |
int32_t | SDL_ecc_aggrForceEDCInterconnectError (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, const SDL_Ecc_AggrEDCInterconnectErrorInfo *pEccForceError) |
int32_t | SDL_ecc_aggrAckIntr (SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc) |
int32_t | SDL_ecc_aggrIsEccRamIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, bool *pIsPend) |
int32_t | SDL_ecc_aggrSetEccRamIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc) |
int32_t | SDL_ecc_aggrSetEccRamNIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, uint32_t numEvents) |
int32_t | SDL_ecc_aggrClrEccRamIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc) |
int32_t | SDL_ecc_aggrClrEccRamNIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, uint32_t numEvents) |
int32_t | SDL_ecc_aggrIsEDCInterconnectIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, bool *pIsPend) |
int32_t | SDL_ecc_aggrSetEDCInterconnectNIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, SDL_Ecc_AggrEDCErrorSubType subType, uint32_t numEvents) |
int32_t | SDL_ecc_aggrClrEDCInterconnectNIntrPending (SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, SDL_Ecc_AggrEDCErrorSubType subType, uint32_t numEvents) |
int32_t | SDL_ecc_aggrIsIntrPending (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, bool *pIsPend) |
int32_t | SDL_ecc_aggrIsAnyIntrPending (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool *pIsPend) |
int32_t | SDL_ecc_aggrEnableIntr (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc) |
int32_t | SDL_ecc_aggrDisableIntr (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc) |
int32_t | SDL_ecc_aggrEnableAllIntr (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId) |
int32_t | SDL_ecc_aggrDisableAllIntr (const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId) |
int32_t | SDL_ecc_aggrEnableIntrs (const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc) |
int32_t | SDL_ecc_aggrDisableIntrs (const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc) |
int32_t | SDL_ecc_aggrEnableAllIntrs (const SDL_ecc_aggrRegs *pEccAggrRegs) |
int32_t | SDL_ecc_aggrDisableAllIntrs (const SDL_ecc_aggrRegs *pEccAggrRegs) |
int32_t | SDL_ecc_aggrReadStaticRegs (SDL_ecc_aggrRegs *pEccAggrRegs, SDL_ECC_staticRegs *pEccAggrStaticRegs) |
int32_t | SDL_ecc_aggrIntrEnableCtrl (SDL_ecc_aggrRegs *pEccAggrRegs, const SDL_ecc_aggrEnableCtrl *pEnableCtrl) |
int32_t | SDL_ecc_aggrIntrStatusCtrl (SDL_ecc_aggrRegs *pEccAggrRegs, const SDL_ecc_aggrStatusCtrl *pStatusCtrl) |
int32_t | SDL_ecc_aggrIntrGetStatus (const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_ecc_aggrStatusCtrl *pStatusCtrl) |
int32_t SDL_ecc_aggrGetRevision | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t * | pRev | ||
) |
SDL_ecc_aggrGetRevision
Description
This function returns the revision information for the ECC Aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
pRev A pointer (of type uint32_t) to hold the rev ID value of the ECC Aggregator module Revision information. See design specification for details.
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrGetNumRams | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t * | pNumRams | ||
) |
SDL_ecc_aggrGetNumRams
Description
This function returns the number of RAMs serviced by this ECC Aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
pNumRams A pointer (of type uint32_t) to hold the value of number of RAMs serviced by this ECC Aggregator
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrReadEccRamReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | regOffset, | ||
uint32_t * | pRegVal | ||
) |
SDL_ecc_aggrReadEccRamReg
Description
This function reads the specified ECC wrapper register from the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
regOffset Byte offset of the ECC wrapper register to read (must be in the range of 0x10..0x24)
pRegVal A pointer (of uint32_t) to hold the value of the specified ECC wrapper register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the arguments such as ramId and/or regOffset are invalid
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrReadEccRamWrapRevReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t * | pRegVal | ||
) |
SDL_ecc_aggrReadEccRamWrapRevReg
Description
This function reads the ECC wrapper revision register from the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
pRegVal A pointer (of type uint32_t) to hold the value of the ECC wrapper revision register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrReadEccRamCtrlReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t * | pRegVal | ||
) |
SDL_ecc_aggrReadEccRamCtrlReg
Description
This function reads the specified ECC wrapper control register from the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
pRegVal A pointer (of type uint32_t) to hold the value of the ECC control register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrReadEccRamErrCtrlReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | instSelect, | ||
uint32_t * | pRegVal | ||
) |
SDL_ecc_aggrReadEccRamErrCtrlReg
Description
This function reads the specified ECC wrapper error control register from the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
instSelect Instance selector (0..1) of the specified register to read
pRegVal A pointer (of type uint32_t) to hold the value of the ECC Error control register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
int32_t SDL_ecc_aggrReadEccRamErrStatReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | instSelect, | ||
uint32_t * | pRegVal | ||
) |
SDL_ecc_aggrReadEccRamErrStatReg
Description
This function reads the specified ECC wrapper error status register from the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
instSelect Instance selector (0..1) of the specified register to read
pRegVal A pointer (of type uint32_t) to hold the value of the ECC error status register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
int32_t SDL_ecc_aggrWriteEccRamReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | regOffset, | ||
uint32_t | val | ||
) |
SDL_ecc_aggrWriteEccRamReg
Description
This function writes a value into the specified ECC wrapper register in the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
regOffset Byte offset of the ECC wrapper register to write (must be in the range of 0x10..0x24)
val The 32-bit value to write into the register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrWriteEccRamCtrlReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | val | ||
) |
SDL_ecc_aggrWriteEccRamCtrlReg
Description
This function write a value into the ECC wrapper control register in the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
val The 32-bit value to write into the register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrWriteEccRamErrCtrlReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | instSelect, | ||
uint32_t | val | ||
) |
SDL_ecc_aggrWriteEccRamErrCtrlReg
Description
This function writes a value into the specified ECC wrapper error control register in the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
instSelect Instance selector (0..1) of the specified register to write
val The 32-bit value to write into the register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrWriteEccRamErrStatReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | instSelect, | ||
uint32_t | val | ||
) |
SDL_ecc_aggrWriteEccRamErrStatReg
Description
This function write a value into the specified ECC wrapper error status register in the specific ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
instSelect Instance selector (0..1) of the specified register to write
val The 32-bit value to write into the register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrConfigEccRam | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
bool | bEnable, | ||
bool | bEccCheck, | ||
bool | bEnableRMW | ||
) |
SDL_ecc_aggrConfigEccRam
Description
This function is used to configure the ECC capabilities of the specified ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
bEnable If true, then enable ECC generation. ECC is completely bypassed if both fEnable and fEccCheck are 0.
bEccCheck If true, then enable ECC check. ECC is completely bypassed if both fEnable and fEccCheck are 0.
bfEnableRMW If true, then enable read-modify-write on partial word writes
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrVerifyConfigEccRam | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
bool | bEnable, | ||
bool | bEccCheck, | ||
bool | bEnableRMW | ||
) |
SDL_ecc_aggrVerifyConfigEccRam
Description
This function is used to verify the configure the ECC capabilities of the specified ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
bEnable If true, then enable ECC generation. ECC is completely bypassed if both fEnable and fEccCheck are 0.
bEccCheck If true, then enable ECC check. ECC is completely bypassed if both fEnable and fEccCheck are 0.
bfEnableRMW If true, then enable read-modify-write on partial word writes
Return Value
SDL_PASS Success, indicates the configuration is successful
SDL_EFAIL Failure, indicates the expected configuration failed
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
SDL_ecc_aggrConfigEccRam() is called previously with the same arguments
Post Condition
None
int32_t SDL_ecc_aggrGetEccRamErrorStatus | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrEccRamErrorStatusInfo * | pEccErrorStatus | ||
) |
SDL_ecc_aggrGetEccRamErrorStatus
Description
This function is used to get the error status of the specified ECC Wrapper type RAM id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
pEccErrorStatus A pointer to a SDL_Ecc_AggrEccRamErrorStatusInfo structure containing returned error information
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrForceEccRamError | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
const SDL_Ecc_AggrErrorInfo * | pEccForceError | ||
) |
SDL_ecc_aggrForceEccRamError
Description
This function is used to force an ECC error on the specified ECC Wrapper type RAM id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
pEccForceError A pointer to a SDL_Ecc_AggrErrorInfo structure containing force error information
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrReadEDCInterconnectReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | regOffset, | ||
uint32_t * | pRegVal | ||
) |
SDL_ecc_aggrReadEDCInterconnectReg
Description
This function reads the specified EDC interconnect register for the specific Interconnect RAM Id
Arguments
SDL_ecc_aggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
regOffset Byte offset of the ECC wrapper register to read (must be in the range of 0x10..0x24)
pRegVal A pointer (of uint32_t) to hold the value of the specified EDC Interconnect register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the arguments such as ramId and/or regOffset are invalid
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrWriteEDCInterconnectReg | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
uint32_t | regOffset, | ||
uint32_t | val | ||
) |
SDL_ecc_aggrWriteEDCInterconnectReg
Description
This function writes a value into the specified EDC Interconnect register in the specific Interconnect RAM Id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
regOffset Byte offset of the EDC Interconnect register to write (must be in the range of 0x10..0x24)
val The 32-bit value to write into the register
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrConfigEDCInterconnect | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
bool | bEccCheck | ||
) |
SDL_ecc_aggrConfigEDCInterconnect
Description
This function is used to configure the EDC control capabilities of the specified Interconnect RAM Id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
bEccCheck If true, then enable ECC check.
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrVerifyConfigEDCInterconnect | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
bool | bEccCheck | ||
) |
SDL_ecc_aggrVerifyConfigEDCInterconnect
Description
This function is used to verify the configure the ECC capabilities of the specified Interconnect RAM Id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
bEccCheck If true, then enable ECC check.
Return Value
SDL_PASS Success, indicates the configuration is successful
SDL_EFAIL Failure, indicates the expected configuration failed
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
SDL_ecc_aggrConfigEDCInterconnect() is called previously with the same arguments
Post Condition
None
int32_t SDL_ecc_aggrGetEDCInterconnectErrorStatus | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrEDCInterconnectErrorStatusInfo * | pEccErrorStatus | ||
) |
SDL_ecc_aggrGetEDCInterconnectErrorStatus
Description
This function is used to get the error status of the specified Interconnect RAM Id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
pEccErrorStatus A pointer to a SDL_Ecc_AggrEDCInterconnectErrorStatusInfo structure containing returned error information
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrForceEDCInterconnectError | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
const SDL_Ecc_AggrEDCInterconnectErrorInfo * | pEccForceError | ||
) |
SDL_ecc_aggrForceEDCInterconnectError
Description
This function is used to force an ECC error on the specified Interconnect RAM Id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
pEccForceError A pointer to a SDL_Ecc_AggrEDCInterconnectErrorInfo structure containing force error information
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrAckIntr | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
SDL_Ecc_AggrIntrSrc | intrSrc | ||
) |
SDL_ecc_aggrAckIntr
Description
This function is used to acknowledged a pending interrupt and to send the next interrupt to the host
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT) to acknowledge
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrIsEccRamIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc, | ||
bool * | pIsPend | ||
) |
SDL_ecc_aggrIsEccRamIntrPending
Description
This function returns the pending interrupt status of the specified interrupt source from the specified ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT, SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT, or SDL_ECC_ADDR_ERROR_TYPE_SUCCESSIVE_SINGLE_BITS)
pIsPend A Pointer (of type bool) to hold the state as below true An interrupt of the specified type is pending false An interrupt of the specified type is not pending, or the ramId and/or intrSrc arguments are invalid
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrSetEccRamIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc | ||
) |
SDL_ecc_aggrSetEccRamIntrPending
Description
This function is used to forceably set the pending status of the specified interrupt source on the specified ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT, SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT, or SDL_ECC_ADDR_ERROR_TYPE_SUCCESSIVE_SINGLE_BITS)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrSetEccRamNIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc, | ||
uint32_t | numEvents | ||
) |
SDL_ecc_aggrSetEccRamNIntrPending
Description
This function is used to forceably set the pending status of the specified interrupt source on the specified ECC RAM Note that multiple events can be triggerred in one call.
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT, SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT, or SDL_ECC_ADDR_ERROR_TYPE_SUCCESSIVE_SINGLE_BITS)
numEvents 1 - 3 are valid number of events to set; 0 or > 3 invalid.
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrClrEccRamIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc | ||
) |
SDL_ecc_aggrClrEccRamIntrPending
Description
This function is used to clear the pending status of the specified interrupt source on the specified ECC RAM
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT, SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT, or SDL_ECC_ADDR_ERROR_TYPE_SUCCESSIVE_SINGLE_BITS)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrClrEccRamNIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc, | ||
uint32_t | numEvents | ||
) |
SDL_ecc_aggrClrEccRamIntrPending
Description
This function is used to clear the pending status of the specified interrupt source on the specified ECC RAM Note that multiple events can be cleared in one call.
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT, SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT, or SDL_ECC_ADDR_ERROR_TYPE_SUCCESSIVE_SINGLE_BITS)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrIsEDCInterconnectIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc, | ||
bool * | pIsPend | ||
) |
SDL_ecc_aggrIsEDCInterconnectIntrPending
Description
This function returns the pending interrupt status of the specified interrupt source from the specified Interconnect RAM Id
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
pIsPend A Pointer (of type bool) to hold the state as below true An interrupt of the specified type is pending false An interrupt of the specified type is not pending, or the ramId and/or intrSrc arguments are invalid
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrSetEDCInterconnectNIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc, | ||
SDL_Ecc_AggrEDCErrorSubType | subType, | ||
uint32_t | numEvents | ||
) |
SDL_ecc_aggrSetEDCInterconnectNIntrPending
Description
This function is used to forceably set the pending status of the specified interrupt source on the specified Interconnect RAM Id. Note that multiple events can be triggerred in one call.
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
subType Specify inject error events or normal error events.
numEvents 1 - 3 are valid number of events to set; 0 or > 3 invalid.
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrClrEDCInterconnectNIntrPending | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc, | ||
SDL_Ecc_AggrEDCErrorSubType | subType, | ||
uint32_t | numEvents | ||
) |
SDL_ecc_aggrClrEDCInterconnectNIntrPending
Description
This function is used to clear the pending status of the specified interrupt source on the specified Interconnect RAM Id Note that multiple events can be cleared in one call.
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
subType Specify inject error events or normal error events.
numEvents 1 - 3 are valid number of events to clear;0 or > 3 invalid.
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrIsIntrPending | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc, | ||
bool * | pIsPend | ||
) |
SDL_ecc_aggrIsIntrPending
Description
This function returns the pending interrupt status for the specified ECC interrupt source from the ECC RAM specified by ramId.
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT; valid only for the SDL_ecc_aggrIsIntrPending function)
pIsPend A pointer (of type bool) to hold the status as below true An interrupt of the specified type is pending false An interrupt of the specified type is not pending, or the ramId and/or intrSrc arguments are invalid
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrIsAnyIntrPending | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
bool * | pIsPend | ||
) |
SDL_ecc_aggrIsAnyIntrPending
Description
This function returns the pending interrupt status for any interrupt source from the ECC RAM specified by ramId.
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrEnableIntr | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc | ||
) |
SDL_ecc_aggrEnableIntr
Description
This function enables the interrupt for the specified interrupt source on the RAM specified by ramId
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrDisableIntr | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId, | ||
SDL_Ecc_AggrIntrSrc | intrSrc | ||
) |
SDL_ecc_aggrDisableIntr
Description
This function disables the interrupt for the specified interrupt source on the RAM specified by ramId
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicate the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrEnableAllIntr | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId | ||
) |
SDL_ecc_aggrEnableAllIntr
Description
This function enables the interrupts for all of the available interrupt sources on the RAM specified by ramId
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrDisableAllIntr | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
uint32_t | ramId | ||
) |
SDL_ecc_aggrDisableAllIntr
Description
This function disables the interrupts for all of the available interrupt sources on the RAM specified by ramId
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
ramId RAM identifier (0..SDL_ecc_aggrGetNumRams()-1)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrEnableIntrs | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
SDL_Ecc_AggrIntrSrc | intrSrc | ||
) |
SDL_ecc_aggrEnableIntrs
Description
This function enables the interrupt for the specified interrupt source on all ECC RAMs serviced by this aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrDisableIntrs | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
SDL_Ecc_AggrIntrSrc | intrSrc | ||
) |
SDL_ecc_aggrDisableIntrs
Description
This function disables the interrupts for the specified interrupt source on all ECC RAMs serviced by this aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
intrSrc The interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrEnableAllIntrs | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs | ) |
SDL_ecc_aggrEnableAllIntrs
Description
This function enables the interrupts for all of the available interrupt sources on all ECC RAMs serviced by this aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrDisableAllIntrs | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs | ) |
SDL_ecc_aggrDisableAllIntrs
Description
This function disables the interrupts for all of the available interrupt sources on all ECC RAMs serviced by this aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrReadStaticRegs | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
SDL_ECC_staticRegs * | pEccAggrStaticRegs | ||
) |
SDL_ecc_aggrReadStaticRegs
Description
This function reads the static registers for ECC aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
pEccAggrStaticRegs A pointer (of type SDL_ECC_staticRegs*) to hold the static register values
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrIntrEnableCtrl | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
const SDL_ecc_aggrEnableCtrl * | pEnableCtrl | ||
) |
SDL_ecc_aggrIntrEnableCtrl
Description
This function reads the static registers for ECC aggregator
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
pEnableCtrl A pointer (of type SDL_ecc_aggrEnableCtrl*) to hold the interrupt enable control values
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrIntrStatusCtrl | ( | SDL_ecc_aggrRegs * | pEccAggrRegs, |
const SDL_ecc_aggrStatusCtrl * | pStatusCtrl | ||
) |
SDL_ecc_aggrIntrStatusCtrl
Description
This function writes the ECC Aggregator Status registers for timeout and parity count values
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
pStatusCtrl A pointer (of type SDL_ecc_aggrStatusCtrl*) to hold the interrupt status control and count values
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None
int32_t SDL_ecc_aggrIntrGetStatus | ( | const SDL_ecc_aggrRegs * | pEccAggrRegs, |
SDL_ecc_aggrStatusCtrl * | pStatusCtrl | ||
) |
SDL_ecc_aggrIntrGetStatus
Description
This function reads the ECC Aggregator Status registers for timeout and parity count values
Arguments
pEccAggrRegs A pointer (of type SDL_ecc_aggrRegs*) to the base address of the ECC Aggregator module
pStatusCtrl A pointer (of type SDL_ecc_aggrStatusCtrl*) to read the timeout and parity count values
Return Value
SDL_PASS Success
SDL_EBADARGS Failure, indicates the bad input arguments
Pre Condition
None
Post Condition
None