![]() |
SDL API Guide for J721E
|
This structure contains error forcing information used by the SDL_ecc_aggrForceEDCInterconnectError function.
Design: PROC_SDL-1277
Data Fields | |
SDL_Ecc_AggrIntrSrc | intrSrc |
uint32_t | eccGroup |
uint32_t | eccBit1 |
uint32_t | eccBit2 |
bool | bNextBit |
uint32_t | eccPattern |
SDL_Ecc_AggrIntrSrc SDL_Ecc_AggrEDCInterconnectErrorInfo::intrSrc |
Identifies the interrupt source (SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT or SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT)
uint32_t SDL_Ecc_AggrEDCInterconnectErrorInfo::eccGroup |
The EDC has a number of checker groups. Each group uses a set of parameters like checker type, bus width, parity width, bus name and number of bits. This parameter indicates a particular checker group where the error will be injected. Please refer to TRM for the different checkers implemented in an SOC
uint32_t SDL_Ecc_AggrEDCInterconnectErrorInfo::eccBit1 |
Bit position of SEC starting from LSB or 1st bit position starting from LSB for DED.
uint32_t SDL_Ecc_AggrEDCInterconnectErrorInfo::eccBit2 |
2nd bit position starting from LSB for DED to inject error.
bool SDL_Ecc_AggrEDCInterconnectErrorInfo::bNextBit |
Increment bit location for next injection.
uint32_t SDL_Ecc_AggrEDCInterconnectErrorInfo::eccPattern |
ECC pattern for error injection.