![]() |
PDK API Guide for J721E
|
data types definitions for ipc module.
Go to the source code of this file.
IPC Error Codes | |
Error codes returned by IPC APIs | |
#define | IPC_SOK (CSL_PASS) |
API call successful. More... | |
#define | IPC_EFAIL (CSL_EFAIL) |
API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure. More... | |
#define | IPC_EBADARGS (CSL_EBADARGS) |
API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected. More... | |
#define | IPC_EINVALID_PARAMS (CSL_EINVALID_PARAMS) |
API call returned with error as invalid parameters. Typically when parameters passed are not valid. More... | |
#define | IPC_ETIMEOUT (CSL_ETIMEOUT) |
API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period. More... | |
#define | IPC_EALLOC (CSL_EALLOC) |
API call returned with error as allocation failed. More... | |
#define | IPC_EUNSUPPORTED (CSL_EUNSUPPORTED_CMD) |
Un Supported service request, API/IOCTLs. More... | |
#define | IPC_E_UNBLOCKED (-50) |
IPC is unblocked mode. More... | |
#define | IPC_INTR_INVALID (0xFFFF0000U) |
Macro used to specify that interrupt number is invalid. More... | |
#define | IPC_RPMESSAGE_TIMEOUT_FOREVER ~(0) |
Timeout foreever for IPC Recv. More... | |
#define | RPMESSAGE_ANY (0xFFFFFFFFU) |
RPMessage Endpoint any available. More... | |
#define | RPMESSAGE_ALL (0xFFFFFFFFU) |
RPMessage type. More... | |
typedef void(* | Ipc_OsalHIsrFxn) (uintptr_t arg0, uintptr_t arg1) |
IPC OSAL High Level ISR type. More... | |
typedef void * | Ipc_OsalHIsrGateHandle |
High Level ISR handle. More... | |
typedef uint32_t(* | Ipc_VirtToPhyFxn) (const void *virtAddr) |
IPC Virtual to Physical address translation callback function. More... | |
typedef void *(* | Ipc_PhyToVirtFxn) (uint32_t phyAddr) |
IPC Physical to Virtual address translation callback function. More... | |
typedef void(* | Ipc_PrintFxn) (const char *str) |
IPC info/debug print function prototype. More... | |
typedef uintptr_t(* | Ipc_OsalDisableAllIntrFxn) (void) |
IPC OSAL interrupt disable function prototype. More... | |
typedef void(* | Ipc_OsalRestoreAllIntrFxn) (uintptr_t cookie) |
IPC OSAL interrupt restore function prototype. More... | |
typedef Ipc_OsalHIsrGateHandle(* | Ipc_OsalCreateHIsrMutexFxn) (void) |
IPC OSAL create high level interrupt lock. More... | |
typedef void(* | Ipc_OsalDeleteHIsrMutexFxn) (Ipc_OsalHIsrGateHandle *handle) |
IPC OSAL delete high level interrupt lock. More... | |
typedef int32_t(* | Ipc_OsalEnterHIsrMutexFxn) (Ipc_OsalHIsrGateHandle handle) |
IPC OSAL Lock High level ISR's. More... | |
typedef void(* | Ipc_OsalExitHIsrMutexFxn) (Ipc_OsalHIsrGateHandle handle, int32_t key) |
IPC OSAL Un Lock High level ISR's. More... | |
typedef void *(* | Ipc_OsalMutexCreateFxn) (void) |
IPC OSAL mutex create function prototype to protect critical section. More... | |
typedef void(* | Ipc_OsalMutexDeleteFxn) (void *mutexHandle) |
IPC OSAL mutex delete function prototype. More... | |
typedef int32_t(* | Ipc_OsalMutexLockFxn) (void *mutexHandle, uint32_t timeout) |
IPC OSAL mutex lock function prototype. More... | |
typedef void(* | Ipc_OsalMutexUnlockFxn) (void *mutexHandle) |
IPC OSAL mutex lock function prototype. More... | |
typedef int32_t(* | Ipc_OsalHIsrCreateFxn) (Ipc_OsalHIsrHandle *handle, Ipc_OsalHIsrFxn fxn, void *arg) |
IPC OSAL create high level interrupt handler. More... | |
typedef void(* | Ipc_OsalHIsrDeleteFxn) (Ipc_OsalHIsrHandle *handle) |
IPC OSAL delete high level interrupt handler. More... | |
typedef int32_t(* | Ipc_OsalHIsrPostFxn) (Ipc_OsalHIsrHandle *handle) |
IPC OSAL Lock High level ISR's. More... | |
typedef void(* | Ipc_OsalIsrFxn) (uintptr_t arg) |
IPC OSAL ISR callback function prototype. More... | |
typedef void *(* | Ipc_OsalRegisterIntrFxn) (Ipc_MbConfig *cfg, Ipc_OsalIsrFxn isrFxn, uintptr_t arg) |
IPC OSAL ISR register function prototype. More... | |
typedef void(* | Ipc_OsalUnRegisterIntrFxn) (void *hwiHandle) |
IPC OSAL ISR unregister function prototype. More... | |
typedef void(* | Ipc_NewMsgReceivedFxn) (uint32_t srcEndPt, uint32_t procId) |
IPC New message notification. More... | |
Data Structures | |
struct | Ipc_MbConfig |
Mailbox interrupt router configuration. More... | |
struct | Ipc_OsalHIsrHandle |
Second level ISR (HISR), used to complete ISR functions. More... | |
struct | Ipc_OsalPrms |
IPC driver OSAL function pointers. More... | |
#define IPC_SOK (CSL_PASS) |
API call successful.
#define IPC_EFAIL (CSL_EFAIL) |
API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure.
#define IPC_EBADARGS (CSL_EBADARGS) |
API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected.
#define IPC_EINVALID_PARAMS (CSL_EINVALID_PARAMS) |
API call returned with error as invalid parameters. Typically when parameters passed are not valid.
#define IPC_ETIMEOUT (CSL_ETIMEOUT) |
API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period.
#define IPC_EALLOC (CSL_EALLOC) |
API call returned with error as allocation failed.
#define IPC_EUNSUPPORTED (CSL_EUNSUPPORTED_CMD) |
Un Supported service request, API/IOCTLs.
#define IPC_E_UNBLOCKED (-50) |
IPC is unblocked mode.
#define IPC_INTR_INVALID (0xFFFF0000U) |
Macro used to specify that interrupt number is invalid.
#define IPC_RPMESSAGE_TIMEOUT_FOREVER ~(0) |
Timeout foreever for IPC Recv.
#define RPMESSAGE_ANY (0xFFFFFFFFU) |
RPMessage Endpoint any available.
#define RPMESSAGE_ALL (0xFFFFFFFFU) |
RPMessage type.
typedef void(* Ipc_OsalHIsrFxn) (uintptr_t arg0, uintptr_t arg1) |
IPC OSAL High Level ISR type.
uintptr_t | arg1, expected to be of type RPMessage_CallbackData |
uintptr_t | arg2, not used |
typedef void* Ipc_OsalHIsrGateHandle |
High Level ISR handle.
typedef uint32_t(* Ipc_VirtToPhyFxn) (const void *virtAddr) |
IPC Virtual to Physical address translation callback function.
This function is used by the driver to convert virtual address to physical address.
virtAddr | [IN] Virtual address |
typedef void*(* Ipc_PhyToVirtFxn) (uint32_t phyAddr) |
IPC Physical to Virtual address translation callback function.
This function is used by the driver to convert physical address to virtual address.
phyAddr | [IN] Physical address |
typedef void(* Ipc_PrintFxn) (const char *str) |
IPC info/debug print function prototype.
This function is used by the driver to print info/debug messages.
str | [OUT] Info string to print. |
typedef uintptr_t(* Ipc_OsalDisableAllIntrFxn) (void) |
IPC OSAL interrupt disable function prototype.
typedef void(* Ipc_OsalRestoreAllIntrFxn) (uintptr_t cookie) |
IPC OSAL interrupt restore function prototype.
cookie | [IN] This is returned in disable interrupt function |
typedef Ipc_OsalHIsrGateHandle(* Ipc_OsalCreateHIsrMutexFxn) (void) |
IPC OSAL create high level interrupt lock.
None |
typedef void(* Ipc_OsalDeleteHIsrMutexFxn) (Ipc_OsalHIsrGateHandle *handle) |
IPC OSAL delete high level interrupt lock.
Ipc_OsalHIsrGateHandle | Handle previously created gate |
typedef int32_t(* Ipc_OsalEnterHIsrMutexFxn) (Ipc_OsalHIsrGateHandle handle) |
IPC OSAL Lock High level ISR's.
Ipc_OsalHIsrGateHandle | Handle previously created gate |
typedef void(* Ipc_OsalExitHIsrMutexFxn) (Ipc_OsalHIsrGateHandle handle, int32_t key) |
IPC OSAL Un Lock High level ISR's.
Ipc_OsalHIsrGateHandle | Handle previously created gate |
int32_t | Unique key value, which received when locking |
typedef void*(* Ipc_OsalMutexCreateFxn) (void) |
IPC OSAL mutex create function prototype to protect critical section.
typedef void(* Ipc_OsalMutexDeleteFxn) (void *mutexHandle) |
IPC OSAL mutex delete function prototype.
mutexHandle | [IN] Pointer to mutex object returned during create |
typedef int32_t(* Ipc_OsalMutexLockFxn) (void *mutexHandle, uint32_t timeout) |
IPC OSAL mutex lock function prototype.
mutexHandle | [IN] Pointer to mutex object returned during create |
typedef void(* Ipc_OsalMutexUnlockFxn) (void *mutexHandle) |
IPC OSAL mutex lock function prototype.
mutexHandle | [IN] Pointer to mutex object returned during create |
typedef int32_t(* Ipc_OsalHIsrCreateFxn) (Ipc_OsalHIsrHandle *handle, Ipc_OsalHIsrFxn fxn, void *arg) |
IPC OSAL create high level interrupt handler.
None |
typedef void(* Ipc_OsalHIsrDeleteFxn) (Ipc_OsalHIsrHandle *handle) |
IPC OSAL delete high level interrupt handler.
Ipc_OsalHIsrHandle | Handle previously created HISR |
typedef int32_t(* Ipc_OsalHIsrPostFxn) (Ipc_OsalHIsrHandle *handle) |
IPC OSAL Lock High level ISR's.
Ipc_OsalHIsrHandle | Handle previously created HISR |
typedef void(* Ipc_OsalIsrFxn) (uintptr_t arg) |
IPC OSAL ISR callback function prototype.
arg | [IN] App data |
typedef void*(* Ipc_OsalRegisterIntrFxn) (Ipc_MbConfig *cfg, Ipc_OsalIsrFxn isrFxn, uintptr_t arg) |
IPC OSAL ISR register function prototype.
cfg | [IN] Defines interrupt details Ipc_MbConfig |
isrFxn | [IN] ISR callback fxn pointer |
arg | [IN] Arg that will be passed back in the ISR |
typedef void(* Ipc_OsalUnRegisterIntrFxn) (void *hwiHandle) |
IPC OSAL ISR unregister function prototype.
hwiHandle | [IN] HWI handle |
typedef void(* Ipc_NewMsgReceivedFxn) (uint32_t srcEndPt, uint32_t procId) |
IPC New message notification.
srcEndPt | [IN] Specifies the source end point number |
srcProcId | [IN] Specifies the source processor identifier |