64 #define IPC_SOK (CSL_PASS) 68 #define IPC_EFAIL (CSL_EFAIL) 72 #define IPC_EBADARGS (CSL_EBADARGS) 76 #define IPC_EINVALID_PARAMS (CSL_EINVALID_PARAMS) 81 #define IPC_ETIMEOUT (CSL_ETIMEOUT) 84 #define IPC_EALLOC (CSL_EALLOC) 87 #define IPC_EUNSUPPORTED (CSL_EUNSUPPORTED_CMD) 90 #define IPC_E_UNBLOCKED (-50) 93 #define IPC_INTR_INVALID (0xFFFF0000U) 98 #define IPC_RPMESSAGE_TIMEOUT_FOREVER ~(0) 103 #define RPMESSAGE_ANY (0xFFFFFFFFU) 108 #define RPMESSAGE_ALL (0xFFFFFFFFU) 113 typedef struct Ipc_MbConfig_s
135 typedef struct Ipc_OsalHIsrHandle_s
174 typedef void *(*Ipc_PhyToVirtFxn)(uint32_t phyAddr);
242 typedef void * (*Ipc_OsalMutexCreateFxn)(void);
331 typedef struct Ipc_OsalPrms_s
void *(* Ipc_OsalRegisterIntrFxn)(Ipc_MbConfig *cfg, Ipc_OsalIsrFxn isrFxn, uintptr_t arg)
IPC OSAL ISR register function prototype.
Definition: ipc_types.h:309
Mailbox interrupt router configuration.
Definition: ipc_types.h:113
Ipc_OsalHIsrPostFxn postHIsr
Definition: ipc_types.h:342
Ipc_OsalHIsrDeleteFxn deleteHIsr
Definition: ipc_types.h:340
uint32_t eventIdBase
Definition: ipc_types.h:119
void(* Ipc_OsalDeleteHIsrMutexFxn)(Ipc_OsalHIsrGateHandle *handle)
IPC OSAL delete high level interrupt lock.
Definition: ipc_types.h:215
uint32_t priority
Definition: ipc_types.h:115
int32_t(* Ipc_OsalHIsrCreateFxn)(Ipc_OsalHIsrHandle *handle, Ipc_OsalHIsrFxn fxn, void *arg)
IPC OSAL create high level interrupt handler.
Definition: ipc_types.h:272
Ipc_OsalEnterHIsrMutexFxn lockHIsrGate
Definition: ipc_types.h:349
uint32_t(* Ipc_VirtToPhyFxn)(const void *virtAddr)
IPC Virtual to Physical address translation callback function.
Definition: ipc_types.h:162
int32_t(* Ipc_OsalMutexLockFxn)(void *mutexHandle, uint32_t timeout)
IPC OSAL mutex lock function prototype.
Definition: ipc_types.h:256
uint32_t eventId
Definition: ipc_types.h:116
Ipc_OsalRegisterIntrFxn registerIntr
Definition: ipc_types.h:364
Ipc_OsalCreateHIsrMutexFxn createHIsrGate
Definition: ipc_types.h:345
Ipc_OsalHIsrFxn hIsrFxn
Definition: ipc_types.h:141
void(* Ipc_OsalHIsrFxn)(uintptr_t arg0, uintptr_t arg1)
IPC OSAL High Level ISR type.
Definition: ipc_types.h:130
uintptr_t(* Ipc_OsalDisableAllIntrFxn)(void)
IPC OSAL interrupt disable function prototype.
Definition: ipc_types.h:190
Ipc_OsalMutexCreateFxn createMutex
Definition: ipc_types.h:355
void(* Ipc_OsalMutexDeleteFxn)(void *mutexHandle)
IPC OSAL mutex delete function prototype.
Definition: ipc_types.h:249
Second level ISR (HISR), used to complete ISR functions.
Definition: ipc_types.h:135
void * Ipc_OsalHIsrGateHandle
High Level ISR handle.
Definition: ipc_types.h:150
void(* Ipc_OsalUnRegisterIntrFxn)(void *hwiHandle)
IPC OSAL ISR unregister function prototype.
Definition: ipc_types.h:318
uintptr_t arg1
Definition: ipc_types.h:139
Ipc_OsalDisableAllIntrFxn disableAllIntr
Definition: ipc_types.h:333
void(* Ipc_OsalHIsrDeleteFxn)(Ipc_OsalHIsrHandle *handle)
IPC OSAL delete high level interrupt handler.
Definition: ipc_types.h:282
Ipc_OsalDeleteHIsrMutexFxn deleteHIsrGate
Definition: ipc_types.h:347
void(* Ipc_NewMsgReceivedFxn)(uint32_t srcEndPt, uint32_t procId)
IPC New message notification.
Definition: ipc_types.h:326
Ipc_OsalExitHIsrMutexFxn unLockHIsrGate
Definition: ipc_types.h:351
void *(* Ipc_OsalMutexCreateFxn)(void)
IPC OSAL mutex create function prototype to protect critical section.
Definition: ipc_types.h:242
int32_t(* Ipc_OsalHIsrPostFxn)(Ipc_OsalHIsrHandle *handle)
IPC OSAL Lock High level ISR's.
Definition: ipc_types.h:291
Ipc_OsalRestoreAllIntrFxn restoreAllIntr
Definition: ipc_types.h:335
void(* Ipc_OsalExitHIsrMutexFxn)(Ipc_OsalHIsrGateHandle handle, int32_t key)
IPC OSAL Un Lock High level ISR's.
Definition: ipc_types.h:234
void(* Ipc_OsalMutexUnlockFxn)(void *mutexHandle)
IPC OSAL mutex lock function prototype.
Definition: ipc_types.h:263
Ipc_OsalMutexLockFxn lockMutex
Definition: ipc_types.h:359
Ipc_OsalHIsrGateHandle(* Ipc_OsalCreateHIsrMutexFxn)(void)
IPC OSAL create high level interrupt lock.
Definition: ipc_types.h:206
Ipc_OsalHIsrCreateFxn createHIsr
Definition: ipc_types.h:338
void * hLosHisrHandle
Definition: ipc_types.h:143
int32_t(* Ipc_OsalEnterHIsrMutexFxn)(Ipc_OsalHIsrGateHandle handle)
IPC OSAL Lock High level ISR's.
Definition: ipc_types.h:224
uintptr_t arg0
Definition: ipc_types.h:137
void(* Ipc_PrintFxn)(const char *str)
IPC info/debug print function prototype.
Definition: ipc_types.h:183
Ipc_OsalMutexUnlockFxn unlockMutex
Definition: ipc_types.h:361
uint32_t inputIntrNum
Definition: ipc_types.h:117
char str[32]
Definition: tisci_core.h:442
Ipc_OsalMutexDeleteFxn deleteMutex
Definition: ipc_types.h:357
IPC driver OSAL function pointers.
Definition: ipc_types.h:331
void(* Ipc_OsalIsrFxn)(uintptr_t arg)
IPC OSAL ISR callback function prototype.
Definition: ipc_types.h:298
void(* Ipc_OsalRestoreAllIntrFxn)(uintptr_t cookie)
IPC OSAL interrupt restore function prototype.
Definition: ipc_types.h:197
Ipc_OsalUnRegisterIntrFxn unRegisterIntr
Definition: ipc_types.h:366
uint32_t outputIntrNum
Definition: ipc_types.h:118