![]() |
![]() |
#include "assert.h"
#include "C6xSimulator.h"
#include "C6xSimulator_type_modifiers.h"
Include dependency graph for c66/DSPF_dp_svd.h:
Go to the source code of this file.
Defines | |
#define | MAX_ITERATION_COUNT 30 |
Functions | |
int | DSPF_dp_svd (const int Nrows, const int Ncols, double *restrict A, double *restrict U, double *restrict V, double *restrict U1, double *restrict diag, double *restrict superdiag) |
#define MAX_ITERATION_COUNT 30 |
Definition at line 42 of file c66/DSPF_dp_svd.h.