68 #include <ti/drv/udma/soc/udma_soc.h> 70 #include <ti/csl/soc.h> 71 #include <ti/csl/csl_psilcfg.h> 72 #if (UDMA_SOC_CFG_RA_NORMAL_PRESENT == 1) 73 #include <ti/csl/csl_ringacc.h> 75 #if (UDMA_SOC_CFG_RA_LCDMA_PRESENT == 1) 76 #include <ti/csl/csl_lcdma_ringacc.h> 78 #if (UDMA_SOC_CFG_UDMAP_PRESENT == 1) 79 #include <ti/csl/csl_udmap.h> 81 #if (UDMA_SOC_CFG_LCDMA_PRESENT == 1) 82 #include <ti/csl/csl_bcdma.h> 83 #include <ti/csl/csl_pktdma.h> 86 #include <ti/csl/csl_intaggr.h> 87 #include <ti/csl/csl_intr_router.h> 88 #if (UDMA_NUM_UTC_INSTANCE > 0) 89 #include <ti/csl/csl_dru.h> 91 #if (UDMA_SOC_CFG_PROXY_PRESENT == 1) 92 #include <ti/csl/csl_proxy.h> 94 #if (UDMA_SOC_CFG_CLEC_PRESENT == 1) 95 #include <ti/csl/csl_clec.h> 110 #if (UDMA_NUM_UTC_INSTANCE > 0) 150 typedef void *(*Udma_PhyToVirtFxn)(uint64_t phyAddr,
180 uint64_t phyDescMem);
183 uint64_t *phyDescMem);
185 typedef void *(*Udma_ringGetMemPtrFxn)(Udma_RingHandle ringHandle);
200 Udma_RingHandle ringHandle,
201 uint64_t *phyDescMem);
204 Udma_RingHandle ringHandle,
205 uint64_t phyDescMem);
208 Udma_RingHandle ringHandle,
209 uint64_t *phyDescMem);
212 Udma_RingHandle ringHandle,
389 return ((uint64_t) virtAddr);
396 #if defined (__aarch64__) 397 uint64_t temp = phyAddr;
400 uint32_t temp = (uint32_t) phyAddr;
403 return ((
void *) temp);
423 #if (UDMA_SOC_CFG_UDMAP_PRESENT == 1) 430 #if (UDMA_SOC_CFG_LCDMA_PRESENT == 1) 434 CSL_BcdmaCfg bcdmaRegs;
436 CSL_PktdmaCfg pktdmaRegs;
439 #if (UDMA_SOC_CFG_RA_NORMAL_PRESENT == 1) 442 #if (UDMA_SOC_CFG_RA_LCDMA_PRESENT == 1) 443 CSL_LcdmaRingaccCfg lcdmaRaRegs;
448 #if (UDMA_NUM_UTC_INSTANCE > 0) 463 #if (UDMA_SOC_CFG_PROXY_PRESENT == 1) 467 CSL_ProxyCfg proxyCfg;
469 CSL_ProxyTargetParams proxyTargetRing;
471 uint32_t proxyTargetNumRing;
475 #if (UDMA_SOC_CFG_CLEC_PRESENT == 1) 479 CSL_CLEC_EVTRegs *clecRegs;
501 #if (UDMA_SOC_CFG_PROXY_PRESENT == 1) 507 #if (UDMA_NUM_UTC_INSTANCE > 0) 603 #if (UDMA_NUM_UTC_INSTANCE > 0) 607 #if (UDMA_NUM_MAPPED_TX_GROUP > 0) 611 #if (UDMA_NUM_MAPPED_RX_GROUP > 0) 615 #if ((UDMA_NUM_MAPPED_TX_GROUP + UDMA_NUM_MAPPED_RX_GROUP) > 0) static void * Udma_defaultPhyToVirtFxn(uint64_t phyAddr, uint32_t chNum, void *appData)
Default physical to virtual translation function.
Definition: udma.h:392
OS Abstraction Layer header.
uint32_t rxUhcChFlag[UDMA_RM_RX_UHC_CH_ARR_SIZE]
Definition: udma.h:600
uint32_t instType
Definition: udma.h:418
Udma_ringGetModeFxn ringGetMode
Definition: udma.h:657
UDMA ring parameters.
Definition: udma_ring.h:133
uint32_t rxChOffset
Definition: udma.h:547
uint32_t(* Udma_ringGetElementCntFxn)(Udma_RingHandle ringHandle)
UDMA Ring get element count function prototype.
Definition: udma.h:189
uint32_t(* Udma_ringGetReverseRingOccFxn)(Udma_RingHandle ringHandle)
UDMA Ring get reverse ring occupancy function prototype.
Definition: udma.h:193
#define UDMA_RM_RX_UHC_CH_ARR_SIZE
Definition: udma_cfg.h:104
#define UDMA_RM_TX_UHC_CH_ARR_SIZE
Definition: udma_cfg.h:101
void(* Udma_ringSetDoorBellFxn)(Udma_RingHandle ringHandle, int32_t count)
UDMA Ring set doorbell function prototype.
Definition: udma.h:176
uint32_t freeRingFlag[UDMA_RM_FREE_RING_ARR_SIZE]
Definition: udma.h:620
uint32_t proxyFlag[UDMA_RM_PROXY_ARR_SIZE]
Definition: udma.h:630
#define UDMA_RM_MAPPED_RX_CH_ARR_SIZE
Definition: udma_cfg.h:107
uint32_t skipRmOverlapCheck
Definition: udma.h:232
uint32_t txRingIrqOffset
Definition: udma.h:523
uint32_t extChOffset
Definition: udma.h:545
Udma_ringFlushRawFxn ringFlushRaw
Definition: udma.h:651
uint32_t txUhcChFlag[UDMA_RM_TX_UHC_CH_ARR_SIZE]
Definition: udma.h:593
uint32_t count
Definition: tisci_rm_ra.h:166
#define UDMA_RM_MAPPED_RING_ARR_SIZE
Definition: udma_cfg.h:108
UDMA utility API to make TR, get TR descriptor memory requirement.
Udma_ringGetReverseRingOccFxn ringGetReverseRingOcc
Definition: udma.h:661
#define UDMA_RM_VINTR_ARR_SIZE
Definition: udma_cfg.h:112
uint16_t devIdPsil
Definition: udma.h:495
uint32_t vintrFlag[UDMA_RM_VINTR_ARR_SIZE]
Definition: udma.h:626
UDMA initialization parameters.
Definition: udma.h:225
This file contains prototypes for APIs contained as a part of SCICLIENT as well as the structures of ...
uint32_t txHcChFlag[UDMA_RM_TX_HC_CH_ARR_SIZE]
Definition: udma.h:591
uint32_t txChOffset
Definition: udma.h:543
UDMA OSAL related parameters and API.
int32_t Udma_init(Udma_DrvHandle drvHandle, const Udma_InitPrms *initPrms)
UDMA init function.
uint32_t instId
Definition: udma.h:227
Udma_RmInitPrms rmInitPrms
Definition: udma.h:230
uint32_t maxProxy
Definition: udma.h:458
Udma_ringGetWrIdxFxn ringGetWrIdx
Definition: udma.h:663
Udma_ringGetRdIdxFxn ringGetRdIdx
Definition: udma.h:665
Udma_ringSetDoorBellFxn ringSetDoorBell
Definition: udma.h:671
#define UDMA_RM_RING_MON_ARR_SIZE
Definition: udma_cfg.h:115
uint32_t(* Udma_ringGetModeFxn)(Udma_RingHandle ringHandle)
UDMA Ring get ring mode function prototype.
Definition: udma.h:187
uint32_t blkCopyHcChFlag[UDMA_RM_BLK_COPY_HC_CH_ARR_SIZE]
Definition: udma.h:584
uint32_t drvInitDone
Definition: udma.h:574
void * printLock
Definition: udma.h:637
uint32_t udmapSrcThreadOffset
Definition: udma.h:452
uint16_t devIdRing
Definition: udma.h:491
void *(* Udma_PhyToVirtFxn)(uint64_t phyAddr, uint32_t chNum, void *appData)
UDMA Physical to Virtual address translation callback function.
Definition: udma.h:150
uint32_t(* Udma_ringGetRdIdxFxn)(Udma_RingHandle ringHandle)
UDMA Ring get read index value function prototype.
Definition: udma.h:197
#define UDMA_RM_GLOBAL_EVENT_ARR_SIZE
Definition: udma_cfg.h:111
uint32_t maxRingMon
Definition: udma.h:460
uint32_t ringMonFlag[UDMA_RM_RING_MON_ARR_SIZE]
Definition: udma.h:632
uint64_t(* Udma_VirtToPhyFxn)(const void *virtAddr, uint32_t chNum, void *appData)
UDMA Virtual to Physical address translation callback function.
Definition: udma.h:135
Udma_ringPrimeReadFxn ringPrimeRead
Definition: udma.h:669
uint32_t rxRingIrqOffset
Definition: udma.h:525
Udma_OsalPrms osalPrms
Definition: udma.h:262
CSL_RingAccCfg contains information to configure the ring accelerator.
Definition: csl_ringacc.h:219
UDMA driver object.
Definition: udma.h:416
void(* Udma_PrintFxn)(const char *str)
UDMA info/debug print function prototype.
Definition: udma.h:161
uint32_t iaGemOffset
Definition: udma.h:561
Udma_VirtToPhyFxn virtToPhyFxn
Definition: udma.h:242
CSL_IntaggrCfg iaRegs
Definition: udma.h:446
#define UDMA_NUM_UTC_INSTANCE
Number of UTC instance.
Definition: udma_soc.h:167
#define UDMA_RM_IR_INTR_ARR_SIZE
Definition: udma_cfg.h:113
Udma_ringSetCfgFxn ringSetCfg
Definition: udma.h:673
uint16_t srcIdTrIrq
Definition: udma.h:532
UDMA ring related parameters and API.
#define UDMA_RM_RX_HC_CH_ARR_SIZE
Definition: udma_cfg.h:103
#define UDMA_RM_BLK_COPY_UHC_CH_ARR_SIZE
Definition: udma_cfg.h:98
#define UDMA_RM_BLK_COPY_CH_ARR_SIZE
Definition: udma_cfg.h:96
UDMA Low Level Driver API/interface data types file.
#define UDMA_RM_UTC_CH_ARR_SIZE
Definition: udma_cfg.h:105
void * rmLock
Definition: udma.h:635
uint32_t rxChFlag[UDMA_RM_RX_CH_ARR_SIZE]
Definition: udma.h:596
uint16_t devIdCore
Definition: udma.h:505
#define UDMA_RM_MAPPED_TX_CH_ARR_SIZE
Definition: udma_cfg.h:106
#define UDMA_RM_RX_CH_ARR_SIZE
Definition: udma_cfg.h:102
UDMA Channel related parameters and API.
Udma_EventHandle globalEventHandle
Definition: udma.h:569
Udma_ringDequeueRawFxn ringDequeueRaw
Definition: udma.h:647
uint32_t txTrIrqOffset
Definition: udma.h:536
uint32_t blkCopyChFlag[UDMA_RM_BLK_COPY_CH_ARR_SIZE]
Definition: udma.h:582
uint32_t blkCopyTrIrqOffset
Definition: udma.h:534
uint32_t globalEventFlag[UDMA_RM_GLOBAL_EVENT_ARR_SIZE]
Definition: udma.h:624
int32_t(* Udma_ringDequeueRawFxn)(Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem)
UDMA Ring dequeue raw function prototype.
Definition: udma.h:199
Udma_ringPrimeFxn ringPrime
Definition: udma.h:667
uint32_t irIntrFlag[UDMA_RM_IR_INTR_ARR_SIZE]
Definition: udma.h:628
UDMA configuration parameters.
static uint64_t Udma_defaultVirtToPhyFxn(const void *virtAddr, uint32_t chNum, void *appData)
Default virtual to physical translation function.
Definition: udma.h:385
uint32_t udmapDestThreadOffset
Definition: udma.h:454
uint32_t txChFlag[UDMA_RM_TX_CH_ARR_SIZE]
Definition: udma.h:589
#define UDMA_RM_FREE_FLOW_ARR_SIZE
Definition: udma_cfg.h:110
void(* Udma_ringPrimeReadFxn)(Udma_RingHandle ringHandle, uint64_t *phyDescMem)
UDMA Ring prime read function prototype.
Definition: udma.h:182
uint32_t freeFlowFlag[UDMA_RM_FREE_FLOW_ARR_SIZE]
Definition: udma.h:622
Udma_ringGetMemPtrFxn ringGetMemPtr
Definition: udma.h:655
Udma_ringGetForwardRingOccFxn ringGetForwardRingOcc
Definition: udma.h:659
char printBuf[UDMA_CFG_PRINT_BUF_LEN]
Definition: udma.h:639
Header file containing various enumerations, structure definitions and function declarations for CPPI...
UDMA DRU related parameters and API.
UDMA event related parameters and API.
struct Udma_EventObj globalEventObj
Definition: udma.h:567
void *(* Udma_ringGetMemPtrFxn)(Udma_RingHandle ringHandle)
UDMA Ring get mem pointer function prototype.
Definition: udma.h:185
uint32_t maxRings
Definition: udma.h:456
Udma_ringHandleClearRegsFxn ringHandleClearRegs
Definition: udma.h:675
Udma_ringQueueRawFxn ringQueueRaw
Definition: udma.h:649
UDMA RM related parameters and API.
uint32_t skipGlobalEventReg
Definition: udma.h:236
Udma_PhyToVirtFxn phyToVirtFxn
Definition: udma.h:250
void(* Udma_ringPrimeFxn)(Udma_RingHandle ringHandle, uint64_t phyDescMem)
UDMA Ring prime function prototype.
Definition: udma.h:179
int32_t(* Udma_ringFlushRawFxn)(Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem)
UDMA Ring flush raw function prototype.
Definition: udma.h:207
#define UDMA_NUM_MAPPED_TX_GROUP
Number of Mapped TX Group.
Definition: udma_soc.h:141
uint32_t(* Udma_ringGetWrIdxFxn)(Udma_RingHandle ringHandle)
UDMA Ring get write index value function prototype.
Definition: udma.h:195
UDMA flow related parameters and API.
Udma_PrintFxn printFxn
Definition: udma.h:258
void(* Udma_ringHandleClearRegsFxn)(Udma_RingHandle ringHandle)
UDMA Ring handle clear register function prototype.
Definition: udma.h:174
#define UDMA_RM_TX_HC_CH_ARR_SIZE
Definition: udma_cfg.h:100
Udma_ringGetElementCntFxn ringGetElementCnt
Definition: udma.h:653
uint16_t srcIdRingIrq
Definition: udma.h:519
uint32_t blkCopyRingIrqOffset
Definition: udma.h:521
UDMAP configuration structure.
Definition: csl_udmap.h:482
UDMA resource manager init parameters.
Definition: udma_rm.h:89
uint32_t rxHcChFlag[UDMA_RM_RX_HC_CH_ARR_SIZE]
Definition: udma.h:598
uint32_t(* Udma_ringGetForwardRingOccFxn)(Udma_RingHandle ringHandle)
UDMA Ring get forward ring occupancy function prototype.
Definition: udma.h:191
uint32_t raType
Definition: udma.h:420
uint32_t blkCopyUhcChFlag[UDMA_RM_BLK_COPY_UHC_CH_ARR_SIZE]
Definition: udma.h:586
char str[32]
Definition: tisci_core.h:439
uint32_t trigGemOffset
Definition: udma.h:563
#define UDMA_RM_BLK_COPY_HC_CH_ARR_SIZE
Definition: udma_cfg.h:97
UDMA event object.
Definition: udma_event.h:505
#define UDMA_RM_PROXY_ARR_SIZE
Definition: udma_cfg.h:114
int32_t UdmaInitPrms_init(uint32_t instId, Udma_InitPrms *initPrms)
Udma_InitPrms structure init function.
void(* Udma_ringSetCfgFxn)(Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, const Udma_RingPrms *ringPrms)
UDMA Ring set Cfg function prototype.
Definition: udma.h:211
#define UDMA_RM_TX_CH_ARR_SIZE
Definition: udma_cfg.h:99
int32_t(* Udma_ringQueueRawFxn)(Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t phyDescMem)
UDMA Ring queue raw function prototype.
Definition: udma.h:203
UDMA driver OSAL function pointers.
Definition: udma_osal.h:166
int32_t Udma_deinit(Udma_DrvHandle drvHandle)
UDMA deinit function.
uint32_t rxTrIrqOffset
Definition: udma.h:538
uint16_t devIdUdma
Definition: udma.h:493
uint16_t devIdIr
Definition: udma.h:499
#define UDMA_RM_FREE_RING_ARR_SIZE
Definition: udma_cfg.h:109
#define UDMA_NUM_MAPPED_RX_GROUP
Number of Mapped RX Group.
Definition: udma_soc.h:154
#define UDMA_CFG_PRINT_BUF_LEN
UDMA print buffer length.
Definition: udma_cfg.h:161
Udma_InitPrms initPrms
Definition: udma.h:572
UDMA proxy related parameters and API.
uint16_t devIdIa
Definition: udma.h:497