PDK API Guide for J721E
|
UDMA DRU related parameters and API.
Go to the source code of this file.
Macros | |
UDMA UTC Type | |
#define | UDMA_UTC_TYPE_DRU (0U) |
#define | UDMA_UTC_TYPE_DRU_VHWA (1U) |
Functions | |
void | Udma_chDruSubmitTr (Udma_ChHandle chHandle, const CSL_UdmapTR *tr) |
This API does a direct TR submission to the specified channel and core ID. More... | |
uint32_t | Udma_druGetNumQueue (Udma_DrvHandle drvHandle, uint32_t utcId) |
This API returns the number of queues present in a DRU. More... | |
int32_t | Udma_druQueueConfig (Udma_DrvHandle drvHandle, uint32_t utcId, uint32_t queueId, const CSL_DruQueueConfig *queueCfg) |
This API configures the DRU queue non-real time configurations. More... | |
volatile uint64_t * | Udma_druGetTriggerRegAddr (Udma_ChHandle chHandle) |
This API returns the software triggers register address for the DRU channel. More... | |
void | UdmaDruQueueConfig_init (CSL_DruQueueConfig *queueCfg) |
CSL_DruQueueConfig structure init function. More... | |