PDK API Guide for J721E
|
Structure for H3A configuration VPAC can output only one of AF or AEWB output. This structure is used for selecting H3A output module AF/AEWB and also used for for setting module configuration. When AF is enabled as an output module, only AF will be configured. Also when AEWB module is enabled/selected as an output module, only AEWB mdule will be configured.
Data Fields | |
uint32_t | module |
Fvid2_PosConfig | pos |
H3a_AewbConfig | aewbCfg |
H3a_AfConfig | afCfg |
uint32_t | outputSize |
uint32_t H3a_Config::module |
H3A module to be configured, Refer H3a_Module for valid values
Fvid2_PosConfig H3a_Config::pos |
Position of the actual frame start for H3A
H3a_AewbConfig H3a_Config::aewbCfg |
AEWB configuration, configured only when H3A_MODULE_AEWB is selected/enabled in module
H3a_AfConfig H3a_Config::afCfg |
AF configuration, configured only when H3A_MODULE_AF is selected/enabled in module
uint32_t H3a_Config::outputSize |
Output Parameter returned by the driver, Internally driver calculates the output buffer required for the given AF/AEWB configuration and returns in this variable. Application can use to allocate H3A output buffer.