PDK API Guide for J721E
|
GLBCE control structure, passed as an argument to IOCTL_GLBCE_SET_CONFIG.
Data Fields | |
uint32_t | module |
Glbce_Config * | glbceCfg |
Glbce_PerceptConfig * | fwdPrcptCfg |
Glbce_PerceptConfig * | revPrcptCfg |
Glbce_WdrConfig * | wdrCfg |
Glbce_StatsInfo * | statsInfo |
uint32_t Glbce_Control::module |
Id of the module to be configured, could be either AF or AEWB configuration Appropriate structure pointer need to be assigned when one of these modules is selected here Refer Glbce_Module for valid values
Glbce_Config* Glbce_Control::glbceCfg |
Glbce Configuration Structure
Glbce_PerceptConfig* Glbce_Control::fwdPrcptCfg |
Forward Percept Config Configuration Structure
Glbce_PerceptConfig* Glbce_Control::revPrcptCfg |
Forward Percept Config Configuration Structure
Glbce_WdrConfig* Glbce_Control::wdrCfg |
WDR Configuration structure
Glbce_StatsInfo* Glbce_Control::statsInfo |
Stats Informaion