PDK API Guide for J721E
|
Structure containing DSS path information. This structure is used as an argument to IOCTL_DSS_DCTRL_SET_PATH. This IOCTL takes the array of edges connected between nodes.
Data Fields | |
uint32_t | numEdges |
Fvid2_GraphEdgeInfo | edgeInfo [DSS_DCTRL_MAX_EDGES] |
uint32_t Dss_DctrlPathInfo::numEdges |
Number edge in the edgeInfo array
Fvid2_GraphEdgeInfo Dss_DctrlPathInfo::edgeInfo[DSS_DCTRL_MAX_EDGES] |
List of edges connecting DSS modules. Display controller parses these edges and enables/disables input/output path in the appropriate DSS module. This edge tells which module is connected to which module enabling output in edge start module and input in edge end module.