PDK API Guide for J721E
|
CSIRX event object.
Note: This is an internal/private driver structure and should not be used or modified by caller.
Data Fields | |
Fdrv_Handle | drvHandle |
Csirx_EventPrms | eventPrms |
uint32_t | coreIntrNum |
HwiP_Handle | hwiHandle |
uint32_t | eventInitDone |
Fdrv_Handle CsirxDrv_EventObj::drvHandle |
Pointer to global driver handle.
Csirx_EventPrms CsirxDrv_EventObj::eventPrms |
Event parameters passed during event registration.
uint32_t CsirxDrv_EventObj::coreIntrNum |
Allocated core interrupt number.
HwiP_Handle CsirxDrv_EventObj::hwiHandle |
HWI handle.
uint32_t CsirxDrv_EventObj::eventInitDone |
Flag to set the event object is init. 0:Un-initialized /1: Initialized