PDK API Guide for J721E
|
CSIRX event related parameters.
Data Fields | |
uint32_t | eventGroup |
uint32_t | eventMasks |
CsirxDrv_EventCallback | eventCb |
uint32_t | intrPriority |
void * | appData |
uint32_t | coreIntrNum |
uint32_t Csirx_EventPrms::eventGroup |
Event type to register. Refer CsirxDrv_EventGroup for event groups
uint32_t Csirx_EventPrms::eventMasks |
Events to register. Application/caller can set multiple flags Refer CsirxDrv_EventTypeError for Error events
CsirxDrv_EventCallback Csirx_EventPrms::eventCb |
When callback function is set (non-NULL), the driver will allocate core level interrupt through Interrupt Router and the function will be called when the registered event occurs. When set to NULL, the API will only allocate event and no interrupt routing is performed.
uint32_t Csirx_EventPrms::intrPriority |
Priority of interrupt to register with OSAL. The interpretation depends on the OSAL implementation
void* Csirx_EventPrms::appData |
Application/caller context pointer passed back in the event callback function. This could be used by the caller to identify the channel/event for which the callback is called. This can be set to NULL, if not required by caller.
uint32_t Csirx_EventPrms::coreIntrNum |
Core interrupt number allocated. This number can be used to register with the OSAL For J7ES SoC this is auto calculated in the driver and hence should be passed as initialized value by 'Csirx_eventPrmsInit()' API