PDK API Guide for J721E
|
DSS Global MFLAG Config parameters.
Data Fields | |
uint32_t | globalMflagStart |
uint32_t | globalMflagCtrl |
uint32_t CSL_DssGlobalMFlagCfg::globalMflagStart |
Mflag start for DMA master port, used to drive mflag signal when DMA buffer is empty at the beginning of pipeline. Refer CSL_DssMflagStartMode for values
uint32_t CSL_DssGlobalMFlagCfg::globalMflagCtrl |
Mflag Control Signal. Refer CSL_DssMflagCtrl for values